<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Processor Expert SoftwareのトピックRe: debug console no option for UART 3,4,5 or 6 or USB CDC</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/debug-console-no-option-for-UART-3-4-5-or-6-or-USB-CDC/m-p/446150#M3632</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks George&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ok the FRDM-K22F board does not have 4 UARTS, however the MCU on our target board is a MK22FX512xxxx which has 6 UARTS.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However PE does not currently support this processor.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Jerome&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 18 Aug 2015 05:57:06 GMT</pubDate>
    <dc:creator>F50SC</dc:creator>
    <dc:date>2015-08-18T05:57:06Z</dc:date>
    <item>
      <title>debug console no option for UART 3,4,5 or 6 or USB CDC</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/debug-console-no-option-for-UART-3-4-5-or-6-or-USB-CDC/m-p/446148#M3630</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The appears to be no option to select a UART past UART 2 with PE as the debug console.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using the FRDM-K22F dev board AND our own target board with same processor but higher pin count package and neither&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;processor allows you to select a UART higher than UART 2???&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also there is no option to select USB CDC as the debug console.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there a way to change this?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If not, will this be supported in a future release of PE?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Jerome&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Aug 2015 00:48:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/debug-console-no-option-for-UART-3-4-5-or-6-or-USB-CDC/m-p/446148#M3630</guid>
      <dc:creator>F50SC</dc:creator>
      <dc:date>2015-08-18T00:48:02Z</dc:date>
    </item>
    <item>
      <title>Re: debug console no option for UART 3,4,5 or 6 or USB CDC</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/debug-console-no-option-for-UART-3-4-5-or-6-or-USB-CDC/m-p/446149#M3631</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Jerome Pitt:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The K22FN512xxx12 only has 3 UART (UART0/UART1/UART2) and 1 LPUART (LPUART0). That is why you cannot select UART3/4/5/...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As for the USB CDC option, that is not supported by Processor Expert. Try doing it manually as indicated in the next thread:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/522617"&gt;How do I setup the debug console to use the Virtual COM port (USB CDC driver)?&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this clarifies.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards!&lt;/P&gt;&lt;P&gt;Jorge Gonzalez&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Aug 2015 01:55:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/debug-console-no-option-for-UART-3-4-5-or-6-or-USB-CDC/m-p/446149#M3631</guid>
      <dc:creator>Jorge_Gonzalez</dc:creator>
      <dc:date>2015-08-18T01:55:05Z</dc:date>
    </item>
    <item>
      <title>Re: debug console no option for UART 3,4,5 or 6 or USB CDC</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/debug-console-no-option-for-UART-3-4-5-or-6-or-USB-CDC/m-p/446150#M3632</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks George&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ok the FRDM-K22F board does not have 4 UARTS, however the MCU on our target board is a MK22FX512xxxx which has 6 UARTS.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However PE does not currently support this processor.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Jerome&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Aug 2015 05:57:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/debug-console-no-option-for-UART-3-4-5-or-6-or-USB-CDC/m-p/446150#M3632</guid>
      <dc:creator>F50SC</dc:creator>
      <dc:date>2015-08-18T05:57:06Z</dc:date>
    </item>
  </channel>
</rss>