<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Possible bug in Processor Expert and KDS 3.0? in Processor Expert Software</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/Possible-bug-in-Processor-Expert-and-KDS-3-0/m-p/445545#M3623</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;This is 100% reproducible for me under KDS 3.0.&amp;nbsp; If I delete the Generated_Code folder and then click "Generate Processor Expert Code" (for example, if I want to clean up a project because I have removed many components), Processor Expert will create the Generated_Code folder and the SDK sub folder and the operation completes, but it will not create the other source files, like Cpu.h, Cpu.cpp, etc.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Anyone else having this problem?&amp;nbsp; If I delete only the contents of the Generated_Code folder, it usually hangs when I click the generate code button.&amp;nbsp; If it hangs on the writing files step, after closing KDS, the files referenced above appear.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 30 Oct 2015 13:53:50 GMT</pubDate>
    <dc:creator>dave408</dc:creator>
    <dc:date>2015-10-30T13:53:50Z</dc:date>
    <item>
      <title>Possible bug in Processor Expert and KDS 3.0?</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Possible-bug-in-Processor-Expert-and-KDS-3-0/m-p/445545#M3623</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;This is 100% reproducible for me under KDS 3.0.&amp;nbsp; If I delete the Generated_Code folder and then click "Generate Processor Expert Code" (for example, if I want to clean up a project because I have removed many components), Processor Expert will create the Generated_Code folder and the SDK sub folder and the operation completes, but it will not create the other source files, like Cpu.h, Cpu.cpp, etc.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Anyone else having this problem?&amp;nbsp; If I delete only the contents of the Generated_Code folder, it usually hangs when I click the generate code button.&amp;nbsp; If it hangs on the writing files step, after closing KDS, the files referenced above appear.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 30 Oct 2015 13:53:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Possible-bug-in-Processor-Expert-and-KDS-3-0/m-p/445545#M3623</guid>
      <dc:creator>dave408</dc:creator>
      <dc:date>2015-10-30T13:53:50Z</dc:date>
    </item>
    <item>
      <title>Re: Possible bug in Processor Expert and KDS 3.0?</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Possible-bug-in-Processor-Expert-and-KDS-3-0/m-p/445546#M3624</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;can you share more details, what processor, what SDK version are you using and if you use stock KDS 3.0 or whether you installed any update?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Libor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Nov 2015 07:54:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Possible-bug-in-Processor-Expert-and-KDS-3-0/m-p/445546#M3624</guid>
      <dc:creator>liborukropec</dc:creator>
      <dc:date>2015-11-02T07:54:38Z</dc:date>
    </item>
    <item>
      <title>Re: Possible bug in Processor Expert and KDS 3.0?</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Possible-bug-in-Processor-Expert-and-KDS-3-0/m-p/445547#M3625</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;This happens with the MK64FN1M0VLL12, MK22FN256VLL12, and MK22FN128VLL10, which are the processors we currently use.&amp;nbsp; I only have installed the required eclipse update for KSDK 1.2 and the MQX TAD plugin.&amp;nbsp; I am using KSDK 1.2.0.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Nov 2015 14:38:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Possible-bug-in-Processor-Expert-and-KDS-3-0/m-p/445547#M3625</guid>
      <dc:creator>dave408</dc:creator>
      <dc:date>2015-11-02T14:38:29Z</dc:date>
    </item>
    <item>
      <title>Re: Possible bug in Processor Expert and KDS 3.0?</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Possible-bug-in-Processor-Expert-and-KDS-3-0/m-p/445548#M3626</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Do you delete the Generated_Code folder inside the Eclipse, or outside (other File manager, Explorer, etc)? The latter can confuse Eclipse.\&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;EDIT: I reproduced the issue when the folder is deleted outside of the eclipse independently on Eclipse preferences for refreshing workspace. I'll log bug report.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Workaround: delete the folder inside the eclipse project explorer.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Nov 2015 13:47:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Possible-bug-in-Processor-Expert-and-KDS-3-0/m-p/445548#M3626</guid>
      <dc:creator>liborukropec</dc:creator>
      <dc:date>2015-11-03T13:47:35Z</dc:date>
    </item>
    <item>
      <title>Re: Possible bug in Processor Expert and KDS 3.0?</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Possible-bug-in-Processor-Expert-and-KDS-3-0/m-p/445549#M3627</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'd recommend to set both "Refresh" check-boxes located under "Window - Preferences - General - Workspace". This improve detection of changes, that are done on the disk outside the Eclipse.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Nov 2015 14:50:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Possible-bug-in-Processor-Expert-and-KDS-3-0/m-p/445549#M3627</guid>
      <dc:creator>MarekTrmac</dc:creator>
      <dc:date>2015-11-03T14:50:06Z</dc:date>
    </item>
    <item>
      <title>Re: Possible bug in Processor Expert and KDS 3.0?</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Possible-bug-in-Processor-Expert-and-KDS-3-0/m-p/445550#M3628</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Setting that 'Refresh' option in "Window - Preferences - General - Workspace" generally is &lt;STRONG&gt;not&lt;/STRONG&gt; recommended, as it slows down Eclipse.&lt;/P&gt;&lt;P&gt;Instead, doing an F5 (or context menu &amp;gt; Refresh) should help too.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Nov 2015 17:01:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Possible-bug-in-Processor-Expert-and-KDS-3-0/m-p/445550#M3628</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2015-11-03T17:01:20Z</dc:date>
    </item>
    <item>
      <title>Re: Possible bug in Processor Expert and KDS 3.0?</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Possible-bug-in-Processor-Expert-and-KDS-3-0/m-p/445551#M3629</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks, Libor.&amp;nbsp; I do delete it from outside of Eclipse, but I will use your workaround in the future!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Nov 2015 18:04:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Possible-bug-in-Processor-Expert-and-KDS-3-0/m-p/445551#M3629</guid>
      <dc:creator>dave408</dc:creator>
      <dc:date>2015-11-03T18:04:57Z</dc:date>
    </item>
  </channel>
</rss>