<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Different TPM clock source in SIM device in Processor Expert Software</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/Different-TPM-clock-source-in-SIM-device/m-p/444409#M3603</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Mike,&lt;/P&gt;&lt;P&gt;This is known issue that has been already fixed in the upcoming release of the KSDK 1.3.0. The release should be published in a few weeks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Marek Neuzil&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 23 Sep 2015 09:00:52 GMT</pubDate>
    <dc:creator>marek_neuzil</dc:creator>
    <dc:date>2015-09-23T09:00:52Z</dc:date>
    <item>
      <title>Different TPM clock source in SIM device</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Different-TPM-clock-source-in-SIM-device/m-p/444408#M3602</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello All,&lt;/P&gt;&lt;P&gt;I am hoping someone has seen this error and can point me to the solution.&amp;nbsp; I am new to both Kinetis (and Arm) as well as Processor Expert (PE).&lt;/P&gt;&lt;P&gt;I am using the MKL27Z256VFT4 part, which has 3 TPM units on it.&amp;nbsp; When I have two TPM units confiured with the KDSK 1.2.0/fsl_tpm I only get a compiler warning (as follows)&lt;/P&gt;&lt;P&gt;Warning: Frequency value should not be 0 Hz. (Frequency) (I get one for each TPM) but they seem to work as desired.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I add the last TPM unit (I added them in the order TPM0, TPM2 and then TPM1) I get the following error:&lt;/P&gt;&lt;P&gt;ERROR: It's illegal to set different TPM clock source in SIM device by components TPM0, TPM1. The clock source setting in SIM device is shared for all TPM instances.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This also adds another warning like above.&lt;/P&gt;&lt;P&gt;When I look at each of the TPM units in PE for clock source it shows Clock Source MCGIRCLK 8MHz.&lt;/P&gt;&lt;P&gt;All of them are set to use clockMan1 and in that I have set the TPM clock selection to disabled.&amp;nbsp; This gets rid of the error &lt;/P&gt;&lt;P&gt;Warning: The TPM clock source is overwritten by the fsl_tpm component(s).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have tried googling the error but have had no success.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am running:&lt;/P&gt;&lt;P&gt;win 8.1&lt;/P&gt;&lt;P&gt;KDS&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Version&amp;nbsp; 3.0.0&lt;/P&gt;&lt;P&gt;KSDK 1.2.0 Eclipse Update&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Version&amp;nbsp; 1.0.0.b150420&lt;/P&gt;&lt;P&gt;Processor Expert for Kinetis&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Version 3.0.0.RT7_b1515-0427&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any help or pointers would be greatly appreciated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mike&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Aug 2015 17:57:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Different-TPM-clock-source-in-SIM-device/m-p/444408#M3602</guid>
      <dc:creator>mike7</dc:creator>
      <dc:date>2015-08-17T17:57:09Z</dc:date>
    </item>
    <item>
      <title>Re: Different TPM clock source in SIM device</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Different-TPM-clock-source-in-SIM-device/m-p/444409#M3603</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Mike,&lt;/P&gt;&lt;P&gt;This is known issue that has been already fixed in the upcoming release of the KSDK 1.3.0. The release should be published in a few weeks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Marek Neuzil&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Sep 2015 09:00:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Different-TPM-clock-source-in-SIM-device/m-p/444409#M3603</guid>
      <dc:creator>marek_neuzil</dc:creator>
      <dc:date>2015-09-23T09:00:52Z</dc:date>
    </item>
    <item>
      <title>Re: Different TPM clock source in SIM device</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Different-TPM-clock-source-in-SIM-device/m-p/444410#M3604</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for letting me know Marek.&amp;nbsp; Sorry it took me so long to respond.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mike Warrem&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Oct 2015 19:05:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Different-TPM-clock-source-in-SIM-device/m-p/444410#M3604</guid>
      <dc:creator>mike7</dc:creator>
      <dc:date>2015-10-01T19:05:09Z</dc:date>
    </item>
  </channel>
</rss>