<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Processor Expert SoftwareのトピックDoes System Oscillator have to be used (with PEx) when cloning and modifying a BSP?</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/Does-System-Oscillator-have-to-be-used-with-PEx-when-cloning-and/m-p/442325#M3587</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I started with the TWRK70F120M BSP, cloned the BSP and PSP, and made clock modifications for my platform specific requirements.&amp;nbsp; Then I created a new MQX 4.1 project, used the USBD-CDC example project based on my new BSP.&amp;nbsp; I get everything compiled and deployed, however, when I attempt to pause when debugging I get a GDI Protocol error, Stop Failed.&amp;nbsp; Any ideas?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I noticed that in PEx, I cannot select System Oscillator 1 for MCG external ref. clock source in my Clock Source Setting 0.&amp;nbsp; So my question next is: Does PEx with MQX, USBD, on the BSP I chose require OSC0 as the MCG external ref. clock source?&amp;nbsp; I cannot seem to select OSC1 even though it's enabled and OSC0 is disabled.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The TWRK70F120M Tower platform uses a 50MHz oscillator for the clock on Oscillator 0 input.&amp;nbsp; Our platform uses only the 12MHz clock input to Oscillator 1, and no input to Oscillator 0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 24 Jul 2015 17:05:26 GMT</pubDate>
    <dc:creator>louiemoye</dc:creator>
    <dc:date>2015-07-24T17:05:26Z</dc:date>
    <item>
      <title>Does System Oscillator have to be used (with PEx) when cloning and modifying a BSP?</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Does-System-Oscillator-have-to-be-used-with-PEx-when-cloning-and/m-p/442325#M3587</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I started with the TWRK70F120M BSP, cloned the BSP and PSP, and made clock modifications for my platform specific requirements.&amp;nbsp; Then I created a new MQX 4.1 project, used the USBD-CDC example project based on my new BSP.&amp;nbsp; I get everything compiled and deployed, however, when I attempt to pause when debugging I get a GDI Protocol error, Stop Failed.&amp;nbsp; Any ideas?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I noticed that in PEx, I cannot select System Oscillator 1 for MCG external ref. clock source in my Clock Source Setting 0.&amp;nbsp; So my question next is: Does PEx with MQX, USBD, on the BSP I chose require OSC0 as the MCG external ref. clock source?&amp;nbsp; I cannot seem to select OSC1 even though it's enabled and OSC0 is disabled.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The TWRK70F120M Tower platform uses a 50MHz oscillator for the clock on Oscillator 0 input.&amp;nbsp; Our platform uses only the 12MHz clock input to Oscillator 1, and no input to Oscillator 0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Jul 2015 17:05:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Does-System-Oscillator-have-to-be-used-with-PEx-when-cloning-and/m-p/442325#M3587</guid>
      <dc:creator>louiemoye</dc:creator>
      <dc:date>2015-07-24T17:05:26Z</dc:date>
    </item>
    <item>
      <title>Re: Does System Oscillator have to be used (with PEx) when cloning and modifying a BSP?</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Does-System-Oscillator-have-to-be-used-with-PEx-when-cloning-and/m-p/442326#M3588</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Louie Moye:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please find this question answered in a couple other threads:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/392688"&gt;Re: Does it work to use only OSC1 for K70?&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/389169"&gt;Re: USB Unknown Device Error&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, in short: you cannot run in &lt;STRONG&gt;PEE&lt;/STRONG&gt; mode only with a 12 Mhz input on OSC1. You temporarily need RTC or OSC0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards!&lt;/P&gt;&lt;P&gt;Jorge Gonzalez&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 26 Jul 2015 22:15:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Does-System-Oscillator-have-to-be-used-with-PEx-when-cloning-and/m-p/442326#M3588</guid>
      <dc:creator>Jorge_Gonzalez</dc:creator>
      <dc:date>2015-07-26T22:15:49Z</dc:date>
    </item>
    <item>
      <title>Re: Does System Oscillator have to be used (with PEx) when cloning and modifying a BSP?</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Does-System-Oscillator-have-to-be-used-with-PEx-when-cloning-and/m-p/442327#M3589</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks - I was able to get my BSP working on my board.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Aug 2015 21:08:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Does-System-Oscillator-have-to-be-used-with-PEx-when-cloning-and/m-p/442327#M3589</guid>
      <dc:creator>louiemoye</dc:creator>
      <dc:date>2015-08-12T21:08:08Z</dc:date>
    </item>
  </channel>
</rss>