<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic How do I set FSL_USB_CDC_Device with MK24FN1M0VDC12? in Processor Expert Software</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/How-do-I-set-FSL-USB-CDC-Device-with-MK24FN1M0VDC12/m-p/438791#M3565</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm porting a project I've made with Kinetis Design Studio 3.0 for the Kinetis K21 (MK21DN512VLK5) to the Kinetis K24 (MK24FN1M0VDC12).&lt;/P&gt;&lt;P&gt;I have to use the FSL_USB_CDC_Device component but in the Component Inspector I cannot choose K24 as CPU because it is not present in the listed CPUs.&lt;/P&gt;&lt;P&gt;The options that I have for Kinetis processor are:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kinetis K20D50&lt;/P&gt;&lt;P&gt;Kinetis K20D72&lt;/P&gt;&lt;P&gt;Kinetis K21D50&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; (I used this with the MK21DN512VLK5)&lt;/P&gt;&lt;P&gt;Kinetis K21F120&lt;/P&gt;&lt;P&gt;Kinetis K22F120&lt;/P&gt;&lt;P&gt;Kinetis K22FN120&lt;/P&gt;&lt;P&gt;Kinetis K40&lt;/P&gt;&lt;P&gt;Kinetis K60&lt;/P&gt;&lt;P&gt;Kinetis K64F&lt;/P&gt;&lt;P&gt;Kinetis K70&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can I use another of these options? Which one?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Dario&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;P.S. I'm using Processor Expert for Kinetis V3.0.1&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 24 Nov 2015 17:12:33 GMT</pubDate>
    <dc:creator>darioesposito</dc:creator>
    <dc:date>2015-11-24T17:12:33Z</dc:date>
    <item>
      <title>How do I set FSL_USB_CDC_Device with MK24FN1M0VDC12?</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/How-do-I-set-FSL-USB-CDC-Device-with-MK24FN1M0VDC12/m-p/438791#M3565</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm porting a project I've made with Kinetis Design Studio 3.0 for the Kinetis K21 (MK21DN512VLK5) to the Kinetis K24 (MK24FN1M0VDC12).&lt;/P&gt;&lt;P&gt;I have to use the FSL_USB_CDC_Device component but in the Component Inspector I cannot choose K24 as CPU because it is not present in the listed CPUs.&lt;/P&gt;&lt;P&gt;The options that I have for Kinetis processor are:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kinetis K20D50&lt;/P&gt;&lt;P&gt;Kinetis K20D72&lt;/P&gt;&lt;P&gt;Kinetis K21D50&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; (I used this with the MK21DN512VLK5)&lt;/P&gt;&lt;P&gt;Kinetis K21F120&lt;/P&gt;&lt;P&gt;Kinetis K22F120&lt;/P&gt;&lt;P&gt;Kinetis K22FN120&lt;/P&gt;&lt;P&gt;Kinetis K40&lt;/P&gt;&lt;P&gt;Kinetis K60&lt;/P&gt;&lt;P&gt;Kinetis K64F&lt;/P&gt;&lt;P&gt;Kinetis K70&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can I use another of these options? Which one?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Dario&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;P.S. I'm using Processor Expert for Kinetis V3.0.1&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Nov 2015 17:12:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/How-do-I-set-FSL-USB-CDC-Device-with-MK24FN1M0VDC12/m-p/438791#M3565</guid>
      <dc:creator>darioesposito</dc:creator>
      <dc:date>2015-11-24T17:12:33Z</dc:date>
    </item>
    <item>
      <title>Re: How do I set FSL_USB_CDC_Device with MK24FN1M0VDC12?</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/How-do-I-set-FSL-USB-CDC-Device-with-MK24FN1M0VDC12/m-p/438792#M3566</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I don't have a K24FN1M, but checking the data sheet it uses the same interrupts as the K22FN120, so this setting should work. Can you give it a try?&lt;/P&gt;&lt;P&gt;If that works, I can happily add that item to the list of supported devices :-)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Nov 2015 20:14:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/How-do-I-set-FSL-USB-CDC-Device-with-MK24FN1M0VDC12/m-p/438792#M3566</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2015-11-25T20:14:44Z</dc:date>
    </item>
    <item>
      <title>Re: How do I set FSL_USB_CDC_Device with MK24FN1M0VDC12?</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/How-do-I-set-FSL-USB-CDC-Device-with-MK24FN1M0VDC12/m-p/438793#M3567</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for your answer Erich.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;At this time I cannot try the solution you proposed, but when I'll have the prototypes of the board with the K24 that the company I work for is developing (in the worst case in January, but with a bit of luck before Christmas) I will surely try it and make you know if it works.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Dario&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Nov 2015 07:53:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/How-do-I-set-FSL-USB-CDC-Device-with-MK24FN1M0VDC12/m-p/438793#M3567</guid>
      <dc:creator>darioesposito</dc:creator>
      <dc:date>2015-11-26T07:53:45Z</dc:date>
    </item>
    <item>
      <title>Re: How do I set FSL_USB_CDC_Device with MK24FN1M0VDC12?</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/How-do-I-set-FSL-USB-CDC-Device-with-MK24FN1M0VDC12/m-p/438794#M3568</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Dario:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Remember this post&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://mcuoneclipse.com/2014/10/25/usb-cdc-with-the-frdm-k64f-finally/" title="https://mcuoneclipse.com/2014/10/25/usb-cdc-with-the-frdm-k64f-finally/"&gt;USB CDC with the FRDM-K64F, finally! | MCU on Eclipse&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;and try with K64F. &amp;nbsp;This worked for me :-)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Dec 2016 14:48:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/How-do-I-set-FSL-USB-CDC-Device-with-MK24FN1M0VDC12/m-p/438794#M3568</guid>
      <dc:creator>benitoar</dc:creator>
      <dc:date>2016-12-20T14:48:54Z</dc:date>
    </item>
  </channel>
</rss>