<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Need help fr setting spi on kml25z in Processor Expert Software</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/Need-help-fr-setting-spi-on-kml25z/m-p/431908#M3517</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;I don't know if I have to set up the SS (slave selected) pin or not?&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;You should check the Slave device signal specification. Sometimes is needed to toggle SS pin by GPIO instead of by SPI peripheral. CPOL, CPHA settings should be double-checked on your side too.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;I don't know if I have to include the SPI_MasterLDD from the component library or not.&lt;/EM&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Init. component just initialize the SPI peripheral and together with PDD macros provides low level run-time functionality but there will be much more coding on your side.&lt;/LI&gt;&lt;LI&gt;SPI_MasterLDD - I would recommend remove the SPI init component from the project and use this component instead. It will initialize the SPI peripheral too + provide run-time API. When you right click on the LDD component you always find typical usage section in the help.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;best regards&lt;/P&gt;&lt;P&gt;Vojtech Filip&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 05 Oct 2015 09:23:30 GMT</pubDate>
    <dc:creator>vfilip</dc:creator>
    <dc:date>2015-10-05T09:23:30Z</dc:date>
    <item>
      <title>Need help fr setting spi on kml25z</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Need-help-fr-setting-spi-on-kml25z/m-p/431907#M3516</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, I'm trying to use for my first time the kinetis software with processor expert and I want to set up the SPI to send digital value to a DAC. I started by including from the component library Init_SPI. I selected my MOSI pin, I disabled the MISO, because my MKL25Z must only send the data to a slave, DAC, (I don't know if it is correct), now, I don't know if I have to set up the SS (slave selected) pin or not? I don't know if I have to include the SPI_MasterLDD from the component library or not. Can you guide me or show me an example? thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 03 Oct 2015 09:57:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Need-help-fr-setting-spi-on-kml25z/m-p/431907#M3516</guid>
      <dc:creator>piergiusepperan</dc:creator>
      <dc:date>2015-10-03T09:57:41Z</dc:date>
    </item>
    <item>
      <title>Re: Need help fr setting spi on kml25z</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Need-help-fr-setting-spi-on-kml25z/m-p/431908#M3517</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;I don't know if I have to set up the SS (slave selected) pin or not?&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;You should check the Slave device signal specification. Sometimes is needed to toggle SS pin by GPIO instead of by SPI peripheral. CPOL, CPHA settings should be double-checked on your side too.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;I don't know if I have to include the SPI_MasterLDD from the component library or not.&lt;/EM&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Init. component just initialize the SPI peripheral and together with PDD macros provides low level run-time functionality but there will be much more coding on your side.&lt;/LI&gt;&lt;LI&gt;SPI_MasterLDD - I would recommend remove the SPI init component from the project and use this component instead. It will initialize the SPI peripheral too + provide run-time API. When you right click on the LDD component you always find typical usage section in the help.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;best regards&lt;/P&gt;&lt;P&gt;Vojtech Filip&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 05 Oct 2015 09:23:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Need-help-fr-setting-spi-on-kml25z/m-p/431908#M3517</guid>
      <dc:creator>vfilip</dc:creator>
      <dc:date>2015-10-05T09:23:30Z</dc:date>
    </item>
    <item>
      <title>Re: Need help fr setting spi on kml25z</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Need-help-fr-setting-spi-on-kml25z/m-p/431909#M3518</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ok thanks. I have setted up the SPIMaster_LDD, so, the output pin the clock pin the clock period and so on, How can I create the function to send&amp;nbsp; data? are there specific function? I don't know how can I find it &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 05 Oct 2015 17:54:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Need-help-fr-setting-spi-on-kml25z/m-p/431909#M3518</guid>
      <dc:creator>piergiusepperan</dc:creator>
      <dc:date>2015-10-05T17:54:26Z</dc:date>
    </item>
    <item>
      <title>Re: Need help fr setting spi on kml25z</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Need-help-fr-setting-spi-on-kml25z/m-p/431910#M3519</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Hello,&lt;/P&gt;&lt;P&gt;If you open the Help of the SPIMaster_LDD component (open the context menu of the SPIMaster_LDD component in the Components windows and select the &lt;EM&gt;Help on Component&lt;/EM&gt; command), you can find code examples on the &lt;EM&gt;Typical Usage &lt;/EM&gt;page of the component's help. For example (SPIMaster_LDD without interrupts):&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#define BLOCK_SIZE 4&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;uint8_t OutData[BLOCK_SIZE] = "0123";&lt;/P&gt;&lt;P&gt;uint8_t InpData[BLOCK_SIZE];&lt;/P&gt;&lt;P&gt;volatile LDD_SPIMASTER_TError ComError = 0U;&lt;/P&gt;&lt;P&gt;LDD_TError Error;&lt;/P&gt;&lt;P&gt;LDD_TDeviceData *MySPIPtr;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;void main(void)&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&amp;nbsp; ...&lt;/P&gt;&lt;P&gt;&amp;nbsp; MySPIPtr = SM1_Init(NULL);&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Initialization of SM1 component */&lt;/P&gt;&lt;P&gt;&amp;nbsp; SM1_SelectConfiguration(MySPIPtr, 1U, 1U);&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Select chip select 1 and attribute set 1 */&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;STRONG&gt;Error = SM1_ReceiveBlock(MySPIPtr, InpData, BLOCK_SIZE); /* Request data block reception */&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&amp;nbsp; Error = SM1_SendBlock(MySPIPtr, OutData, BLOCK_SIZE);&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Start transmission/reception */&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; while (!SM1_GetBlockReceivedStatus(MySPIPtr)) {&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Wait until data block is transmitted/received */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; SM1_Main(MySPIPtr);&lt;/P&gt;&lt;P&gt;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;&amp;nbsp; SM1_SelectConfiguration(MySPIPtr, 0U, 0U);&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Select chip select 0 and attribute set 0 */&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&amp;nbsp; Error = SM1_ReceiveBlock(MySPIPtr, InpData, BLOCK_SIZE); /* Request data block reception */&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&amp;nbsp; Error = SM1_SendBlock(MySPIPtr, OutData, BLOCK_SIZE);&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Start transmission/reception */&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; while (!SM1_GetBlockReceivedStatus(MySPIPtr)) {&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Wait until data block is transmitted/received */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; SM1_Main(MySPIPtr);&lt;/P&gt;&lt;P&gt;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Marek Neuzil&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Nov 2015 07:28:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Need-help-fr-setting-spi-on-kml25z/m-p/431910#M3519</guid>
      <dc:creator>marek_neuzil</dc:creator>
      <dc:date>2015-11-27T07:28:00Z</dc:date>
    </item>
  </channel>
</rss>