<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Processor Expert SoftwareのトピックRe: _lwevent_create() causes Unhandled_ivINT_Hard_Fault interrupt</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/lwevent-create-causes-Unhandled-ivINT-Hard-Fault-interrupt/m-p/427275#M3486</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Zachary Walton:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you tell me what software (CodeWarrior, KDS, PE Driver Suite) and the version you are using?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For example I tried to create a MQX Lite project in CodeWarrior v10.6 for the KE06 and I did not see a hardfault when creating a LWEVENT. That is why I need more information to replicate the issue and report it to developers.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jorge Gonzalez&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 06 Oct 2015 00:35:59 GMT</pubDate>
    <dc:creator>Jorge_Gonzalez</dc:creator>
    <dc:date>2015-10-06T00:35:59Z</dc:date>
    <item>
      <title>_lwevent_create() causes Unhandled_ivINT_Hard_Fault interrupt</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/lwevent-create-causes-Unhandled-ivINT-Hard-Fault-interrupt/m-p/427274#M3485</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using MQX_Lite on a FRDM-KE06Z dev board, and when I try to create a lwevent group at the beginning of a task, the Unhandled_ivINT_Hard_Fault ISR is called.&amp;nbsp; I have lwevents enabled in the MQX_Lite PEx Component, but is there something else that I need to include to be able to use them?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Oct 2015 15:31:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/lwevent-create-causes-Unhandled-ivINT-Hard-Fault-interrupt/m-p/427274#M3485</guid>
      <dc:creator>zacharywalton</dc:creator>
      <dc:date>2015-10-01T15:31:03Z</dc:date>
    </item>
    <item>
      <title>Re: _lwevent_create() causes Unhandled_ivINT_Hard_Fault interrupt</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/lwevent-create-causes-Unhandled-ivINT-Hard-Fault-interrupt/m-p/427275#M3486</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Zachary Walton:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you tell me what software (CodeWarrior, KDS, PE Driver Suite) and the version you are using?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For example I tried to create a MQX Lite project in CodeWarrior v10.6 for the KE06 and I did not see a hardfault when creating a LWEVENT. That is why I need more information to replicate the issue and report it to developers.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jorge Gonzalez&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Oct 2015 00:35:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/lwevent-create-causes-Unhandled-ivINT-Hard-Fault-interrupt/m-p/427275#M3486</guid>
      <dc:creator>Jorge_Gonzalez</dc:creator>
      <dc:date>2015-10-06T00:35:59Z</dc:date>
    </item>
  </channel>
</rss>