<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Processor Expert SoftwareのトピックSYSTEM_SMC_PMPROT_VALUE and high speed mode in K66</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/SYSTEM-SMC-PMPROT-VALUE-and-high-speed-mode-in-K66/m-p/422885#M3440</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;When using K66 to set up 180 MHz high speed mode the SMC-&amp;gt;PMPROT register must be set to allow high speed mode. In KSDK 1.2.0 system_MK66F18.h sets SYSTEM_SMC_PMPROT_VALUE to 0. Since this register is a one time writeable after reset it is not possible to change this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Basic objective should be that Processor Expert clock configuration should be possible to use also for high speed mode.&lt;/P&gt;&lt;P&gt;/Peter&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Realized that this is a processor expert question only...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 03 Jun 2015 08:01:15 GMT</pubDate>
    <dc:creator>PeterFromSweden</dc:creator>
    <dc:date>2015-06-03T08:01:15Z</dc:date>
    <item>
      <title>SYSTEM_SMC_PMPROT_VALUE and high speed mode in K66</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/SYSTEM-SMC-PMPROT-VALUE-and-high-speed-mode-in-K66/m-p/422885#M3440</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;When using K66 to set up 180 MHz high speed mode the SMC-&amp;gt;PMPROT register must be set to allow high speed mode. In KSDK 1.2.0 system_MK66F18.h sets SYSTEM_SMC_PMPROT_VALUE to 0. Since this register is a one time writeable after reset it is not possible to change this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Basic objective should be that Processor Expert clock configuration should be possible to use also for high speed mode.&lt;/P&gt;&lt;P&gt;/Peter&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Realized that this is a processor expert question only...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Jun 2015 08:01:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/SYSTEM-SMC-PMPROT-VALUE-and-high-speed-mode-in-K66/m-p/422885#M3440</guid>
      <dc:creator>PeterFromSweden</dc:creator>
      <dc:date>2015-06-03T08:01:15Z</dc:date>
    </item>
    <item>
      <title>Re: SYSTEM_SMC_PMPROT_VALUE and high speed mode in K66</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/SYSTEM-SMC-PMPROT-VALUE-and-high-speed-mode-in-K66/m-p/422886#M3441</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;you can set in in CPU component. Anyway we will improve this in next release of ProcessorExpert for Kinetis SDK.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/29864iA7C12D4D9D92DE29/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;best regards&lt;/P&gt;&lt;P&gt;Vojtech Filip&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Jun 2015 09:54:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/SYSTEM-SMC-PMPROT-VALUE-and-high-speed-mode-in-K66/m-p/422886#M3441</guid>
      <dc:creator>vfilip</dc:creator>
      <dc:date>2015-06-04T09:54:09Z</dc:date>
    </item>
  </channel>
</rss>