<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Processor Expert Flexbus port size setting in Processor Expert Software</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/Processor-Expert-Flexbus-port-size-setting/m-p/418482#M3387</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;When I set Processor expert Flexbus (external bus) port size to 32 bits, It is actually setting port size to 8 bits.&amp;nbsp; I confirmed by looking at FB_CSCRn register setting in "generated code".&amp;nbsp; Has anyone else seen this issue ?&amp;nbsp; I noticed this because I am doing 32 bit wide read/write to external bus and the CPU is generating 4 bus transactions instead of 1.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Processor:&amp;nbsp; Kinetis K70&lt;/P&gt;&lt;P&gt;CodeWarrior 10.6&lt;/P&gt;&lt;P&gt;Windows 7 machine&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Jim&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 22 Jun 2015 16:55:02 GMT</pubDate>
    <dc:creator>jimbrady</dc:creator>
    <dc:date>2015-06-22T16:55:02Z</dc:date>
    <item>
      <title>Processor Expert Flexbus port size setting</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Processor-Expert-Flexbus-port-size-setting/m-p/418482#M3387</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;When I set Processor expert Flexbus (external bus) port size to 32 bits, It is actually setting port size to 8 bits.&amp;nbsp; I confirmed by looking at FB_CSCRn register setting in "generated code".&amp;nbsp; Has anyone else seen this issue ?&amp;nbsp; I noticed this because I am doing 32 bit wide read/write to external bus and the CPU is generating 4 bus transactions instead of 1.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Processor:&amp;nbsp; Kinetis K70&lt;/P&gt;&lt;P&gt;CodeWarrior 10.6&lt;/P&gt;&lt;P&gt;Windows 7 machine&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Jim&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Jun 2015 16:55:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Processor-Expert-Flexbus-port-size-setting/m-p/418482#M3387</guid>
      <dc:creator>jimbrady</dc:creator>
      <dc:date>2015-06-22T16:55:02Z</dc:date>
    </item>
    <item>
      <title>Re: Processor Expert Flexbus port size setting</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Processor-Expert-Flexbus-port-size-setting/m-p/418483#M3388</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Jim,&lt;/P&gt;&lt;P&gt;In the generate code , it seems have a bug , from the Reference Manual , when set the 32-bit port size,&lt;/P&gt;&lt;P&gt;the PS is "00", while the generate code is "01"(8 - bit port size):&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_0.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/30469iF6B1B875FDBF7B8D/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/4499i864838649FE31759/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;The workaround is change the "01" to "00" by hand , and in order to prevent the code change to "01 ," please disable the generate code of CPU at here:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/30681i1D20A48B0FB50752/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Hope it helps&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Alice Yang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Jan 2016 09:08:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Processor-Expert-Flexbus-port-size-setting/m-p/418483#M3388</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2016-01-28T09:08:28Z</dc:date>
    </item>
  </channel>
</rss>