<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Processor Expert Software中的主题 Re: Win-7 and USB-CDC</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/Win-7-and-USB-CDC/m-p/405111#M3237</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ole,&lt;/P&gt;&lt;P&gt;That seems to be typical operation.&lt;/P&gt;&lt;P&gt;If the Kinetis device disconnect and the PC application does not disconnect prior to the Kinetis "re-connecting" then the connection is not possible.&lt;/P&gt;&lt;P&gt;My general rule of thumb is that once the Kinetis device disconnects, I close out the terminal utility.&amp;nbsp; Once Kinetis re-enumerate, then open the terminal utility.&lt;/P&gt;&lt;P&gt;Not sure there is any other workaround.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;David &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 06 May 2015 14:32:06 GMT</pubDate>
    <dc:creator>DavidS</dc:creator>
    <dc:date>2015-05-06T14:32:06Z</dc:date>
    <item>
      <title>Win-7 and USB-CDC</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Win-7-and-USB-CDC/m-p/405110#M3236</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm working on a FRDM-K64 with a USB-CDC sw. After some problems I'm now able to sometimes get it to connect to my PC and communicate.&lt;/P&gt;&lt;P&gt;For the moment I'm using Win-7, TeraTerm and the FRDM-K64.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I stop my target windows removes the serial port, (pling-plong) and TeraTerm disconnects.&lt;/P&gt;&lt;P&gt;When restarting the target windows re-connects the serial port, (pling-plong), but often the serial-port is not visible to TeraTerm,&lt;/P&gt;&lt;P&gt;(COM-24 is not visible in the COM drop-down list). The Computer --&amp;gt; Manage --&amp;gt; Device Manager shows COM-24 as OK and working.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've tried to disconnect the COM-24, and re-connect. The re-connect typically ends in an infinite loop, and I have to re-boot my PC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How am I supposed to do development work on the CDC device???&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 May 2015 12:27:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Win-7-and-USB-CDC/m-p/405110#M3236</guid>
      <dc:creator>oaf</dc:creator>
      <dc:date>2015-05-06T12:27:21Z</dc:date>
    </item>
    <item>
      <title>Re: Win-7 and USB-CDC</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Win-7-and-USB-CDC/m-p/405111#M3237</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ole,&lt;/P&gt;&lt;P&gt;That seems to be typical operation.&lt;/P&gt;&lt;P&gt;If the Kinetis device disconnect and the PC application does not disconnect prior to the Kinetis "re-connecting" then the connection is not possible.&lt;/P&gt;&lt;P&gt;My general rule of thumb is that once the Kinetis device disconnects, I close out the terminal utility.&amp;nbsp; Once Kinetis re-enumerate, then open the terminal utility.&lt;/P&gt;&lt;P&gt;Not sure there is any other workaround.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;David &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 May 2015 14:32:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Win-7-and-USB-CDC/m-p/405111#M3237</guid>
      <dc:creator>DavidS</dc:creator>
      <dc:date>2015-05-06T14:32:06Z</dc:date>
    </item>
  </channel>
</rss>