<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic K70 display control with PE? in Processor Expert Software</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/K70-display-control-with-PE/m-p/398525#M3151</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Our goal is to develop a demonstration application for various SPI, I2C and UART peripherals.&lt;/P&gt;&lt;P&gt;We would like to use a TWR-K70F120 board with a twr-lcd module for the display&lt;/P&gt;&lt;P&gt;This doesn't sound to be an unusual combination since the K70 has a built-in display controller but:&lt;/P&gt;&lt;P&gt;As far as support for PE goes we are a bit lost.&lt;/P&gt;&lt;P&gt;PE supports a peripheral driver LCDC but it looks like there is no GUI library supporting this driver as a back end.&lt;/P&gt;&lt;P&gt;EGUI is a free library, has an example for the K70, but only for an IAR compiler - we are using Kinetis Design Studio.&lt;/P&gt;&lt;P&gt;The documentation for the TWR-LCD demo applications mentiones a processor expert component library to import - but I cannot find it anywhere.&lt;/P&gt;&lt;P&gt;There is a PEG software solution available but it is not clear to me whether or not it is necessary to actually purchase a license when using it with a Kinetis controller - the license description is somewhat contradicting. In addition it is not mentioned that this library will integrate with PE.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So the question is:&lt;/P&gt;&lt;P&gt;Is there any (preferably Processor expert based) support for the K70 display controller in terms of basic GUI elements?&lt;/P&gt;&lt;P&gt;TIA, Roland&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 13 Jun 2015 10:55:16 GMT</pubDate>
    <dc:creator>rolandz</dc:creator>
    <dc:date>2015-06-13T10:55:16Z</dc:date>
    <item>
      <title>K70 display control with PE?</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/K70-display-control-with-PE/m-p/398525#M3151</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Our goal is to develop a demonstration application for various SPI, I2C and UART peripherals.&lt;/P&gt;&lt;P&gt;We would like to use a TWR-K70F120 board with a twr-lcd module for the display&lt;/P&gt;&lt;P&gt;This doesn't sound to be an unusual combination since the K70 has a built-in display controller but:&lt;/P&gt;&lt;P&gt;As far as support for PE goes we are a bit lost.&lt;/P&gt;&lt;P&gt;PE supports a peripheral driver LCDC but it looks like there is no GUI library supporting this driver as a back end.&lt;/P&gt;&lt;P&gt;EGUI is a free library, has an example for the K70, but only for an IAR compiler - we are using Kinetis Design Studio.&lt;/P&gt;&lt;P&gt;The documentation for the TWR-LCD demo applications mentiones a processor expert component library to import - but I cannot find it anywhere.&lt;/P&gt;&lt;P&gt;There is a PEG software solution available but it is not clear to me whether or not it is necessary to actually purchase a license when using it with a Kinetis controller - the license description is somewhat contradicting. In addition it is not mentioned that this library will integrate with PE.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So the question is:&lt;/P&gt;&lt;P&gt;Is there any (preferably Processor expert based) support for the K70 display controller in terms of basic GUI elements?&lt;/P&gt;&lt;P&gt;TIA, Roland&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 13 Jun 2015 10:55:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/K70-display-control-with-PE/m-p/398525#M3151</guid>
      <dc:creator>rolandz</dc:creator>
      <dc:date>2015-06-13T10:55:16Z</dc:date>
    </item>
    <item>
      <title>Re: K70 display control with PE?</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/K70-display-control-with-PE/m-p/398526#M3152</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Roland,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does this thread can help you ? &lt;A href="https://community.nxp.com/message/304066"&gt;TWR-K70 + TWR-LCD-RGB demo projects&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Alice Yang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Jan 2016 09:28:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/K70-display-control-with-PE/m-p/398526#M3152</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2016-01-28T09:28:07Z</dc:date>
    </item>
  </channel>
</rss>