<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Processor Expert SoftwareのトピックRe: Processor Expert MQXLite component only works if KDS run as root (ubuntu)</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/Processor-Expert-MQXLite-component-only-works-if-KDS-run-as-root/m-p/397403#M3143</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;This known issue of Processor Expert that has been fixed in the upcoming release (it will be available soon). In KDS 2.0.0 you can use workaround that is described in the discussion thread &lt;A href="https://community.nxp.com/thread/349340"&gt;Error using MQXlite from Linux&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Marek Neuzil&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 21 Apr 2015 10:49:23 GMT</pubDate>
    <dc:creator>marek_neuzil</dc:creator>
    <dc:date>2015-04-21T10:49:23Z</dc:date>
    <item>
      <title>Processor Expert MQXLite component only works if KDS run as root (ubuntu)</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Processor-Expert-MQXLite-component-only-works-if-KDS-run-as-root/m-p/397402#M3142</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm running KDS in Ubuntu (tested on 14.04, 14.10 and 15.05).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I run KDS without root permissions (without sudo), and I add MQXLite component, I get this message:&lt;/P&gt;&lt;P&gt;"Warning: Selected version does not exist in directory \opt\Freescale\KDS_2.0.0\eclipse\ProcessorExpert\lib\mqxlite\. (MQX Lite version)"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I run KDS with sudo, no problems.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="Screenshot from 2015-04-10 08_53_37.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/50779iA1FC414ABE6FC97D/image-size/large?v=v2&amp;amp;px=999" role="button" title="Screenshot from 2015-04-10 08_53_37.png" alt="Screenshot from 2015-04-10 08_53_37.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Apr 2015 11:58:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Processor-Expert-MQXLite-component-only-works-if-KDS-run-as-root/m-p/397402#M3142</guid>
      <dc:creator>lopesjeronimo</dc:creator>
      <dc:date>2015-04-10T11:58:44Z</dc:date>
    </item>
    <item>
      <title>Re: Processor Expert MQXLite component only works if KDS run as root (ubuntu)</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Processor-Expert-MQXLite-component-only-works-if-KDS-run-as-root/m-p/397403#M3143</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;This known issue of Processor Expert that has been fixed in the upcoming release (it will be available soon). In KDS 2.0.0 you can use workaround that is described in the discussion thread &lt;A href="https://community.nxp.com/thread/349340"&gt;Error using MQXlite from Linux&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Marek Neuzil&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Apr 2015 10:49:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Processor-Expert-MQXLite-component-only-works-if-KDS-run-as-root/m-p/397403#M3143</guid>
      <dc:creator>marek_neuzil</dc:creator>
      <dc:date>2015-04-21T10:49:23Z</dc:date>
    </item>
  </channel>
</rss>