<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Processor Expert Software中的主题 Re: Re: Can anyone share sample code for a MQX-Lite ISR for LLWU?</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/Can-anyone-share-sample-code-for-a-MQX-Lite-ISR-for-LLWU/m-p/387475#M3018</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi James&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;&amp;gt; But perhaps these are cleared automatically when entering a sleep mode that uses them?&amp;nbsp; Or, maybe you only need to clear them if you plan on looking at them when you next wake up??&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Since the LLWU is in fact only active when the LLS mode is entered I could imagine that only the flags for the enabled sources need to be cleared before entering/re-entering the mode. However, I also think that it is good practice to clear the flags consistently and this is always done and 'may' solve issues when not doing so, but I never tested doing it in a different fashion.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have posted some more code from the uTasker project in case it gives any ideas. The actual LLWU is very simple (the uTasker project allows multiple interrupt handlers to be managed as well as multiple LLWU_Px pins to be assigned to each, which makes it look a bit more complicated, Most of the potentially more difficult stuff is correctly managing moving in and out of the modes, which is why I wrote that it will depend on how well the MQX / PE frame-work is prepared as to whether the "overall" operation is suitable. There is usually some preparation to be performed before going to the mode (as well as delaying in case of critical system operation) if you want to recover later, plus some clean-up work after the wake up - before the actual LLWU interrupt is called.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is the interrupt routine that handles LLWU pins and modules as three separate entities (since the pins are spead over two registers and the modules over a third).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;PRE __default_attr="c++" __jive_macro_name="code" class="jive_text_macro jive_macro_code _jivemacro_uid_14210889582421239" jivemacro_uid="_14210889582421239" modifiedtitle="true"&gt;
&lt;P&gt;static __interrupt void _wakeup_isr(void)&lt;/P&gt;
&lt;P&gt;{&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; fnHandleWakeupSources(LLWU_FLAG_ADDRESS, 0); // handle the LLWU_P0..P7 input source(s) that woke the processor&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; fnHandleWakeupSources((LLWU_FLAG_ADDRESS + 1), 8); // handle the LLWU_P8..P5 input source(s) that woke the processor&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; fnHandleWakeupSources((LLWU_FLAG_ADDRESS + 2), 16); // handle the LLWU_M0..7 peripheral source(s) that woke the processor&lt;/P&gt;
&lt;P&gt;}&lt;/P&gt;
&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The generic handling routine (allowing a user interrupt callback on each possible source and also allowing multiple ones to be handled in case a wakeup was due to multiple sources at the same time) is below:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;PRE __default_attr="c++" __jive_macro_name="code" class="_jivemacro_uid_14210891335082029 jive_text_macro jive_macro_code" jivemacro_uid="_14210891335082029"&gt;
&lt;P&gt;static void fnHandleWakeupSources(volatile unsigned char *prtFlagRegister, int iSouceStart)&lt;/P&gt;
&lt;P&gt;{&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; register unsigned char ucBit;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; register unsigned char ucFlags = *prtFlagRegister;// check whether a source woke the processor&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; if (ucFlags == 0) {&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; return;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; ucBit = 0x01;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; while (ucFlags != 0) { // while sources are flagged&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; if (ucFlags &amp;amp; ucBit) {&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ucFlags &amp;amp;= ~ucBit;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; *prtFlagRegister = ucBit; // reset the interrupt flag (write '1' to clear)&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; if (wakeup_handlers[iSouceStart] != 0) { // if there is a user handler for the source&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; uDisable_Interrupt(); // ensure interrupts remain blocked when user callback operates&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; wakeup_handlers[iSouceStart]();&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; uEnable_Interrupt();&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; iSouceStart++;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ucBit &amp;lt;&amp;lt;= 1;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;
&lt;P&gt;}&lt;/P&gt;
&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The actual configuration of the pins (as noted, it looks complicated since it allow multiple pins to be configured at the same time and has a map to convert between port pins and LLWU pins available on the particular Kinetis part) does:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;PRE __default_attr="c++" __jive_macro_name="code" class="jive_text_macro jive_macro_code _jivemacro_uid_14210892734636497" jivemacro_uid="_14210892734636497" modifiedtitle="true"&gt;
&lt;P&gt;// The port inputs are now mapped to available LLWU pins (pins that do not have LLWU functionality will not be configured)&lt;/P&gt;
&lt;P&gt;//&lt;/P&gt;
&lt;P&gt;while (ulPortBits != 0) { // handle each bit on the port&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; if (waveup_interrupt-&amp;gt;int_port_bits &amp;amp; ulBit) { // if the port bit is to be enabled&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; if (cWakeupPorts[waveup_interrupt-&amp;gt;int_port][iBitRef] != NO_WAKEUP) {&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; int iShift = ((cWakeupPorts[waveup_interrupt-&amp;gt;int_port][iBitRef]%4) * LLWU_PE_WUPE_SHIFT);&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; volatile unsigned char *ptrFlagRegister = LLWU_FLAG_ADDRESS + (cWakeupPorts[waveup_interrupt-&amp;gt;int_port][iBitRef]/8);&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; unsigned char *ptrWakeupEnable = (unsigned char *)LLWU_BLOCK + (cWakeupPorts[waveup_interrupt-&amp;gt;int_port][iBitRef]/4); // set the enable register pointer&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; unsigned char ucValueMask = (LLWU_PE_WUPE_MASK &amp;lt;&amp;lt; iShift); // set the mask in the enable register&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; *ptrWakeupEnable &amp;amp;= ~ucValueMask; // disable the wakeup functionality&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; wakeup_handlers[cWakeupPorts[waveup_interrupt-&amp;gt;int_port][iBitRef]] = waveup_interrupt-&amp;gt;int_handler; // enter the user interrupt handler for this wakeup input&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; fnEnterInterrupt(irq_LL_wakeup_ID, waveup_interrupt-&amp;gt;int_priority, _wakeup_isr); // ensure that the handler is entered&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; *ptrFlagRegister = (LLWU_F_WUF0 &amp;lt;&amp;lt; (cWakeupPorts[waveup_interrupt-&amp;gt;int_port][iBitRef]%8)); // reset pending flags&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; *ptrWakeupEnable |= (ucInterruptType &amp;lt;&amp;lt; iShift); // set/enable the type required&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; else {&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; _EXCEPTION("Invalid wakeup port bit being selected!");&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ulPortBits &amp;amp;= ~ulBit;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; ulBit &amp;lt;&amp;lt;= 1;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; iBitRef++;&lt;/P&gt;
&lt;P&gt;}&lt;/P&gt;
&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For each pin enabled, the sequence (in the middle) is however:&lt;/P&gt;&lt;P&gt;1. Disable the pin's wakeup functionality (although it isn't actually function in the processor's RUN state any way)&lt;/P&gt;&lt;P&gt;2. Enter its (new) interrupt handler&lt;/P&gt;&lt;P&gt;3. Reset pending flags on the source&lt;/P&gt;&lt;P&gt;4. Set the pin mode to enable its operation&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In fact there are only about about 4 lines of code that actually do any LLWU register/interrupt configuration - the rest is more overall system design/operation on the bigger scale.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 12 Jan 2015 19:10:59 GMT</pubDate>
    <dc:creator>mjbcswitzerland</dc:creator>
    <dc:date>2015-01-12T19:10:59Z</dc:date>
    <item>
      <title>Can anyone share sample code for a MQX-Lite ISR for LLWU?</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Can-anyone-share-sample-code-for-a-MQX-Lite-ISR-for-LLWU/m-p/387472#M3015</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-family: verdana,geneva; font-size: 12pt;"&gt;I want to use the LLS mode of the Kinesis K24 processor we are using for sleep mode.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: verdana,geneva; font-size: 12pt;"&gt;We are using Processor Expert 10.4 and I finally found the "Init_LLWU" component [HINT: it is NOT added automatically when you set STOP operation mode to LLS or VLLS3] and added that.&amp;nbsp; And I think I have correctly configured the pin I want to wake the device (LLWU pin 4).&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: verdana,geneva; font-size: 12pt;"&gt;However, this component generates an error if you do not enter a name in the "ISR Name" field.&amp;nbsp; [ASIDE: This is true whether or not the "Interrupt request" checkbox is checked so it's not clear what that checkbox is doing--if anything.&amp;nbsp; Is this a bug?]&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: verdana,geneva; font-size: 12pt;"&gt;Once I enter a name, I can successfully "Generate Processor Expert Code."&amp;nbsp; However, when I try to build the project, the linker (IAR in this case) complains about there being no definition for the ISR.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: verdana,geneva; font-size: 12pt;"&gt;Can anyone provide an example of a simple ISR that can be linked in to handle this interrupt.&amp;nbsp; All it needs to do is to allow the processor to continue running after an edge is detected on the GPIO (I'm using PTA13 which I have also shared with an ExtInt_LDD component).&amp;nbsp; While I can find multiple examples of how to use the low-power modes when running on a bare-metal processor, I have been unable to find one that uses MQX-Lite.&amp;nbsp; This is surprising since I'd think that the majority of users of these processors would need to put the processor into one of the low-power modes sooner or later!!&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: verdana,geneva; font-size: 12pt;"&gt;Anyhow, any help will be appreciated!!&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: verdana,geneva; font-size: 12pt;"&gt;Thanks in advance,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: verdana,geneva; font-size: 12pt;"&gt;James&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Jan 2015 01:20:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Can-anyone-share-sample-code-for-a-MQX-Lite-ISR-for-LLWU/m-p/387472#M3015</guid>
      <dc:creator>jvasil</dc:creator>
      <dc:date>2015-01-06T01:20:06Z</dc:date>
    </item>
    <item>
      <title>Re: Can anyone share sample code for a MQX-Lite ISR for LLWU?</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Can-anyone-share-sample-code-for-a-MQX-Lite-ISR-for-LLWU/m-p/387473#M3016</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi James&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can't help with PE (or MQX lite) but the LLS mode/LLWU is fully integrated in the uTasker project as detailed here:&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.utasker.com/kinetis/LLWU.html" title="http://www.utasker.com/kinetis/LLWU.html"&gt;http://www.utasker.com/kinetis/LLWU.html&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you have a TWR-K24F120M you can also load reference binary to it showing LLS mode recovery via LLWU inputs (it will temporarily recover when SW2 [LLWUP10] is pressed before automatically moving back to the LLS mode after work is done, or it will wake and restore the original power mode (120MHz operation with full-functionality) when there is an event on LLWU_P4 [the one you want]):&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.utasker.com/kinetis/TWR-K24F120M.html" title="http://www.utasker.com/kinetis/TWR-K24F120M.html"&gt;µTasker Kinetis TWR-K24F120M support&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you have a specific question about the LLWU I can certainly help but I don't know whether MQX/PE allow a complete integration (without various other work) to achieve the same level of functionality.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.utasker.com/kinetis.html" title="http://www.utasker.com/kinetis.html"&gt;http://www.utasker.com/kinetis.html&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;P.S. The LLWU is integrated in the uTasker Kinetis simulator and allows it to be fully verified without the need for HW.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;P.P.S. In case you need boot loaders these are also available at the K24 link (KBOOT compatible UART, USB-HID in parallel with USB-MSD or SD-card loading). These can be used together with applications developed in any environment.&lt;BR /&gt;&lt;/EM&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 11 Jan 2015 22:25:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Can-anyone-share-sample-code-for-a-MQX-Lite-ISR-for-LLWU/m-p/387473#M3016</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2015-01-11T22:25:57Z</dc:date>
    </item>
    <item>
      <title>Re: Can anyone share sample code for a MQX-Lite ISR for LLWU?</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Can-anyone-share-sample-code-for-a-MQX-Lite-ISR-for-LLWU/m-p/387474#M3017</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the info, Mark.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In another discussion, I found a comment that said something about needing to call CPU_SetOperationMode from the LLWU ISR.&amp;nbsp; I suspect this is similar to the calls to fnSetLowPowerMode that exist in the uTasker code you shared.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Solely from reading the processor datasheet I thought that I'd also need to clear the flags that indicate the source of the wakeup.&amp;nbsp; Something like:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Clear flags that may have caused wakeup.. */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; LLWU_F1 = LLWU_F1_VALUE;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; LLWU_F2 = LLWU_F2_VALUE;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; LLWU_FILT1 = LLWU_FILT1_VALUE;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; LLWU_FILT2 = LLWU_FILT2_VALUE;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But perhaps these are cleared automatically when entering a sleep mode that uses them?&amp;nbsp; Or, maybe you only need to clear them if you plan on looking at them when you next wake up??&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In any event, thanks for the help!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;James&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Jan 2015 18:37:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Can-anyone-share-sample-code-for-a-MQX-Lite-ISR-for-LLWU/m-p/387474#M3017</guid>
      <dc:creator>jvasil</dc:creator>
      <dc:date>2015-01-12T18:37:06Z</dc:date>
    </item>
    <item>
      <title>Re: Re: Can anyone share sample code for a MQX-Lite ISR for LLWU?</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Can-anyone-share-sample-code-for-a-MQX-Lite-ISR-for-LLWU/m-p/387475#M3018</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi James&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;&amp;gt; But perhaps these are cleared automatically when entering a sleep mode that uses them?&amp;nbsp; Or, maybe you only need to clear them if you plan on looking at them when you next wake up??&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Since the LLWU is in fact only active when the LLS mode is entered I could imagine that only the flags for the enabled sources need to be cleared before entering/re-entering the mode. However, I also think that it is good practice to clear the flags consistently and this is always done and 'may' solve issues when not doing so, but I never tested doing it in a different fashion.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have posted some more code from the uTasker project in case it gives any ideas. The actual LLWU is very simple (the uTasker project allows multiple interrupt handlers to be managed as well as multiple LLWU_Px pins to be assigned to each, which makes it look a bit more complicated, Most of the potentially more difficult stuff is correctly managing moving in and out of the modes, which is why I wrote that it will depend on how well the MQX / PE frame-work is prepared as to whether the "overall" operation is suitable. There is usually some preparation to be performed before going to the mode (as well as delaying in case of critical system operation) if you want to recover later, plus some clean-up work after the wake up - before the actual LLWU interrupt is called.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is the interrupt routine that handles LLWU pins and modules as three separate entities (since the pins are spead over two registers and the modules over a third).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;PRE __default_attr="c++" __jive_macro_name="code" class="jive_text_macro jive_macro_code _jivemacro_uid_14210889582421239" jivemacro_uid="_14210889582421239" modifiedtitle="true"&gt;
&lt;P&gt;static __interrupt void _wakeup_isr(void)&lt;/P&gt;
&lt;P&gt;{&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; fnHandleWakeupSources(LLWU_FLAG_ADDRESS, 0); // handle the LLWU_P0..P7 input source(s) that woke the processor&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; fnHandleWakeupSources((LLWU_FLAG_ADDRESS + 1), 8); // handle the LLWU_P8..P5 input source(s) that woke the processor&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; fnHandleWakeupSources((LLWU_FLAG_ADDRESS + 2), 16); // handle the LLWU_M0..7 peripheral source(s) that woke the processor&lt;/P&gt;
&lt;P&gt;}&lt;/P&gt;
&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The generic handling routine (allowing a user interrupt callback on each possible source and also allowing multiple ones to be handled in case a wakeup was due to multiple sources at the same time) is below:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;PRE __default_attr="c++" __jive_macro_name="code" class="_jivemacro_uid_14210891335082029 jive_text_macro jive_macro_code" jivemacro_uid="_14210891335082029"&gt;
&lt;P&gt;static void fnHandleWakeupSources(volatile unsigned char *prtFlagRegister, int iSouceStart)&lt;/P&gt;
&lt;P&gt;{&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; register unsigned char ucBit;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; register unsigned char ucFlags = *prtFlagRegister;// check whether a source woke the processor&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; if (ucFlags == 0) {&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; return;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; ucBit = 0x01;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; while (ucFlags != 0) { // while sources are flagged&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; if (ucFlags &amp;amp; ucBit) {&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ucFlags &amp;amp;= ~ucBit;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; *prtFlagRegister = ucBit; // reset the interrupt flag (write '1' to clear)&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; if (wakeup_handlers[iSouceStart] != 0) { // if there is a user handler for the source&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; uDisable_Interrupt(); // ensure interrupts remain blocked when user callback operates&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; wakeup_handlers[iSouceStart]();&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; uEnable_Interrupt();&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; iSouceStart++;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ucBit &amp;lt;&amp;lt;= 1;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;
&lt;P&gt;}&lt;/P&gt;
&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The actual configuration of the pins (as noted, it looks complicated since it allow multiple pins to be configured at the same time and has a map to convert between port pins and LLWU pins available on the particular Kinetis part) does:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;PRE __default_attr="c++" __jive_macro_name="code" class="jive_text_macro jive_macro_code _jivemacro_uid_14210892734636497" jivemacro_uid="_14210892734636497" modifiedtitle="true"&gt;
&lt;P&gt;// The port inputs are now mapped to available LLWU pins (pins that do not have LLWU functionality will not be configured)&lt;/P&gt;
&lt;P&gt;//&lt;/P&gt;
&lt;P&gt;while (ulPortBits != 0) { // handle each bit on the port&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; if (waveup_interrupt-&amp;gt;int_port_bits &amp;amp; ulBit) { // if the port bit is to be enabled&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; if (cWakeupPorts[waveup_interrupt-&amp;gt;int_port][iBitRef] != NO_WAKEUP) {&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; int iShift = ((cWakeupPorts[waveup_interrupt-&amp;gt;int_port][iBitRef]%4) * LLWU_PE_WUPE_SHIFT);&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; volatile unsigned char *ptrFlagRegister = LLWU_FLAG_ADDRESS + (cWakeupPorts[waveup_interrupt-&amp;gt;int_port][iBitRef]/8);&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; unsigned char *ptrWakeupEnable = (unsigned char *)LLWU_BLOCK + (cWakeupPorts[waveup_interrupt-&amp;gt;int_port][iBitRef]/4); // set the enable register pointer&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; unsigned char ucValueMask = (LLWU_PE_WUPE_MASK &amp;lt;&amp;lt; iShift); // set the mask in the enable register&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; *ptrWakeupEnable &amp;amp;= ~ucValueMask; // disable the wakeup functionality&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; wakeup_handlers[cWakeupPorts[waveup_interrupt-&amp;gt;int_port][iBitRef]] = waveup_interrupt-&amp;gt;int_handler; // enter the user interrupt handler for this wakeup input&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; fnEnterInterrupt(irq_LL_wakeup_ID, waveup_interrupt-&amp;gt;int_priority, _wakeup_isr); // ensure that the handler is entered&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; *ptrFlagRegister = (LLWU_F_WUF0 &amp;lt;&amp;lt; (cWakeupPorts[waveup_interrupt-&amp;gt;int_port][iBitRef]%8)); // reset pending flags&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; *ptrWakeupEnable |= (ucInterruptType &amp;lt;&amp;lt; iShift); // set/enable the type required&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; else {&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; _EXCEPTION("Invalid wakeup port bit being selected!");&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ulPortBits &amp;amp;= ~ulBit;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; ulBit &amp;lt;&amp;lt;= 1;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; iBitRef++;&lt;/P&gt;
&lt;P&gt;}&lt;/P&gt;
&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For each pin enabled, the sequence (in the middle) is however:&lt;/P&gt;&lt;P&gt;1. Disable the pin's wakeup functionality (although it isn't actually function in the processor's RUN state any way)&lt;/P&gt;&lt;P&gt;2. Enter its (new) interrupt handler&lt;/P&gt;&lt;P&gt;3. Reset pending flags on the source&lt;/P&gt;&lt;P&gt;4. Set the pin mode to enable its operation&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In fact there are only about about 4 lines of code that actually do any LLWU register/interrupt configuration - the rest is more overall system design/operation on the bigger scale.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Jan 2015 19:10:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Can-anyone-share-sample-code-for-a-MQX-Lite-ISR-for-LLWU/m-p/387475#M3018</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2015-01-12T19:10:59Z</dc:date>
    </item>
    <item>
      <title>Re: Can anyone share sample code for a MQX-Lite ISR for LLWU?</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Can-anyone-share-sample-code-for-a-MQX-Lite-ISR-for-LLWU/m-p/387476#M3019</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi James,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can refer to the KL25 source code rev.10 it includes an example that demonstrates the use of the Low Power modes in the Kinetis KL25 device using Processor Expert, you will find it very useful.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In this example you can select to enter VLLS mode and wake up via LLWU.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The source code is available &lt;A href="http://www.freescale.com/files/32bit/software/KL25_SC.exe?WT_TYPE=Lab%20and%20Test%20Software&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=exe&amp;amp;WT_ASSET=Downloads&amp;amp;fileExt=.exe" title="http://www.freescale.com/files/32bit/software/KL25_SC.exe?WT_TYPE=Lab%20and%20Test%20Software&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=exe&amp;amp;WT_ASSET=Downloads&amp;amp;fileExt=.exe"&gt;HERE&lt;/A&gt; follow the path &amp;lt;install_folder&amp;gt;\kl25_sc_rev10\klxx-sc-pex\projects\PEx_low_power_demo\cw&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope this information can help you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;Adrian Sanchez Cano&lt;BR /&gt;Technical Support Engineer&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Jan 2015 22:05:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Can-anyone-share-sample-code-for-a-MQX-Lite-ISR-for-LLWU/m-p/387476#M3019</guid>
      <dc:creator>adriancano</dc:creator>
      <dc:date>2015-01-12T22:05:51Z</dc:date>
    </item>
    <item>
      <title>Re: Re: Can anyone share sample code for a MQX-Lite ISR for LLWU?</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Can-anyone-share-sample-code-for-a-MQX-Lite-ISR-for-LLWU/m-p/387477#M3020</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks! Is it available as a zip or 7z archive instead of as an exe file? I assume this is a self-extracting archive but I'm a little hesitant to download it!&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;James&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Jan 2015 00:39:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Can-anyone-share-sample-code-for-a-MQX-Lite-ISR-for-LLWU/m-p/387477#M3020</guid>
      <dc:creator>jvasil</dc:creator>
      <dc:date>2015-01-13T00:39:56Z</dc:date>
    </item>
    <item>
      <title>Re: Re: Can anyone share sample code for a MQX-Lite ISR for LLWU?</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Can-anyone-share-sample-code-for-a-MQX-Lite-ISR-for-LLWU/m-p/387478#M3021</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ahh, thanks again.&amp;nbsp; The comments on the three functions listed on the &lt;A href="http://www.utasker.com/kinetis/LLWU.html" title="http://www.utasker.com/kinetis/LLWU.html"&gt;µTasker LLWU Support&lt;/A&gt; page refer to them as "interrupt handlers" so I thought that was all that was being done!&amp;nbsp; The additional code you posted makes it much more clear.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;James&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Jan 2015 00:43:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Can-anyone-share-sample-code-for-a-MQX-Lite-ISR-for-LLWU/m-p/387478#M3021</guid>
      <dc:creator>jvasil</dc:creator>
      <dc:date>2015-01-13T00:43:19Z</dc:date>
    </item>
    <item>
      <title>Re: Can anyone share sample code for a MQX-Lite ISR for LLWU?</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Can-anyone-share-sample-code-for-a-MQX-Lite-ISR-for-LLWU/m-p/387479#M3022</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes it is a self extracting archive&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Adrian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Jan 2015 15:47:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Can-anyone-share-sample-code-for-a-MQX-Lite-ISR-for-LLWU/m-p/387479#M3022</guid>
      <dc:creator>adriancano</dc:creator>
      <dc:date>2015-01-13T15:47:34Z</dc:date>
    </item>
  </channel>
</rss>