<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Processor Expert Software中的主题 Re: SetOperationMode of various components</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/SetOperationMode-of-various-components/m-p/386369#M3005</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Dominic,&lt;/P&gt;&lt;P&gt;Basically the SetOperationMode method is implemented for CPU component and allows entering of low power modes. You can find detailed description of these operation modes in the document &lt;A href="https://community.nxp.com/docs/DOC-102163"&gt;Operation modes in Processor Expert&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Other Processor Expert LDD components also implement this function but these component usually just set the clock gate based on requested mode, e.g. ADC_LDD (DOM_RUN operation mode enable the clock gate and DOM_STOP disable the clock gate; other modes are not supported).&lt;/P&gt;&lt;P&gt;If you need additional information about a PEx component don't hesitate to contact me.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Marek Neuzil&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 05 Feb 2015 13:04:43 GMT</pubDate>
    <dc:creator>marek_neuzil</dc:creator>
    <dc:date>2015-02-05T13:04:43Z</dc:date>
    <item>
      <title>SetOperationMode of various components</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/SetOperationMode-of-various-components/m-p/386368#M3004</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As I see I can enable the functions XX_SetOperationMode of nearly all components. I don't see the meaning of this function - it seams be connectec with clock gateing somehow. Maybe I can use a different clock in dirrerent modes for the components. In the ProcessorExport guide is not written much about it:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"Each LDD component define two methods related to the low power capability – SetOperationMode() and GetDriverState(). For more details, refer to the documentation of components."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;and I dont find much more information in documentatin of the components. Does anyone know more about these functions - for example when I have to use them?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for any hint.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards, Dominic&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 05 Jan 2015 15:29:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/SetOperationMode-of-various-components/m-p/386368#M3004</guid>
      <dc:creator>astdom01</dc:creator>
      <dc:date>2015-01-05T15:29:18Z</dc:date>
    </item>
    <item>
      <title>Re: SetOperationMode of various components</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/SetOperationMode-of-various-components/m-p/386369#M3005</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Dominic,&lt;/P&gt;&lt;P&gt;Basically the SetOperationMode method is implemented for CPU component and allows entering of low power modes. You can find detailed description of these operation modes in the document &lt;A href="https://community.nxp.com/docs/DOC-102163"&gt;Operation modes in Processor Expert&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Other Processor Expert LDD components also implement this function but these component usually just set the clock gate based on requested mode, e.g. ADC_LDD (DOM_RUN operation mode enable the clock gate and DOM_STOP disable the clock gate; other modes are not supported).&lt;/P&gt;&lt;P&gt;If you need additional information about a PEx component don't hesitate to contact me.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Marek Neuzil&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Feb 2015 13:04:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/SetOperationMode-of-various-components/m-p/386369#M3005</guid>
      <dc:creator>marek_neuzil</dc:creator>
      <dc:date>2015-02-05T13:04:43Z</dc:date>
    </item>
  </channel>
</rss>