<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Processor Expert Software中的主题 Re: How to configure and enable pulldown resistor in the GPIO pins of Kinetis DSC?</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/How-to-configure-and-enable-pulldown-resistor-in-the-GPIO-pins/m-p/378348#M2930</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Cesar:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Somehow I agree with you. However it is not the same peripheral. We are talking about two different modules: PORT and GPIO. You can find a dedicated chapter for each of them in the Reference Manual.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;PORT:&lt;/STRONG&gt; Controls the particular physical pin settings (muxing, pull resistors, slew rate, drive strength, etc).&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;GPIO:&lt;/STRONG&gt; As the name indicates this module handles input/output digital states. Think of it as the logical interface with the hardware layer (PORT module).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Nonetheless, thanks for your feedback and suggestions. Unfortunately LDD components are not being updated, unless a bug is detected. This is because all development is focused on the new KSDK platform.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;PS.&lt;/STRONG&gt; About the posting spaces, you can even move a thread once you posted it. I recommend you to check the next link:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-99909"&gt;Where to post a Discussion?&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards!,&lt;BR /&gt;Jorge Gonzalez&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 05 Nov 2014 02:28:28 GMT</pubDate>
    <dc:creator>Jorge_Gonzalez</dc:creator>
    <dc:date>2014-11-05T02:28:28Z</dc:date>
    <item>
      <title>How to configure and enable pulldown resistor in the GPIO pins of Kinetis DSC?</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/How-to-configure-and-enable-pulldown-resistor-in-the-GPIO-pins/m-p/378344#M2926</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I understand Kinetis family of MCU/DSC have a Portx_PCR register for configuring and enabling pulldown or pullup resistors.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However this does not appear to be available in the configuration of the component (at least if one is interested in an individual bit I/O pin) be it in the High Level BitIO component or the logical LDD bit IO one, not even in Advanced mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there a means of achieving this via PE software or the only recourse is to write to the register in the main routine after the call to PE_low_level_init()?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;--&lt;/P&gt;&lt;P&gt;Cesar Rabak&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Nov 2014 17:46:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/How-to-configure-and-enable-pulldown-resistor-in-the-GPIO-pins/m-p/378344#M2926</guid>
      <dc:creator>cesarrabak</dc:creator>
      <dc:date>2014-11-04T17:46:51Z</dc:date>
    </item>
    <item>
      <title>Re: How to configure and enable pulldown resistor in the GPIO pins of Kinetis DSC?</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/How-to-configure-and-enable-pulldown-resistor-in-the-GPIO-pins/m-p/378345#M2927</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Cesar:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You are correct, such settings cannot be configured with &lt;STRONG&gt;BitIO&lt;/STRONG&gt; components. For this you can use the &lt;STRONG&gt;Init_GPIO&lt;/STRONG&gt; component.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;:smileyinfo: Heads-up: You may receive an error when using the same pin in both: &lt;STRONG&gt;Init_GPIO&lt;/STRONG&gt; and &lt;STRONG&gt;BitIO&lt;/STRONG&gt; components. Just right click in the pin on any of the components and select "&lt;STRONG&gt;Pin Sharing Enabled"&lt;/STRONG&gt;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A very good tutorial by Erich Styger covering this topic:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://mcuoneclipse.com/2012/11/12/tutorial-bits-and-pins-with-kinetis/" title="http://mcuoneclipse.com/2012/11/12/tutorial-bits-and-pins-with-kinetis/"&gt;http://mcuoneclipse.com/2012/11/12/tutorial-bits-and-pins-with-kinetis/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;PS.&lt;/STRONG&gt; Always post to specialized community spaces, such as &lt;A href="https://community.nxp.com/space/2022"&gt;Processor Expert Software&lt;/A&gt;.This way your questions have more visibility.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards!,&lt;BR /&gt;Jorge Gonzalez&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Nov 2014 18:07:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/How-to-configure-and-enable-pulldown-resistor-in-the-GPIO-pins/m-p/378345#M2927</guid>
      <dc:creator>Jorge_Gonzalez</dc:creator>
      <dc:date>2014-11-04T18:07:56Z</dc:date>
    </item>
    <item>
      <title>Re: How to configure and enable pulldown resistor in the GPIO pins of Kinetis DSC?</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/How-to-configure-and-enable-pulldown-resistor-in-the-GPIO-pins/m-p/378346#M2928</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for your reply Jorge!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;--&lt;/P&gt;&lt;P&gt;Cesar Rabak&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PS.: :smileyblush: I really thought this time I'd made this right on posting in the correct space, but I see I still have mileage to go on using this interface...!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Nov 2014 01:29:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/How-to-configure-and-enable-pulldown-resistor-in-the-GPIO-pins/m-p/378346#M2928</guid>
      <dc:creator>cesarrabak</dc:creator>
      <dc:date>2014-11-05T01:29:38Z</dc:date>
    </item>
    <item>
      <title>Re: How to configure and enable pulldown resistor in the GPIO pins of Kinetis DSC?</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/How-to-configure-and-enable-pulldown-resistor-in-the-GPIO-pins/m-p/378347#M2929</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;On the specifics of the link which offer a path for the solution, I've two comments:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is somewhat unintuitive that you have to configure (by two different means) the same peripheral!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The tool itself has not an easy path for finding this in the embedded documentation.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My suggestion is that these possibilities be include in the configuration of the pin itself! I think it will help with the rationale of the Processor Expert SW!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;my 0.019999....&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;--&lt;/P&gt;&lt;P&gt;Cesar Rabak&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Nov 2014 01:36:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/How-to-configure-and-enable-pulldown-resistor-in-the-GPIO-pins/m-p/378347#M2929</guid>
      <dc:creator>cesarrabak</dc:creator>
      <dc:date>2014-11-05T01:36:33Z</dc:date>
    </item>
    <item>
      <title>Re: How to configure and enable pulldown resistor in the GPIO pins of Kinetis DSC?</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/How-to-configure-and-enable-pulldown-resistor-in-the-GPIO-pins/m-p/378348#M2930</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Cesar:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Somehow I agree with you. However it is not the same peripheral. We are talking about two different modules: PORT and GPIO. You can find a dedicated chapter for each of them in the Reference Manual.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;PORT:&lt;/STRONG&gt; Controls the particular physical pin settings (muxing, pull resistors, slew rate, drive strength, etc).&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;GPIO:&lt;/STRONG&gt; As the name indicates this module handles input/output digital states. Think of it as the logical interface with the hardware layer (PORT module).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Nonetheless, thanks for your feedback and suggestions. Unfortunately LDD components are not being updated, unless a bug is detected. This is because all development is focused on the new KSDK platform.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;PS.&lt;/STRONG&gt; About the posting spaces, you can even move a thread once you posted it. I recommend you to check the next link:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-99909"&gt;Where to post a Discussion?&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards!,&lt;BR /&gt;Jorge Gonzalez&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Nov 2014 02:28:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/How-to-configure-and-enable-pulldown-resistor-in-the-GPIO-pins/m-p/378348#M2930</guid>
      <dc:creator>Jorge_Gonzalez</dc:creator>
      <dc:date>2014-11-05T02:28:28Z</dc:date>
    </item>
    <item>
      <title>Re: How to configure and enable pulldown resistor in the GPIO pins of Kinetis DSC?</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/How-to-configure-and-enable-pulldown-resistor-in-the-GPIO-pins/m-p/378349#M2931</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Jorge,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I see your points.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the link, will check it later as I get some spare timeQ&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;--&lt;/P&gt;&lt;P&gt;Cesar Rabak&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Nov 2014 13:18:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/How-to-configure-and-enable-pulldown-resistor-in-the-GPIO-pins/m-p/378349#M2931</guid>
      <dc:creator>cesarrabak</dc:creator>
      <dc:date>2014-11-05T13:18:04Z</dc:date>
    </item>
  </channel>
</rss>