<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Processor Expert Software中的主题 Error using LPTMR with PeX</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/Error-using-LPTMR-with-PeX/m-p/374014#M2875</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using KDS 2.0.0 and MQX for KSDK 1.1.0 in a Processor Expert (PeX) project using a MK64F12. I've added a low power timer to my project and when I try to generate the code I get the following error message with respect to the LPTMR component:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;No inherited component assigned (HAL1)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Looking at the Help on Component for the LPTMR component:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_0.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/49530iACD9C7C86571767E/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;It refers to HAL1 under a properties heading called InhrGrp but the InhrGrp setting does not show up in the Component Inspector for LPTMR, only in the Help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can someone help? Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 23 Jan 2015 19:29:01 GMT</pubDate>
    <dc:creator>larrykoos</dc:creator>
    <dc:date>2015-01-23T19:29:01Z</dc:date>
    <item>
      <title>Error using LPTMR with PeX</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Error-using-LPTMR-with-PeX/m-p/374014#M2875</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using KDS 2.0.0 and MQX for KSDK 1.1.0 in a Processor Expert (PeX) project using a MK64F12. I've added a low power timer to my project and when I try to generate the code I get the following error message with respect to the LPTMR component:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;No inherited component assigned (HAL1)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Looking at the Help on Component for the LPTMR component:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_0.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/49530iACD9C7C86571767E/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;It refers to HAL1 under a properties heading called InhrGrp but the InhrGrp setting does not show up in the Component Inspector for LPTMR, only in the Help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can someone help? Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 23 Jan 2015 19:29:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Error-using-LPTMR-with-PeX/m-p/374014#M2875</guid>
      <dc:creator>larrykoos</dc:creator>
      <dc:date>2015-01-23T19:29:01Z</dc:date>
    </item>
    <item>
      <title>Re: Error using LPTMR with PeX</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Error-using-LPTMR-with-PeX/m-p/374015#M2876</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Larry,&lt;/P&gt;&lt;P&gt;I had various issues with getting MQX working until I reviewed the following post:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-103429"&gt;How To: Create an MQX RTOS project with Processor Expert in Kinetis Design Studio IDE  &lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I was trying to pull in the MQX component rather than using the OSA to target using MQX.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;David &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Jan 2015 18:16:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Error-using-LPTMR-with-PeX/m-p/374015#M2876</guid>
      <dc:creator>DavidS</dc:creator>
      <dc:date>2015-01-27T18:16:22Z</dc:date>
    </item>
    <item>
      <title>Re: Error using LPTMR with PeX</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Error-using-LPTMR-with-PeX/m-p/374016#M2877</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;David,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the reply. Unfortunately, the project was created as you describe by adding the OSA component and configuring it to use MQX. There must be another issue.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Jan 2015 18:36:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Error-using-LPTMR-with-PeX/m-p/374016#M2877</guid>
      <dc:creator>larrykoos</dc:creator>
      <dc:date>2015-01-27T18:36:25Z</dc:date>
    </item>
    <item>
      <title>Re: Error using LPTMR with PeX</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Error-using-LPTMR-with-PeX/m-p/374017#M2878</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Larry,&lt;/P&gt;&lt;P&gt;Can you retry the process and post the project?&lt;/P&gt;&lt;P&gt;What Host OS are you using?&lt;/P&gt;&lt;P&gt;Do any of the demo or MQX examples in KSDK1.1.0 work for you?&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;David &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Jan 2015 20:47:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Error-using-LPTMR-with-PeX/m-p/374017#M2878</guid>
      <dc:creator>DavidS</dc:creator>
      <dc:date>2015-01-27T20:47:28Z</dc:date>
    </item>
    <item>
      <title>Re: Error using LPTMR with PeX</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Error-using-LPTMR-with-PeX/m-p/374018#M2879</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;David,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have loaded MQX examples, built them and run them on a MK6412 tower eval board. Of course, the examples do not use Processor Expert while the problem I'm having is related to the LPTMR PeX component.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm developing on a Windows 7 machine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm not sure what you mean by "post the project". A screenshot, a zipfile of the project, something else?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 01 Feb 2015 22:16:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Error-using-LPTMR-with-PeX/m-p/374018#M2879</guid>
      <dc:creator>larrykoos</dc:creator>
      <dc:date>2015-02-01T22:16:16Z</dc:date>
    </item>
    <item>
      <title>Re: Re: Error using LPTMR with PeX</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Error-using-LPTMR-with-PeX/m-p/374019#M2880</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Larry,&lt;/P&gt;&lt;P&gt;I cannot get the error you are. &lt;/P&gt;&lt;P&gt;I have started with a new project for frdm-k64f + KSDK + PE and set the OS to be MQX (not MQXLite).&lt;/P&gt;&lt;P&gt;I then added in fsl_lptmr_hal component.&lt;/P&gt;&lt;P&gt;I did have to enable the clock to LPTMR module and then configure the fsl_lptmr.&lt;/P&gt;&lt;P&gt;My project is attached.&lt;/P&gt;&lt;P&gt;You should be able to unZIP into C:\Freescale\KSDK_1.1.0\.&lt;/P&gt;&lt;P&gt;Then import it.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;David&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Feb 2015 18:29:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Error-using-LPTMR-with-PeX/m-p/374019#M2880</guid>
      <dc:creator>DavidS</dc:creator>
      <dc:date>2015-02-02T18:29:10Z</dc:date>
    </item>
  </channel>
</rss>