<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Processor Expert SoftwareのトピックRe: IIC Slave Address</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/IIC-Slave-Address/m-p/372425#M2864</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello overdamped:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you share your code?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To avoid K60 sending the I2C slave address again, you have to use a unique call to the &lt;STRONG&gt;MasterSendBlock()&lt;/STRONG&gt; method, considering that the total size of the block includes in this case the sensor's "Register Address" and all the "Bytes to Write".&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards!,&lt;BR /&gt;Jorge Gonzalez&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 23 Dec 2014 23:04:41 GMT</pubDate>
    <dc:creator>Jorge_Gonzalez</dc:creator>
    <dc:date>2014-12-23T23:04:41Z</dc:date>
    <item>
      <title>IIC Slave Address</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/IIC-Slave-Address/m-p/372424#M2863</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm trying to interface with a freescale sensor as per &lt;A href="http://cache.freescale.com/files/sensors/doc/app_note/AN4481.pdf"&gt;AN4481&lt;/A&gt;, but it seems under processor expert for the k60 that a multi-byte write that i2c always transmits the slave address before each byte (the 3rd and 4th starts in the photo are the multibyte write). Is there any way to avoid this other than bitbanging spi or is the IIC k60 peripheral designed to perform this way?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="i2c_pex_MultibyteWrite.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/48725i7AEC5FA8BE1FB1EE/image-size/large?v=v2&amp;amp;px=999" role="button" title="i2c_pex_MultibyteWrite.jpg" alt="i2c_pex_MultibyteWrite.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Dec 2014 19:58:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/IIC-Slave-Address/m-p/372424#M2863</guid>
      <dc:creator>overdamped</dc:creator>
      <dc:date>2014-12-23T19:58:58Z</dc:date>
    </item>
    <item>
      <title>Re: IIC Slave Address</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/IIC-Slave-Address/m-p/372425#M2864</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello overdamped:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you share your code?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To avoid K60 sending the I2C slave address again, you have to use a unique call to the &lt;STRONG&gt;MasterSendBlock()&lt;/STRONG&gt; method, considering that the total size of the block includes in this case the sensor's "Register Address" and all the "Bytes to Write".&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards!,&lt;BR /&gt;Jorge Gonzalez&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Dec 2014 23:04:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/IIC-Slave-Address/m-p/372425#M2864</guid>
      <dc:creator>Jorge_Gonzalez</dc:creator>
      <dc:date>2014-12-23T23:04:41Z</dc:date>
    </item>
    <item>
      <title>Re: IIC Slave Address</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/IIC-Slave-Address/m-p/372426#M2865</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Correct you are. Figured out my size parameter to the _MasterSendBlock function was incorrect. Thanks for the tip in the right direction.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 29 Dec 2014 15:02:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/IIC-Slave-Address/m-p/372426#M2865</guid>
      <dc:creator>overdamped</dc:creator>
      <dc:date>2014-12-29T15:02:29Z</dc:date>
    </item>
  </channel>
</rss>