<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Get source of reset in Processor Expert Software</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/Get-source-of-reset/m-p/364896#M2802</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;The CPU_GetResetSource() method is not supported on Kinetis but you can use Cpu_OnReset(uint16_t Reason) event where the reset reason is provided as a parameter (value of RCM_SRS1 and RCM_SRS0 registers) or you can use PDD macros of RCM module, see below:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="RCM_ReadSystemStatus.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/50297iF2165BE9E12F753A/image-size/large?v=v2&amp;amp;px=999" role="button" title="RCM_ReadSystemStatus.png" alt="RCM_ReadSystemStatus.png" /&gt;&lt;/span&gt;&lt;BR /&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Marek Neuzil&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 06 Feb 2015 10:55:33 GMT</pubDate>
    <dc:creator>marek_neuzil</dc:creator>
    <dc:date>2015-02-06T10:55:33Z</dc:date>
    <item>
      <title>Get source of reset</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Get-source-of-reset/m-p/364895#M2801</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;When I'm using ProcessorExpert on my HC12 targets I use Cpu_GetResetSource() to get the source of my current startup.&lt;/P&gt;&lt;P&gt;Is there any similar function for Kinetis?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Jan 2015 16:10:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Get-source-of-reset/m-p/364895#M2801</guid>
      <dc:creator>oaf</dc:creator>
      <dc:date>2015-01-21T16:10:43Z</dc:date>
    </item>
    <item>
      <title>Re: Get source of reset</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Get-source-of-reset/m-p/364896#M2802</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;The CPU_GetResetSource() method is not supported on Kinetis but you can use Cpu_OnReset(uint16_t Reason) event where the reset reason is provided as a parameter (value of RCM_SRS1 and RCM_SRS0 registers) or you can use PDD macros of RCM module, see below:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="RCM_ReadSystemStatus.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/50297iF2165BE9E12F753A/image-size/large?v=v2&amp;amp;px=999" role="button" title="RCM_ReadSystemStatus.png" alt="RCM_ReadSystemStatus.png" /&gt;&lt;/span&gt;&lt;BR /&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Marek Neuzil&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 Feb 2015 10:55:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Get-source-of-reset/m-p/364896#M2802</guid>
      <dc:creator>marek_neuzil</dc:creator>
      <dc:date>2015-02-06T10:55:33Z</dc:date>
    </item>
    <item>
      <title>Re: Get source of reset</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Get-source-of-reset/m-p/364897#M2803</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I was looking for the file RCM but I couldn't find it. I am using a M60DN512VLQ10&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Aug 2016 17:08:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Get-source-of-reset/m-p/364897#M2803</guid>
      <dc:creator>norbertoj</dc:creator>
      <dc:date>2016-08-19T17:08:27Z</dc:date>
    </item>
  </channel>
</rss>