<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Processor Expert not working. in Processor Expert Software</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/Processor-Expert-not-working/m-p/357518#M2730</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Alice,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using the TWR-K24F120M Evaluation board. The uC in the Board is MK24FN256VDC12 (121 MBGA).&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 10 Feb 2015 04:06:13 GMT</pubDate>
    <dc:creator>rafaelzambrano</dc:creator>
    <dc:date>2015-02-10T04:06:13Z</dc:date>
    <item>
      <title>Processor Expert not working.</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Processor-Expert-not-working/m-p/357513#M2725</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to add a component (BITIO) to my project. I get the following error "This component is not supported in Kinetis SDK project mode"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What d I need to set up in the tools or import so I can use those components?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Rafael-&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Feb 2015 00:16:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Processor-Expert-not-working/m-p/357513#M2725</guid>
      <dc:creator>rafaelzambrano</dc:creator>
      <dc:date>2015-02-09T00:16:09Z</dc:date>
    </item>
    <item>
      <title>Re: Processor Expert not working.</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Processor-Expert-not-working/m-p/357514#M2726</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Rafael.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please tell me which chip do you use ? and the SDK version ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Alice&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Feb 2015 01:29:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Processor-Expert-not-working/m-p/357514#M2726</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2015-02-09T01:29:43Z</dc:date>
    </item>
    <item>
      <title>Re: Processor Expert not working.</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Processor-Expert-not-working/m-p/357515#M2727</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It looks like you have created a project with the Kinetis SDK option. In that case, you cannot use any of the LDD (Logical Device Driver) components, only the fsl_* components will work, except you are using some of the McuOnEclipse components (which work both for SDK and non-SDK projects).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Feb 2015 07:24:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Processor-Expert-not-working/m-p/357515#M2727</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2015-02-09T07:24:10Z</dc:date>
    </item>
    <item>
      <title>Re: Processor Expert not working.</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Processor-Expert-not-working/m-p/357516#M2728</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Erich, Thank you for your answer. What would be the correct procedure to create the project and be able to use the LDD components. When I try to use the fsl components the system seems to accept them but I cannot get then to work properly. ie, I always get an error after I built the code. " function has not enough arguments" I thought with processor expert once you configured the component, you do not need to do anything else in the code when you are using the method. I am just trying to do a simple LED on and OFF and read the input value of a GPIO.&lt;/P&gt;&lt;P&gt;I looked at examples in Youtube but none of them use the fsl components. Any idea where can I go and look for some help in this matter.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Feb 2015 16:28:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Processor-Expert-not-working/m-p/357516#M2728</guid>
      <dc:creator>rafaelzambrano</dc:creator>
      <dc:date>2015-02-09T16:28:30Z</dc:date>
    </item>
    <item>
      <title>Re: Processor Expert not working.</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Processor-Expert-not-working/m-p/357517#M2729</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Rafael,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please install the SDK to&amp;nbsp; your IDE .&lt;/P&gt;&lt;P&gt;For example , if use KDS,&amp;nbsp; please refer to here :&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-101862"&gt;Writing your first toggle LED application with FRMD-K64F + KDS 1.1.0 + KSDK 1.0.0 Non-Processor Expert    &lt;/A&gt;&lt;/P&gt;&lt;P&gt;(install sdk to kds )&lt;/P&gt;&lt;P&gt;&lt;A href="http://mcuoneclipse.com/2014/11/08/tutorial-freertos-with-the-kinetis-sdk-and-processor-expert/" title="http://mcuoneclipse.com/2014/11/08/tutorial-freertos-with-the-kinetis-sdk-and-processor-expert/"&gt;Tutorial: FreeRTOS with the Kinetis SDK and Processor Expert | MCU on Eclipse&lt;/A&gt;&amp;nbsp;&amp;nbsp; （create PE project on sdk）&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can also refer to the "Getting Stared with Kinetis SDK.pdf"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Feb 2015 02:48:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Processor-Expert-not-working/m-p/357517#M2729</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2015-02-10T02:48:08Z</dc:date>
    </item>
    <item>
      <title>Re: Processor Expert not working.</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Processor-Expert-not-working/m-p/357518#M2730</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Alice,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using the TWR-K24F120M Evaluation board. The uC in the Board is MK24FN256VDC12 (121 MBGA).&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Feb 2015 04:06:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Processor-Expert-not-working/m-p/357518#M2730</guid>
      <dc:creator>rafaelzambrano</dc:creator>
      <dc:date>2015-02-10T04:06:13Z</dc:date>
    </item>
    <item>
      <title>Re: Processor Expert not working.</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Processor-Expert-not-working/m-p/357519#M2731</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Rafael,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes , use the KSDK PE , the method TWR-K24 is the same with FRDM-K64 ().&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Feb 2015 09:38:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Processor-Expert-not-working/m-p/357519#M2731</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2015-02-10T09:38:45Z</dc:date>
    </item>
  </channel>
</rss>