<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: FTM Output Trigger using Processor Expert in Processor Expert Software</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/FTM-Output-Trigger-using-Processor-Expert/m-p/357220#M2721</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Processor expert often does not give you complete control.&amp;nbsp; Its a great tool to use as a starting point to get stuff kinda working.&amp;nbsp; Then you can look at what it does to write the real driver.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 20 Nov 2014 22:34:31 GMT</pubDate>
    <dc:creator>robotjosh</dc:creator>
    <dc:date>2014-11-20T22:34:31Z</dc:date>
    <item>
      <title>FTM Output Trigger using Processor Expert</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/FTM-Output-Trigger-using-Processor-Expert/m-p/357219#M2720</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using the MK21FN1M0 and I want to trigger the PDB from FTM output. Unfortunately I can't enable the trigger output on the TimerUnit in Processor Expert. Do you have any suggestions?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_0.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/47398iDF74878184C3063B/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/47399i1982A1C7145C0A2E/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Nov 2014 15:50:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/FTM-Output-Trigger-using-Processor-Expert/m-p/357219#M2720</guid>
      <dc:creator>philipp_laemmle</dc:creator>
      <dc:date>2014-11-20T15:50:25Z</dc:date>
    </item>
    <item>
      <title>Re: FTM Output Trigger using Processor Expert</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/FTM-Output-Trigger-using-Processor-Expert/m-p/357220#M2721</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Processor expert often does not give you complete control.&amp;nbsp; Its a great tool to use as a starting point to get stuff kinda working.&amp;nbsp; Then you can look at what it does to write the real driver.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Nov 2014 22:34:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/FTM-Output-Trigger-using-Processor-Expert/m-p/357220#M2721</guid>
      <dc:creator>robotjosh</dc:creator>
      <dc:date>2014-11-20T22:34:31Z</dc:date>
    </item>
    <item>
      <title>Re: FTM Output Trigger using Processor Expert</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/FTM-Output-Trigger-using-Processor-Expert/m-p/357221#M2722</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Philipp,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I look at your PDB clock have not enable .&lt;/P&gt;&lt;P&gt;&lt;IMG alt="" class="jiveImage" src="https://community.nxp.com/" style="max-width: 1200px; max-height: 900px;" /&gt;&lt;/P&gt;&lt;P&gt;And Why FTM cant trigger PDB,&amp;nbsp; this is not only depend on your processor expert configuration , but also your code.&lt;/P&gt;&lt;P&gt;Please attach your code , or say in detailed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards!&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 22 Nov 2014 08:14:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/FTM-Output-Trigger-using-Processor-Expert/m-p/357221#M2722</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2014-11-22T08:14:20Z</dc:date>
    </item>
    <item>
      <title>Re: FTM Output Trigger using Processor Expert</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/FTM-Output-Trigger-using-Processor-Expert/m-p/357222#M2723</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Hello Philipp,&lt;/P&gt;&lt;P&gt;You are right that TimerUnit_LDD does not provide properties to configure the external trigger (FTM_EXTTRIG register) that are used by PDB device. You can used TimerUnit_LDD and configure the FTM_EXTTRIG register by the &lt;EM&gt;FTM_PDD_WriteExternalTriggerReg(PeripheralBase, Value)&lt;/EM&gt; PDD macro. Or you can use Init_FTM component that cover all register of the FTM (there are version specific registers; use the Advance view in the Component Inspector), see the following screenshot:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="Init_FTM_ExternalTriggers.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/47578iCEA907B6A70DABDF/image-size/large?v=v2&amp;amp;px=999" role="button" title="Init_FTM_ExternalTriggers.png" alt="Init_FTM_ExternalTriggers.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Marek Neuzil&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Nov 2014 15:00:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/FTM-Output-Trigger-using-Processor-Expert/m-p/357222#M2723</guid>
      <dc:creator>marek_neuzil</dc:creator>
      <dc:date>2014-11-25T15:00:07Z</dc:date>
    </item>
    <item>
      <title>Re: FTM Output Trigger using Processor Expert</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/FTM-Output-Trigger-using-Processor-Expert/m-p/357223#M2724</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Marek&lt;/P&gt;&lt;P&gt;Thanks for your help.&lt;/P&gt;&lt;P&gt;In case of using the peripheral init module, I have to implement the methods for the timer by myself. Is this right?&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Philipp&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Jan 2015 09:54:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/FTM-Output-Trigger-using-Processor-Expert/m-p/357223#M2724</guid>
      <dc:creator>philipp_laemmle</dc:creator>
      <dc:date>2015-01-06T09:54:00Z</dc:date>
    </item>
  </channel>
</rss>