<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Logical Device Driver vs High Level Component in Processor Expert Software</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/Logical-Device-Driver-vs-High-Level-Component/m-p/351698#M2682</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Jorge&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 16 Jan 2015 17:29:08 GMT</pubDate>
    <dc:creator>pratiekbhadrana</dc:creator>
    <dc:date>2015-01-16T17:29:08Z</dc:date>
    <item>
      <title>Logical Device Driver vs High Level Component</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Logical-Device-Driver-vs-High-Level-Component/m-p/351694#M2678</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What is the difference between an LDD and a High Level component (let's call this an HLC) ? If I am right, an LDD allows integration into an RTOS, but can also be used in a bareboard application. Whereas an HLC can only be used bareboard. To build a sort of tree showing each component as a subset of a bigger component, I'd say ((( Peripheral Initialization component - most basic, only init() calls) LDD) HLC). Is this correct?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What are the additional features of an HLC over an LDD?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, to use an LDD bareboard, is it necessary to include bareboard OS component in the project?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Jan 2015 12:18:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Logical-Device-Driver-vs-High-Level-Component/m-p/351694#M2678</guid>
      <dc:creator>pratiekbhadrana</dc:creator>
      <dc:date>2015-01-16T12:18:43Z</dc:date>
    </item>
    <item>
      <title>Re: Logical Device Driver vs High Level Component</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Logical-Device-Driver-vs-High-Level-Component/m-p/351695#M2679</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Pratiek:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;That is a common question and your understanding is correct. Check the next threads:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/413322"&gt;Re: n00b question - What's the difference between a low-levevel device driver and a high-level component, exactly?&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/319174"&gt;difference between ExtInt and ExtInt_LDD&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you want to go without an OS then just add the LDD components to a bareboard project and the code will disregard any RTOS related stuff such as the handlers.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards!,&lt;BR /&gt;Jorge Gonzalez&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Jan 2015 14:17:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Logical-Device-Driver-vs-High-Level-Component/m-p/351695#M2679</guid>
      <dc:creator>Jorge_Gonzalez</dc:creator>
      <dc:date>2015-01-16T14:17:53Z</dc:date>
    </item>
    <item>
      <title>Re: Logical Device Driver vs High Level Component</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Logical-Device-Driver-vs-High-Level-Component/m-p/351696#M2680</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Jorge. I searched for logical device driver before asking, but these options didn't show up. Regarding bareboard OS component, I've attached a snapshot. I am running KDS 2.0.0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="bareboad.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/49028iE6C7023D57D61CFA/image-size/large?v=v2&amp;amp;px=999" role="button" title="bareboad.jpg" alt="bareboad.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Jan 2015 16:53:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Logical-Device-Driver-vs-High-Level-Component/m-p/351696#M2680</guid>
      <dc:creator>pratiekbhadrana</dc:creator>
      <dc:date>2015-01-16T16:53:10Z</dc:date>
    </item>
    <item>
      <title>Re: Logical Device Driver vs High Level Component</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Logical-Device-Driver-vs-High-Level-Component/m-p/351697#M2681</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Pratiek:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sorry, I did not recall that component exists. According to the description (right click on the component -&amp;gt; Help on component -&amp;gt; Component Bareboard) this is to ease migration from Bareboard to RTOS in the future:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="Bareboard_component.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/47574i675AB4B3AB499500/image-size/large?v=v2&amp;amp;px=999" role="button" title="Bareboard_component.png" alt="Bareboard_component.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Personally I have never used that component and if you do not plan to add an RTOS then you don't have to use it either, just use the LDD beans alone.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards!,&lt;BR /&gt;Jorge Gonzalez&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Jan 2015 17:21:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Logical-Device-Driver-vs-High-Level-Component/m-p/351697#M2681</guid>
      <dc:creator>Jorge_Gonzalez</dc:creator>
      <dc:date>2015-01-16T17:21:29Z</dc:date>
    </item>
    <item>
      <title>Re: Logical Device Driver vs High Level Component</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Logical-Device-Driver-vs-High-Level-Component/m-p/351698#M2682</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Jorge&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Jan 2015 17:29:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Logical-Device-Driver-vs-High-Level-Component/m-p/351698#M2682</guid>
      <dc:creator>pratiekbhadrana</dc:creator>
      <dc:date>2015-01-16T17:29:08Z</dc:date>
    </item>
  </channel>
</rss>