<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Processor Expert SoftwareのトピックWhy are values in the configuration register window read only?</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/Why-are-values-in-the-configuration-register-window-read-only/m-p/349942#M2659</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am new to codewarrior, so I'm still getting familiar with everything.&amp;nbsp; My microcontroller is a Kinetis K20.&amp;nbsp; I want to set up UART1 to drive an infrared trasceiver.&amp;nbsp; I dont see any settings in the component inspector, but I did find the UART1_IR register under the configuration registers window.&amp;nbsp; I see the bits that I need to change, but they are all read only.&amp;nbsp; Why is this?&amp;nbsp; How can I edit these values?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 11 Aug 2014 10:56:22 GMT</pubDate>
    <dc:creator>kreu</dc:creator>
    <dc:date>2014-08-11T10:56:22Z</dc:date>
    <item>
      <title>Why are values in the configuration register window read only?</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Why-are-values-in-the-configuration-register-window-read-only/m-p/349942#M2659</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am new to codewarrior, so I'm still getting familiar with everything.&amp;nbsp; My microcontroller is a Kinetis K20.&amp;nbsp; I want to set up UART1 to drive an infrared trasceiver.&amp;nbsp; I dont see any settings in the component inspector, but I did find the UART1_IR register under the configuration registers window.&amp;nbsp; I see the bits that I need to change, but they are all read only.&amp;nbsp; Why is this?&amp;nbsp; How can I edit these values?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Aug 2014 10:56:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Why-are-values-in-the-configuration-register-window-read-only/m-p/349942#M2659</guid>
      <dc:creator>kreu</dc:creator>
      <dc:date>2014-08-11T10:56:22Z</dc:date>
    </item>
    <item>
      <title>Re: Why are values in the configuration register window read only?</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Why-are-values-in-the-configuration-register-window-read-only/m-p/349943#M2660</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Configuration register window is used for showing value of register but it can also be used for modification of register values. If you want to use Processor Expert effectivelly start by using&amp;nbsp; PEx components. There si Component Library windows (click in the &lt;EM&gt;Processor Expert&lt;/EM&gt; main menu on &lt;EM&gt;Show Views&lt;/EM&gt;) that allow you to select proper components for your application design. You can use the &lt;EM&gt;Categories&lt;/EM&gt;, &lt;EM&gt;Alphabetical&lt;/EM&gt; or &lt;EM&gt;Assistant &lt;/EM&gt;page in the &lt;EM&gt;Component Library&lt;/EM&gt; window.&lt;/P&gt;&lt;P&gt;When you add a component (e.g. Init_UART) into your project you can also modify values of registers and the Init_UART component is set accordingly (but you must not modify value of read-only bits - it is not allowed). When you modify a value of property the affected registers are marked by yellow. When you modify a value of a register the affected properties are marked by yellow too.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="CW MCU 10.5 Init_UART Configuration Registers windows.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/45307i48CF62A5371D2615/image-size/large?v=v2&amp;amp;px=999" role="button" title="CW MCU 10.5 Init_UART Configuration Registers windows.png" alt="CW MCU 10.5 Init_UART Configuration Registers windows.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Aug 2014 12:47:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Why-are-values-in-the-configuration-register-window-read-only/m-p/349943#M2660</guid>
      <dc:creator>marek_neuzil</dc:creator>
      <dc:date>2014-08-19T12:47:27Z</dc:date>
    </item>
  </channel>
</rss>