<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Processor Expert SoftwareのトピックRe: How to add an SPI component ?</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/How-to-add-an-SPI-component/m-p/348116#M2639</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Well, I finally worked it out. For some reason I do not know I had multiple clock configurations (4 of them) and it turns out the "Timing dialog window" can't deal with that.&lt;/P&gt;&lt;P&gt;Reducing the clock configurations to 1 cures it completely.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the mean time I have included the fsl_cmp, fsl_i2c, fsl_spi and fsl_lpuart components.&lt;/P&gt;&lt;P&gt;The last three all showed the same problem until the number of clock configurations was reduced to 1.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can now generate the processor expert code, build the application etc....&lt;/P&gt;&lt;P&gt;Problem solved but it took the best part of today and a fair dose of irritation and headache.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 25 Mar 2015 15:04:31 GMT</pubDate>
    <dc:creator>filipdossche</dc:creator>
    <dc:date>2015-03-25T15:04:31Z</dc:date>
    <item>
      <title>How to add an SPI component ?</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/How-to-add-an-SPI-component/m-p/348115#M2638</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying to add an SPI component using processor expert.&lt;/P&gt;&lt;P&gt;I can't do it because it reports an error when I try to generate the code.&lt;/P&gt;&lt;P&gt;Using the Component Inspector I see where the error is&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/49838iE350AFBA312052A6/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Logically I try to correct it using the Timing dialog box:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/49887iE5F84E4EC5E593FB/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;By selecting a clock configuration I get a list of possible settings but whichever I choose it keeps saying there is an error.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Obviously I am doing something wrong or I am missing something.&lt;/P&gt;&lt;P&gt;Can anyone tell me what that might be ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;No joy yet, I have been at this all morning and I Have noticed the following extra things:&lt;/P&gt;&lt;P&gt;- The timing dialog box does not show any possible values when the selected clock configuration is "ALL".&lt;/P&gt;&lt;P&gt;- If I select a value in any one of the single Clock configurations I always get a "Timing setting failed in Clock configuration x" message for another clock configuration.&lt;/P&gt;&lt;P&gt;- If there are no applicable common values that would be logical but how do you set it up so there are&lt;/P&gt;&lt;P&gt;- I can click on "clock path" and it shows the path for "Clock configuration 0". I can't select another one or make changes to it.&lt;/P&gt;&lt;P&gt;- Advanced stays greyed out.&lt;/P&gt;&lt;P&gt;- I have messed around with activating clock configurations 0...3 in the CPU but no difference whatsoever.&lt;/P&gt;&lt;P&gt;- How do you specify to use a particular clock configuration ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Message was edited by: Filip Dossche&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Mar 2015 09:19:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/How-to-add-an-SPI-component/m-p/348115#M2638</guid>
      <dc:creator>filipdossche</dc:creator>
      <dc:date>2015-03-25T09:19:01Z</dc:date>
    </item>
    <item>
      <title>Re: How to add an SPI component ?</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/How-to-add-an-SPI-component/m-p/348116#M2639</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Well, I finally worked it out. For some reason I do not know I had multiple clock configurations (4 of them) and it turns out the "Timing dialog window" can't deal with that.&lt;/P&gt;&lt;P&gt;Reducing the clock configurations to 1 cures it completely.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the mean time I have included the fsl_cmp, fsl_i2c, fsl_spi and fsl_lpuart components.&lt;/P&gt;&lt;P&gt;The last three all showed the same problem until the number of clock configurations was reduced to 1.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can now generate the processor expert code, build the application etc....&lt;/P&gt;&lt;P&gt;Problem solved but it took the best part of today and a fair dose of irritation and headache.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Mar 2015 15:04:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/How-to-add-an-SPI-component/m-p/348116#M2639</guid>
      <dc:creator>filipdossche</dc:creator>
      <dc:date>2015-03-25T15:04:31Z</dc:date>
    </item>
  </channel>
</rss>