<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: SPIMaster_LDD Slave Select Always Enabled in Processor Expert Software</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/SPIMaster-LDD-Slave-Select-Always-Enabled/m-p/342038#M2609</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;the SS pin toggling depend on the settings of CPHA bit (see the functional description of the SPI in the KL25P80M48SF0RM reference manual). When the CPHA bit is set to 0 the Chip select toggling is enabled and the SPI slave select work according to your requirement. You can see the settings of SPIMaster_LDD component on the following screenshot and the result (signals) on digital osciloscope snapshot (first channel - Chip select pin, second channel clock pin).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/50482i8FC4C9D8F6007FC9/image-size/large?v=v2&amp;amp;px=999" title="SPIMaster settings.png" alt="SPIMaster settings.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/50483i6BA805571B7CA72B/image-size/large?v=v2&amp;amp;px=999" title="F0000TEK.BMP.bmp" alt="F0000TEK.BMP.bmp" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I have also attached the application that I have created in CW MCU 10.6.3.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Marek Neuzil&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 13 Feb 2015 09:36:30 GMT</pubDate>
    <dc:creator>marek_neuzil</dc:creator>
    <dc:date>2015-02-13T09:36:30Z</dc:date>
    <item>
      <title>SPIMaster_LDD Slave Select Always Enabled</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/SPIMaster-LDD-Slave-Select-Always-Enabled/m-p/342034#M2605</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, I have the SynchroMaster component using the SPIMaster_LDD configured in my project with the Slave Select enabled for the component.&amp;nbsp; I do see SPI data being transmitted when I send data using SyncCAN_SendBlock().&amp;nbsp; The problem is, the Slave Select line is always low (enabled state)- even when I am not transmitting data.&amp;nbsp; Do I have to enable/disable this pin on my own even though I have set the SPIMaster component to take control of it?&amp;nbsp; If so, how do I toggle this bit?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I running this through CodeWarrior on the FRDM-KL25Z board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for any help.&lt;/P&gt;&lt;P&gt;Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Feb 2015 20:58:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/SPIMaster-LDD-Slave-Select-Always-Enabled/m-p/342034#M2605</guid>
      <dc:creator>ttahut</dc:creator>
      <dc:date>2015-02-02T20:58:10Z</dc:date>
    </item>
    <item>
      <title>Re: SPIMaster_LDD Slave Select Always Enabled</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/SPIMaster-LDD-Slave-Select-Always-Enabled/m-p/342035#M2606</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tom,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The simple method&amp;nbsp; is configuration the "select pin " as GPIO, when transmit data, configuration it to low ,when not to transmit , high.&lt;/P&gt;&lt;P&gt;Use&amp;nbsp; the "BitIO" component,&amp;nbsp; use the "ClrVal" and "SetVal" set the pin to 0 and 1 .&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/50142iE739FD459C4D2106/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Alice&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Feb 2015 02:52:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/SPIMaster-LDD-Slave-Select-Always-Enabled/m-p/342035#M2606</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2015-02-03T02:52:45Z</dc:date>
    </item>
    <item>
      <title>Re: SPIMaster_LDD Slave Select Always Enabled</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/SPIMaster-LDD-Slave-Select-Always-Enabled/m-p/342036#M2607</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Alice- Yes that works.&amp;nbsp; But I guess I don't understand the reason the Slave Select setting is in the component if I have to toggle it on my own anyways.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In fact I got rid of the SynchroMaster because it is too slow and went straight to the SPIMaster_LDD component.&amp;nbsp; The Slave Select is in &lt;SPAN style="font-size: 13.3333330154419px;"&gt;SPIMaster_LDD &lt;/SPAN&gt;as well but the BitIO works as you would expect.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Feb 2015 18:53:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/SPIMaster-LDD-Slave-Select-Always-Enabled/m-p/342036#M2607</guid>
      <dc:creator>ttahut</dc:creator>
      <dc:date>2015-02-04T18:53:10Z</dc:date>
    </item>
    <item>
      <title>Re: SPIMaster_LDD Slave Select Always Enabled</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/SPIMaster-LDD-Slave-Select-Always-Enabled/m-p/342037#M2608</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tom,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;About the "chip select toggling " on KL2x family , there is a bug , so I recommend you configuration the pin to GPIO.&lt;/P&gt;&lt;P&gt;The detail introduce you can refer to here :&amp;nbsp;&amp;nbsp; &lt;A href="https://community.nxp.com/message/461566"&gt;SPI Chip select toggles between bytes&lt;/A&gt; , please see the talking of&amp;nbsp;&amp;nbsp; &lt;A href="https://community.nxp.com/people/xiangjun.rong"&gt;xiangjun.rong&lt;/A&gt;&amp;nbsp; .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Feb 2015 02:31:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/SPIMaster-LDD-Slave-Select-Always-Enabled/m-p/342037#M2608</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2015-02-05T02:31:27Z</dc:date>
    </item>
    <item>
      <title>Re: SPIMaster_LDD Slave Select Always Enabled</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/SPIMaster-LDD-Slave-Select-Always-Enabled/m-p/342038#M2609</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;the SS pin toggling depend on the settings of CPHA bit (see the functional description of the SPI in the KL25P80M48SF0RM reference manual). When the CPHA bit is set to 0 the Chip select toggling is enabled and the SPI slave select work according to your requirement. You can see the settings of SPIMaster_LDD component on the following screenshot and the result (signals) on digital osciloscope snapshot (first channel - Chip select pin, second channel clock pin).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/50482i8FC4C9D8F6007FC9/image-size/large?v=v2&amp;amp;px=999" title="SPIMaster settings.png" alt="SPIMaster settings.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/50483i6BA805571B7CA72B/image-size/large?v=v2&amp;amp;px=999" title="F0000TEK.BMP.bmp" alt="F0000TEK.BMP.bmp" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I have also attached the application that I have created in CW MCU 10.6.3.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Marek Neuzil&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Feb 2015 09:36:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/SPIMaster-LDD-Slave-Select-Always-Enabled/m-p/342038#M2609</guid>
      <dc:creator>marek_neuzil</dc:creator>
      <dc:date>2015-02-13T09:36:30Z</dc:date>
    </item>
  </channel>
</rss>