<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Processor Expert SoftwareのトピックRe: Timer interrupt LDD Component - set period at runtime?</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/Timer-interrupt-LDD-Component-set-period-at-runtime/m-p/324676#M2455</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I ended up using the PPG: Programmable Pulse Generator and it works very well.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 28 Apr 2015 00:12:26 GMT</pubDate>
    <dc:creator>daveboyle</dc:creator>
    <dc:date>2015-04-28T00:12:26Z</dc:date>
    <item>
      <title>Timer interrupt LDD Component - set period at runtime?</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Timer-interrupt-LDD-Component-set-period-at-runtime/m-p/324672#M2451</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using the Periodic timer interrupt LDD component in PE on a Kinetis K20. I'm trying to turn on the "SetPeriodUS", "SetFrequencyHz", etc. methods, but they are greyed out, saying that I need to go to "Runtime setting type" and set it to "from interval". When I go to properties-&amp;gt;Interrupt period-&amp;gt;Runtime setting type and the only option is "fixed value". How can I enable the methods I want?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Many thanks,&lt;/P&gt;&lt;P&gt;Chris&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Jul 2014 19:04:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Timer-interrupt-LDD-Component-set-period-at-runtime/m-p/324672#M2451</guid>
      <dc:creator>thatonesaxkid</dc:creator>
      <dc:date>2014-07-24T19:04:48Z</dc:date>
    </item>
    <item>
      <title>Re: Timer interrupt LDD Component - set period at runtime?</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Timer-interrupt-LDD-Component-set-period-at-runtime/m-p/324673#M2452</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It seems to me that this is not implemented. I ususally use the TimerInt component (which inherits from the TimerInt_LLD. But if I enable 'from list of values' in the TimerInt component, then it says that this is not supported in the underlying component.&lt;/P&gt;&lt;P&gt;What you could do is to change the timer modulo register directly from your application.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 Jul 2014 05:43:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Timer-interrupt-LDD-Component-set-period-at-runtime/m-p/324673#M2452</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2014-07-25T05:43:16Z</dc:date>
    </item>
    <item>
      <title>Re: Timer interrupt LDD Component - set period at runtime?</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Timer-interrupt-LDD-Component-set-period-at-runtime/m-p/324674#M2453</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;unfortunatelly, the Timerint component on component doesn't provide these function for runtime time change on Kinetis (it's mentioned in the general info page of the component help).&lt;/P&gt;&lt;P&gt;What you can do is to use TimerUnit_LDD instead, which has functions for changing the period - &lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;SetPeriodTicks (you need to switch to Advanced view mode to see all methods).&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;See also &lt;A href="https://community.nxp.com/message/371057"&gt;Re: How to change a period at runtime&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;The SetPeriodTicks sets the period in ticks of the timer. If you need compute time from real time unit, you can use constants generated in the component .h file that specify the frequency of the ticks:&lt;/P&gt;&lt;P&gt;like this:&lt;/P&gt;&lt;P&gt;#define TU1_CNT_INP_FREQ_U_0 0x01400000UL /* Counter input frequency in Hz */&lt;/P&gt;&lt;P&gt;#define TU1_CNT_INP_FREQ_R_0 20971395.017196544F /* Counter input frequency in Hz */&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Petr Hradsky&lt;/P&gt;&lt;P&gt;Processor Expert Support Team&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 Jul 2014 08:52:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Timer-interrupt-LDD-Component-set-period-at-runtime/m-p/324674#M2453</guid>
      <dc:creator>Petr_H</dc:creator>
      <dc:date>2014-07-25T08:52:23Z</dc:date>
    </item>
    <item>
      <title>Re: Timer interrupt LDD Component - set period at runtime?</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Timer-interrupt-LDD-Component-set-period-at-runtime/m-p/324675#M2454</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You guys should hire more people!&amp;nbsp; Its almost 6 months later and the timer beans still only half work for kinetis.&amp;nbsp; What is the point of a timer bean if you can't use it to change the period?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Nov 2014 00:24:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Timer-interrupt-LDD-Component-set-period-at-runtime/m-p/324675#M2454</guid>
      <dc:creator>robotjosh</dc:creator>
      <dc:date>2014-11-21T00:24:02Z</dc:date>
    </item>
    <item>
      <title>Re: Timer interrupt LDD Component - set period at runtime?</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Timer-interrupt-LDD-Component-set-period-at-runtime/m-p/324676#M2455</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I ended up using the PPG: Programmable Pulse Generator and it works very well.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Apr 2015 00:12:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Timer-interrupt-LDD-Component-set-period-at-runtime/m-p/324676#M2455</guid>
      <dc:creator>daveboyle</dc:creator>
      <dc:date>2015-04-28T00:12:26Z</dc:date>
    </item>
  </channel>
</rss>