<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Re: Re: Low Power Wakeup using TSI in PEx in Processor Expert Software</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/Low-Power-Wakeup-using-TSI-in-PEx/m-p/316608#M2395</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Pablo,&lt;/P&gt;&lt;P&gt;The code was developed for CW 10.6 using Processor Expert. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hoe this helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Adrian Sanchez Cano&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 24 Feb 2016 16:27:22 GMT</pubDate>
    <dc:creator>adriancano</dc:creator>
    <dc:date>2016-02-24T16:27:22Z</dc:date>
    <item>
      <title>Low Power Wakeup using TSI in PEx</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Low-Power-Wakeup-using-TSI-in-PEx/m-p/316598#M2385</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can anyone share a kinetis example on how to use tsi as interrupt when wakeup from any of the lowpower modes using a processor expert? Cant find a good example yet.:smileysad:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance..:smileyhappy:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Jun 2014 13:00:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Low-Power-Wakeup-using-TSI-in-PEx/m-p/316598#M2385</guid>
      <dc:creator>javervalino</dc:creator>
      <dc:date>2014-06-10T13:00:55Z</dc:date>
    </item>
    <item>
      <title>Re: Low Power Wakeup using TSI in PEx</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Low-Power-Wakeup-using-TSI-in-PEx/m-p/316599#M2386</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which device or board are you using?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Jun 2014 20:45:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Low-Power-Wakeup-using-TSI-in-PEx/m-p/316599#M2386</guid>
      <dc:creator>adriancano</dc:creator>
      <dc:date>2014-06-10T20:45:43Z</dc:date>
    </item>
    <item>
      <title>Re: Low Power Wakeup using TSI in PEx</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Low-Power-Wakeup-using-TSI-in-PEx/m-p/316600#M2387</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Adrian,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your reply.&lt;/P&gt;&lt;P&gt;Im using a kl25z freedom board. I saw some examples in tss, but its not using a processor expert.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope someone has an example.:smileyhappy:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Jun 2014 07:39:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Low-Power-Wakeup-using-TSI-in-PEx/m-p/316600#M2387</guid>
      <dc:creator>javervalino</dc:creator>
      <dc:date>2014-06-11T07:39:51Z</dc:date>
    </item>
    <item>
      <title>Re: Re: Low Power Wakeup using TSI in PEx</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Low-Power-Wakeup-using-TSI-in-PEx/m-p/316601#M2388</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is a errata with the TSI using Low Power modes.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&lt;BR /&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;e5515:&lt;/STRONG&gt; TSI: The end of scan flag is not automatically cleared when continuously&lt;/P&gt;&lt;P&gt;scanning&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Description:&lt;/STRONG&gt; The TSI requires the end of scan flag (TSIx_GENCS[EOSF]) to be cleared after each scan.&lt;/P&gt;&lt;P&gt;This prevents the out of range interrupt from being available in continuous scanning as each&lt;/P&gt;&lt;P&gt;scan needs the TSIx_GENCS[EOSF] bit to be cleared by software. This limits the TSI from&lt;/P&gt;&lt;P&gt;providing an optimal low power wake-up capability.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Basically it is that the KL25 can not be woken up via TSI. Probably this affect the requirements of your project, if not, the workaround shown in the errata document could be implemented.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Errata documentation:&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/microcontrollers/doc/errata/KINETIS_L_1N97F.pdf?fasp=1&amp;amp;WT_TYPE=Errata&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;Parent_nodeId=1339527982286712105629&amp;amp;Parent_pageType=product" title="http://cache.freescale.com/files/microcontrollers/doc/errata/KINETIS_L_1N97F.pdf?fasp=1&amp;amp;WT_TYPE=Errata&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;Parent_nodeId=1339527982286712105629&amp;amp;Parent_pageType=product"&gt;http://cache.freescale.com/files/microcontrollers/doc/errata/KINETIS_L_1N97F.pdf?fasp=1&amp;amp;WT_TYPE=Errata&amp;amp;WT_VENDOR=FREESCA…&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Jun 2014 15:54:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Low-Power-Wakeup-using-TSI-in-PEx/m-p/316601#M2388</guid>
      <dc:creator>adriancano</dc:creator>
      <dc:date>2014-06-11T15:54:23Z</dc:date>
    </item>
    <item>
      <title>Re: Re: Low Power Wakeup using TSI in PEx</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Low-Power-Wakeup-using-TSI-in-PEx/m-p/316602#M2389</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Adrian,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How about using it in another mcu, let say kl15 etc? Basically, I just want to have an idea how to implement such interrupt using processor expert, not necessarily using it only in kl25. So any example using any mcu, as long as it is done in PEx would be a great help.. :smileyhappy:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks again Adrian..&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Jun 2014 12:47:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Low-Power-Wakeup-using-TSI-in-PEx/m-p/316602#M2389</guid>
      <dc:creator>javervalino</dc:creator>
      <dc:date>2014-06-12T12:47:23Z</dc:date>
    </item>
    <item>
      <title>Re: Re: Re: Low Power Wakeup using TSI in PEx</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Low-Power-Wakeup-using-TSI-in-PEx/m-p/316603#M2390</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here is an example for the KL46. In this example the core is moved to VLPR (Very Low Power Run) mode via the interrupt of the SW1 and you can send it back to normal run mode touching the slider; a led is constantly blinking and you can see that when the core is moved to VLPR the led blinks slower, this is because that in VLPR the max frequency is 4MHz.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this information can help you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. It would be nice!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Jun 2014 23:50:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Low-Power-Wakeup-using-TSI-in-PEx/m-p/316603#M2390</guid>
      <dc:creator>adriancano</dc:creator>
      <dc:date>2014-06-13T23:50:30Z</dc:date>
    </item>
    <item>
      <title>Re: Re: Re: Low Power Wakeup using TSI in PEx</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Low-Power-Wakeup-using-TSI-in-PEx/m-p/316604#M2391</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Adrian,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Cant find any attachment..&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks..&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 14 Jun 2014 03:16:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Low-Power-Wakeup-using-TSI-in-PEx/m-p/316604#M2391</guid>
      <dc:creator>javervalino</dc:creator>
      <dc:date>2014-06-14T03:16:38Z</dc:date>
    </item>
    <item>
      <title>Re: Low Power Wakeup using TSI in PEx</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Low-Power-Wakeup-using-TSI-in-PEx/m-p/316605#M2392</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;This is very helpful Adrian.. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks a lot..:smileyhappy:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 14 Jun 2014 09:01:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Low-Power-Wakeup-using-TSI-in-PEx/m-p/316605#M2392</guid>
      <dc:creator>javervalino</dc:creator>
      <dc:date>2014-06-14T09:01:58Z</dc:date>
    </item>
    <item>
      <title>Re: Re: Re: Low Power Wakeup using TSI in PEx</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Low-Power-Wakeup-using-TSI-in-PEx/m-p/316606#M2393</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Adrian,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Your example was very helpful for me. Can you also give an example how to wakeup from lls using tsi. I really dont know how to configure it in Processor Expert. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Im using kl15 for this project. I hope you can help me.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you and best regards,&lt;/P&gt;&lt;P&gt;Javer&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 14 Sep 2014 13:43:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Low-Power-Wakeup-using-TSI-in-PEx/m-p/316606#M2393</guid>
      <dc:creator>javervalino</dc:creator>
      <dc:date>2014-09-14T13:43:23Z</dc:date>
    </item>
    <item>
      <title>Re: Re: Re: Low Power Wakeup using TSI in PEx</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Low-Power-Wakeup-using-TSI-in-PEx/m-p/316607#M2394</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Adrian,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please could you give us details on version of KDS that was used for the project, also other needed settings for building binary.&amp;nbsp; I've tried with KDS 2.0.0 and KDS 3.0.0 but is not even launching compile process. Thanks in advance,&amp;nbsp; Pablo.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="compile.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/53876i9D896BCF481F9D58/image-size/large?v=v2&amp;amp;px=999" role="button" title="compile.png" alt="compile.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="compile2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/53919i57513638EBCFFB03/image-size/large?v=v2&amp;amp;px=999" role="button" title="compile2.png" alt="compile2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Feb 2016 22:21:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Low-Power-Wakeup-using-TSI-in-PEx/m-p/316607#M2394</guid>
      <dc:creator>PabloBaena</dc:creator>
      <dc:date>2016-02-23T22:21:39Z</dc:date>
    </item>
    <item>
      <title>Re: Re: Re: Low Power Wakeup using TSI in PEx</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Low-Power-Wakeup-using-TSI-in-PEx/m-p/316608#M2395</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Pablo,&lt;/P&gt;&lt;P&gt;The code was developed for CW 10.6 using Processor Expert. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hoe this helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Adrian Sanchez Cano&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Feb 2016 16:27:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Low-Power-Wakeup-using-TSI-in-PEx/m-p/316608#M2395</guid>
      <dc:creator>adriancano</dc:creator>
      <dc:date>2016-02-24T16:27:22Z</dc:date>
    </item>
  </channel>
</rss>