<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Problem Processor Expert configuration, please help me! in Processor Expert Software</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/Problem-Processor-Expert-configuration-please-help-me/m-p/304654#M2289</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;it is possible to share these pins. However, please note that you will not be able to download or debug the application once they are active as GPIO.&lt;/P&gt;&lt;P&gt;In Processor Expert, it's necessary to :&lt;/P&gt;&lt;P&gt;1. go to GPIO or BitIO component where you are using the pin, right-click on the pin and select "Pin sharing enabled".&lt;/P&gt;&lt;P&gt;2. In the GPIO/BitIO component go to Methods tab and enable "ConnectPin" method (you need Advanced view mode)&lt;/P&gt;&lt;P&gt;3. When you want to use the function of the GPIO/BitIO, you need to call ConectPin of the GPIO/BitIO method first. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Petr Hradsky&lt;/P&gt;&lt;P&gt;Processor Expert Support Team&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 02 Apr 2014 13:04:48 GMT</pubDate>
    <dc:creator>Petr_H</dc:creator>
    <dc:date>2014-04-02T13:04:48Z</dc:date>
    <item>
      <title>Problem Processor Expert configuration, please help me!</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Problem-Processor-Expert-configuration-please-help-me/m-p/304653#M2288</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello! I'm working on the FRDM-K20D50M evaluation board and I use Eclipse-based Processor Expert to create a project.But I've got some troubles with GPIO configuration in the Processor Expert.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm trying to set the pin TSI0_CH3/PTA2/JTAG_TDO... as an output port in the GPIO_LDD component, but it tells me that this pin is already used by the CPU.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/43332i5A85436656BFC7BE/image-size/large?v=v2&amp;amp;px=999" title="Capture1.JPG" alt="Capture1.JPG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;In the CPU panel, it shows,&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/43331iB8DC2D2E387F11BE/image-size/large?v=v2&amp;amp;px=999" title="Capture.JPG" alt="Capture.JPG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;In fact, what I wanna do is that, when the program runs, this pin should be a GPIO and when I download or debug the program, this pin should work as a JTAG port. Then how to deal with this problem? Please help me!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Mar 2014 16:50:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Problem-Processor-Expert-configuration-please-help-me/m-p/304653#M2288</guid>
      <dc:creator>kenansun</dc:creator>
      <dc:date>2014-03-26T16:50:49Z</dc:date>
    </item>
    <item>
      <title>Re: Problem Processor Expert configuration, please help me!</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Problem-Processor-Expert-configuration-please-help-me/m-p/304654#M2289</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;it is possible to share these pins. However, please note that you will not be able to download or debug the application once they are active as GPIO.&lt;/P&gt;&lt;P&gt;In Processor Expert, it's necessary to :&lt;/P&gt;&lt;P&gt;1. go to GPIO or BitIO component where you are using the pin, right-click on the pin and select "Pin sharing enabled".&lt;/P&gt;&lt;P&gt;2. In the GPIO/BitIO component go to Methods tab and enable "ConnectPin" method (you need Advanced view mode)&lt;/P&gt;&lt;P&gt;3. When you want to use the function of the GPIO/BitIO, you need to call ConectPin of the GPIO/BitIO method first. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Petr Hradsky&lt;/P&gt;&lt;P&gt;Processor Expert Support Team&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Apr 2014 13:04:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Problem-Processor-Expert-configuration-please-help-me/m-p/304654#M2289</guid>
      <dc:creator>Petr_H</dc:creator>
      <dc:date>2014-04-02T13:04:48Z</dc:date>
    </item>
    <item>
      <title>Re: Problem Processor Expert configuration, please help me!</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Problem-Processor-Expert-configuration-please-help-me/m-p/304655#M2290</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks :smileyhappy:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Apr 2014 08:36:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Problem-Processor-Expert-configuration-please-help-me/m-p/304655#M2290</guid>
      <dc:creator>kenansun</dc:creator>
      <dc:date>2014-04-15T08:36:32Z</dc:date>
    </item>
  </channel>
</rss>