<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Processor Expert SoftwareのトピックCAN LDD problem</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/CAN-LDD-problem/m-p/164472#M219</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm using tha CAN LDD component into a twrk60n512 bsp, the problem I'm facing is that when I transmit a frame and there's no other node in the bus,&lt;/P&gt;&lt;P&gt;some ACK field of the frame it is not set by the receiver to dominant value,&lt;/P&gt;&lt;P&gt;in that case the transmitter interpretes it as an error so it begins to retry the frame tranmission&lt;/P&gt;&lt;P&gt;I want to disable this transmitter error check and I don't see such property inte the component&lt;/P&gt;&lt;P&gt;Any help/idea will be great!!!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Br's&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Jordi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 18 May 2012 23:25:21 GMT</pubDate>
    <dc:creator>jordimerc</dc:creator>
    <dc:date>2012-05-18T23:25:21Z</dc:date>
    <item>
      <title>CAN LDD problem</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/CAN-LDD-problem/m-p/164472#M219</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm using tha CAN LDD component into a twrk60n512 bsp, the problem I'm facing is that when I transmit a frame and there's no other node in the bus,&lt;/P&gt;&lt;P&gt;some ACK field of the frame it is not set by the receiver to dominant value,&lt;/P&gt;&lt;P&gt;in that case the transmitter interpretes it as an error so it begins to retry the frame tranmission&lt;/P&gt;&lt;P&gt;I want to disable this transmitter error check and I don't see such property inte the component&lt;/P&gt;&lt;P&gt;Any help/idea will be great!!!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Br's&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Jordi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 May 2012 23:25:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/CAN-LDD-problem/m-p/164472#M219</guid>
      <dc:creator>jordimerc</dc:creator>
      <dc:date>2012-05-18T23:25:21Z</dc:date>
    </item>
    <item>
      <title>Re: CAN LDD problem</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/CAN-LDD-problem/m-p/164473#M220</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jordi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Function of the CAN_LDD is correct, when a transmitting Frame isn’t received by some node (= it isn’t acknowledged), CAN device try send the frame again with OnError() event calling.&lt;/P&gt;&lt;P&gt;Aborting a transmission frame is possible do by CAN_PDD_SetMessageBufferCode() macro (it is macro defined in CAN_PDD.h library, must be included).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Example:&lt;/P&gt;&lt;P&gt;&amp;nbsp; CAN_PDD_SetMessageBufferCode(CAN1_BASE_PTR, 1U, CAN_PDD_MB_TX_ABORT);&amp;nbsp; // aborts a transmitting frame for CAN1 device, Message buffer 1&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;J.R.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 May 2012 19:11:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/CAN-LDD-problem/m-p/164473#M220</guid>
      <dc:creator>jiri_rezler</dc:creator>
      <dc:date>2012-05-22T19:11:45Z</dc:date>
    </item>
  </channel>
</rss>