<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Processor Expert SoftwareのトピックRe: TWR k60 Ethernet barecode codewarrior 10.5 mac address issue</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/TWR-k60-Ethernet-barecode-codewarrior-10-5-mac-address-issue/m-p/294159#M2158</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ladislav ,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for the reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Shiju&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 17 May 2014 05:07:27 GMT</pubDate>
    <dc:creator>shiju_cg</dc:creator>
    <dc:date>2014-05-17T05:07:27Z</dc:date>
    <item>
      <title>TWR k60 Ethernet barecode codewarrior 10.5 mac address issue</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/TWR-k60-Ethernet-barecode-codewarrior-10-5-mac-address-issue/m-p/294157#M2156</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I am using TWR K60DN512 and code warrior 10.5. I have imported the PE code for Ethernet communication in the example list&amp;nbsp; for twr k60DN512 board.It is working perfectly. The&amp;nbsp; mac address given in the program is uint8_t MACAddress[] = { 0x06, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF }; but the device mac address written on the board is&amp;nbsp; 00:04:9F:01:64:3B . when i tried to replace the mac address in the program with the mac address written on board the program is not receiving data back. Can anybody tell the reason? I need to establish an Ethernet communication interface. Which mac should i use? Thanks and regards Shiju&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 May 2014 10:11:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/TWR-k60-Ethernet-barecode-codewarrior-10-5-mac-address-issue/m-p/294157#M2156</guid>
      <dc:creator>shiju_cg</dc:creator>
      <dc:date>2014-05-09T10:11:57Z</dc:date>
    </item>
    <item>
      <title>Re: TWR k60 Ethernet barecode codewarrior 10.5 mac address issue</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/TWR-k60-Ethernet-barecode-codewarrior-10-5-mac-address-issue/m-p/294158#M2157</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Shiju,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;if you change the MACAddress variable, you must change the MAC address property value in the Ethernet_LDD component in the Processor Expert project too. The property value is the address which is set into the ENET module during component initialization. The variable value is the address used as the source and destination address of the transmitted ethernet frame.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Ladislav Vadkerti&lt;/P&gt;&lt;P&gt;Freescale Processor Expert Team&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 May 2014 13:16:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/TWR-k60-Ethernet-barecode-codewarrior-10-5-mac-address-issue/m-p/294158#M2157</guid>
      <dc:creator>LadislavVadkerti</dc:creator>
      <dc:date>2014-05-14T13:16:58Z</dc:date>
    </item>
    <item>
      <title>Re: TWR k60 Ethernet barecode codewarrior 10.5 mac address issue</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/TWR-k60-Ethernet-barecode-codewarrior-10-5-mac-address-issue/m-p/294159#M2158</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ladislav ,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for the reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Shiju&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 17 May 2014 05:07:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/TWR-k60-Ethernet-barecode-codewarrior-10-5-mac-address-issue/m-p/294159#M2158</guid>
      <dc:creator>shiju_cg</dc:creator>
      <dc:date>2014-05-17T05:07:27Z</dc:date>
    </item>
  </channel>
</rss>