<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Processor Expert SoftwareのトピックRe: Generating RESET signal using MCF51JM128 platform</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/Generating-RESET-signal-using-MCF51JM128-platform/m-p/282147#M1954</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you write more details on what kind of LCD do you use and how it's connected to the MCU? &lt;/P&gt;&lt;P&gt;The Init_COP provides an initialization of the COP module which is a kind of watchdog that resets two whole processor if it's not refreshed.&lt;/P&gt;&lt;P&gt;If the mentioned RESET pin is s standard digital IO you can drive it using BitIO component.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;best regards&lt;/P&gt;&lt;P&gt;Petr Hradsky&lt;/P&gt;&lt;P&gt;Processor Expert Support Team&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 30 Aug 2013 07:54:46 GMT</pubDate>
    <dc:creator>Petr_H</dc:creator>
    <dc:date>2013-08-30T07:54:46Z</dc:date>
    <item>
      <title>Generating RESET signal using MCF51JM128 platform</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Generating-RESET-signal-using-MCF51JM128-platform/m-p/282146#M1953</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm developing an application using CodeWarrior which will run on an MCF51JM128-based system and would like to get the processor to drive a RESET signal for an LCD display. I've looped at the Init_COP component and thought this might be the solution but I'm not sure. Can anyone provide some guidance please..?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ken&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Aug 2013 13:09:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Generating-RESET-signal-using-MCF51JM128-platform/m-p/282146#M1953</guid>
      <dc:creator>MWMinor</dc:creator>
      <dc:date>2013-08-29T13:09:43Z</dc:date>
    </item>
    <item>
      <title>Re: Generating RESET signal using MCF51JM128 platform</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Generating-RESET-signal-using-MCF51JM128-platform/m-p/282147#M1954</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you write more details on what kind of LCD do you use and how it's connected to the MCU? &lt;/P&gt;&lt;P&gt;The Init_COP provides an initialization of the COP module which is a kind of watchdog that resets two whole processor if it's not refreshed.&lt;/P&gt;&lt;P&gt;If the mentioned RESET pin is s standard digital IO you can drive it using BitIO component.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;best regards&lt;/P&gt;&lt;P&gt;Petr Hradsky&lt;/P&gt;&lt;P&gt;Processor Expert Support Team&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 30 Aug 2013 07:54:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Generating-RESET-signal-using-MCF51JM128-platform/m-p/282147#M1954</guid>
      <dc:creator>Petr_H</dc:creator>
      <dc:date>2013-08-30T07:54:46Z</dc:date>
    </item>
  </channel>
</rss>