<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: PE components are created but do not show up in CW10 in Processor Expert Software</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/PE-components-are-created-but-do-not-show-up-in-CW10/m-p/160532#M192</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You are right. I could not find the Embedded Components folder because it is within the "Processor Expert.pe" element. The icon for this looks like a text file, thus I did not notice the "+" sign that allowed me to expand that element. Now I can see all PE components, PWMs and CPU.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 19 Aug 2011 21:41:16 GMT</pubDate>
    <dc:creator>quevedo</dc:creator>
    <dc:date>2011-08-19T21:41:16Z</dc:date>
    <item>
      <title>PE components are created but do not show up in CW10</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/PE-components-are-created-but-do-not-show-up-in-CW10/m-p/160530#M190</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am moving to CW10, and I am trying to create a new project from scratch for the TWR-MECH board (target processor MCF52259). I want to use Processor Expert (PE). My CodeWarrior is&amp;nbsp;Version 10.1, Build Id 110726﻿, Special Edition.﻿&amp;nbsp;During the "create new project" wizard, I selected the bare target processor, not any of the option for tower boards.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I selected a PE component (PWM Component) at the Components Library pane, then I clicked on it with the right button, and selected "Add to project" option. However, the PWM component did not show up at the Project Panel (and I cannot see any "Embedded Components" folder inside the project either). My first thought was that I did not select the Add option correctly, so I tried that again. No changes. The CPU component &amp;nbsp;also does not show up right after the new project wizard finished, as it happened in previous versions of CW.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So I tried to click on the "Generate Processor Expert Project" button at the Project Panel. I get an error message stating that there is some error. Looking at the Problems tab, I find errors related to PWM1 and PWM2 components. When I double-click on one of these messages, the Component Inspector pane is loaded with the config options of the PWM component, showing the errors: unassigned timings for period and starting pulse width. it means that the components were created, but do not show up in the Project Panel.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I right-clicked at the project panel and chose Refresh to see what happened. Nothing.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I suppose it has something to do with the CW configuration. I can configure any components that are not fully configured when created (because of the errors), but after configured i cannot access them anymore.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;How can I fix it? Just a reminder, the installation is brand new, I did not alter any default configs. I also tried the same install in 2 computers (one running WinXP and the other on Windows 7).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Aug 2011 18:23:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/PE-components-are-created-but-do-not-show-up-in-CW10/m-p/160530#M190</guid>
      <dc:creator>quevedo</dc:creator>
      <dc:date>2011-08-19T18:23:04Z</dc:date>
    </item>
    <item>
      <title>Re: PE components are created but do not show up in CW10</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/PE-components-are-created-but-do-not-show-up-in-CW10/m-p/160531#M191</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It seems you have overlooked “Embedded Component” folder on the project panel. You should unfold this folder to show all components in the project. I have also tried to add the PWM component to the M52559 PE project in CW V10.1 (B110726) and I have not encountered any problem.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Below, you can find steps how to properly add a new component to the project in eclipse:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Make a focus on the project where you want add a component (e.g. click on the CPU component).&lt;/LI&gt;&lt;LI&gt;Go to the “Components Library” and add a component by double clicking on it or using appropriate menu command from selected component´s pop-menu.&lt;/LI&gt;&lt;LI&gt;Unfold Embedded Components folder.&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For more details please see enclosed scren-shot.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;best regards&lt;BR /&gt;Vojtech Filip&lt;BR /&gt;Processor Expert Support Team﻿&lt;/P&gt;&lt;P&gt;﻿&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Aug 2011 20:10:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/PE-components-are-created-but-do-not-show-up-in-CW10/m-p/160531#M191</guid>
      <dc:creator>ProcessorExpert</dc:creator>
      <dc:date>2011-08-19T20:10:46Z</dc:date>
    </item>
    <item>
      <title>Re: PE components are created but do not show up in CW10</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/PE-components-are-created-but-do-not-show-up-in-CW10/m-p/160532#M192</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You are right. I could not find the Embedded Components folder because it is within the "Processor Expert.pe" element. The icon for this looks like a text file, thus I did not notice the "+" sign that allowed me to expand that element. Now I can see all PE components, PWMs and CPU.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Aug 2011 21:41:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/PE-components-are-created-but-do-not-show-up-in-CW10/m-p/160532#M192</guid>
      <dc:creator>quevedo</dc:creator>
      <dc:date>2011-08-19T21:41:16Z</dc:date>
    </item>
  </channel>
</rss>