<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Processor Expert SoftwareのトピックRe: ADC Init Problem</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/ADC-Init-Problem/m-p/275585#M1849</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Vojtech,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks for the hint. I just overlooked that item. Is there a difference in LDD components in Init components concerning that item. If I remember correctly the LDD components work even if clockgate is not enabled. But I am not sure and will double check this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Markus&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 17 Jul 2013 05:20:13 GMT</pubDate>
    <dc:creator>mkrug</dc:creator>
    <dc:date>2013-07-17T05:20:13Z</dc:date>
    <item>
      <title>ADC Init Problem</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/ADC-Init-Problem/m-p/275583#M1847</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;after that I realized that Enable/Diable ADC with the LDD component does not really do what I expectI decided to go to the Init_ADC component. It gives me the additional advantage to setup a DMA transfer what I will very likely need.&lt;/P&gt;&lt;P&gt;However even the normal Init() function leads to some suspect problem. It seems to me that the Init() function (in my case the function is called Line_Camera_Init() want to change registers but is not successful. In my actual case I realized that the first call to ADC1_CFG1 does not lead to the desired change in the register - I hope you can see this from the screenshot. For example ADICLK is not changed to 3 (the last two&amp;nbsp; bits in ADC1_CFG1. It gets even worse. In the second command the Init() function wants to change ADC2_CFG2. The access to this register leads to a crash and I find myself in the ISR CPU_Interrupt.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can anyone explain this behaviour? I am using CW10.4 on a Kinetis K60 Tower System.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Markus&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="ADC_Init01.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/119617iFED09DC8B2F01185/image-size/large?v=v2&amp;amp;px=999" role="button" title="ADC_Init01.jpg" alt="ADC_Init01.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Jul 2013 16:31:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/ADC-Init-Problem/m-p/275583#M1847</guid>
      <dc:creator>mkrug</dc:creator>
      <dc:date>2013-07-16T16:31:40Z</dc:date>
    </item>
    <item>
      <title>Re: ADC Init Problem</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/ADC-Init-Problem/m-p/275584#M1848</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;you have to enable clockgate for ADC device. Check top of the component there is item you need to enable.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;rgds&lt;/P&gt;&lt;P&gt;Vojtech Filip&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Jul 2013 17:05:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/ADC-Init-Problem/m-p/275584#M1848</guid>
      <dc:creator>vfilip</dc:creator>
      <dc:date>2013-07-16T17:05:06Z</dc:date>
    </item>
    <item>
      <title>Re: ADC Init Problem</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/ADC-Init-Problem/m-p/275585#M1849</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Vojtech,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks for the hint. I just overlooked that item. Is there a difference in LDD components in Init components concerning that item. If I remember correctly the LDD components work even if clockgate is not enabled. But I am not sure and will double check this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Markus&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Jul 2013 05:20:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/ADC-Init-Problem/m-p/275585#M1849</guid>
      <dc:creator>mkrug</dc:creator>
      <dc:date>2013-07-17T05:20:13Z</dc:date>
    </item>
  </channel>
</rss>