<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Processor Expert SoftwareのトピックProcessor Expert component development/installation issue on older CodeWarrior.</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/Processor-Expert-component-development-installation-issue-on/m-p/258020#M1590</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm now diving into the world of PEx/CDE, and having trouble using my component with older CW (CW for HCS12 v5.1, with PEx v3.02).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The problem is that it takes nearly 30minutes to install even a small (~20KB) PEupd file. It kind of works after that, but is simply a pain to use. Strange part is that the same PEupd file installs instantly and works fine on CW v10.5.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This only happens with the component I packaged, and does not happen with other PEupd files. For example, following installs and works just fine:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;A href="https://github.com/ErichStyger/mcuoneclipse/tree/master/PEupd" title="https://github.com/ErichStyger/mcuoneclipse/tree/master/PEupd"&gt;mcuoneclipse/PEupd at master · ErichStyger/mcuoneclipse · GitHub&lt;/A&gt;&lt;/LI&gt;&lt;LI&gt;&lt;A href="https://community.nxp.com/docs/DOC-93247"&gt;S19_1.025.PEupd&lt;/A&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To troubleshoot this, I grabbed above S19 PEupd, imported into CDE on v10.5, and simply re-exported it. It doesn't work (works with v10.5, but painfully slow on v5.1). &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now, I re-imported above "painfully slow, re-packaged S19 PEupd" into CDE on v5.1 (this v5.1 is an eval edition, so CDE is enabled), and again did a re-re-export. Surprisingly, now it installs instantly and works fine on both v10.5 and v5.1 CW.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Whenever this "slow installation" issue occurs, PEx keeps showing a dialog with a progress meter saying "Gathering data about component".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After some investigations, I found that&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;For those that have this installation issue, they seem to go into "System" PEx folder (C:\Program Files\Freescale\CWS12v5.1\ProcessorExpert).&lt;/LI&gt;&lt;LI&gt;For others that install instantly, they go into "User" PXe folder (C:\ProgramData\Processor Expert\CW12_PE3_02).&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My guess is installation to "System" PEx folder causes whole rebuild of component database, which takes time.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there any configuration I need to do to control this behavior?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I know CW v5.1 is outdated, but I'm still using HCS12 and I'm also wondering what I'm missing with my PEupd file, as other PEupd files installs just fine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 25 Feb 2014 12:08:07 GMT</pubDate>
    <dc:creator>tyamadajp</dc:creator>
    <dc:date>2014-02-25T12:08:07Z</dc:date>
    <item>
      <title>Processor Expert component development/installation issue on older CodeWarrior.</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Processor-Expert-component-development-installation-issue-on/m-p/258020#M1590</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm now diving into the world of PEx/CDE, and having trouble using my component with older CW (CW for HCS12 v5.1, with PEx v3.02).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The problem is that it takes nearly 30minutes to install even a small (~20KB) PEupd file. It kind of works after that, but is simply a pain to use. Strange part is that the same PEupd file installs instantly and works fine on CW v10.5.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This only happens with the component I packaged, and does not happen with other PEupd files. For example, following installs and works just fine:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;A href="https://github.com/ErichStyger/mcuoneclipse/tree/master/PEupd" title="https://github.com/ErichStyger/mcuoneclipse/tree/master/PEupd"&gt;mcuoneclipse/PEupd at master · ErichStyger/mcuoneclipse · GitHub&lt;/A&gt;&lt;/LI&gt;&lt;LI&gt;&lt;A href="https://community.nxp.com/docs/DOC-93247"&gt;S19_1.025.PEupd&lt;/A&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To troubleshoot this, I grabbed above S19 PEupd, imported into CDE on v10.5, and simply re-exported it. It doesn't work (works with v10.5, but painfully slow on v5.1). &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now, I re-imported above "painfully slow, re-packaged S19 PEupd" into CDE on v5.1 (this v5.1 is an eval edition, so CDE is enabled), and again did a re-re-export. Surprisingly, now it installs instantly and works fine on both v10.5 and v5.1 CW.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Whenever this "slow installation" issue occurs, PEx keeps showing a dialog with a progress meter saying "Gathering data about component".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After some investigations, I found that&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;For those that have this installation issue, they seem to go into "System" PEx folder (C:\Program Files\Freescale\CWS12v5.1\ProcessorExpert).&lt;/LI&gt;&lt;LI&gt;For others that install instantly, they go into "User" PXe folder (C:\ProgramData\Processor Expert\CW12_PE3_02).&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My guess is installation to "System" PEx folder causes whole rebuild of component database, which takes time.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there any configuration I need to do to control this behavior?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I know CW v5.1 is outdated, but I'm still using HCS12 and I'm also wondering what I'm missing with my PEupd file, as other PEupd files installs just fine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Feb 2014 12:08:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Processor-Expert-component-development-installation-issue-on/m-p/258020#M1590</guid>
      <dc:creator>tyamadajp</dc:creator>
      <dc:date>2014-02-25T12:08:07Z</dc:date>
    </item>
    <item>
      <title>Re: Processor Expert component development/installation issue on older CodeWarrior.</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Processor-Expert-component-development-installation-issue-on/m-p/258021#M1591</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;unfortunatelly, the component packages created by the CDE contain the settings that make the package very slow in CW classic fro HCS12 V5.1. &lt;/P&gt;&lt;P&gt;If you create the components in classic CodeWarrior, pleause use the Component Wizard tool delivered with the CodeWarrior classic, which should work properly there.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Petr Hradsky&lt;/P&gt;&lt;P&gt;Processor Expert Support Team&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 May 2014 08:14:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Processor-Expert-component-development-installation-issue-on/m-p/258021#M1591</guid>
      <dc:creator>Petr_H</dc:creator>
      <dc:date>2014-05-12T08:14:41Z</dc:date>
    </item>
  </channel>
</rss>