<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Processor Expert SoftwareのトピックRe: Moving a component from CW Processor Expert to Driver Suite (FreeMaster)</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/Moving-a-component-from-CW-Processor-Expert-to-Driver-Suite/m-p/251018#M1425</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Mike,&lt;/P&gt;&lt;P&gt;This was known limitation the peupd files. The update integrates the component, but does not update the list of supported devices. I expected that this was already solved. The workarround in CodeWarrior was that you could disable the component filter.&lt;/P&gt;&lt;P&gt;If stand alone suite driver does not have any option to disable component filter, I worry that you have to wait for next suite driver release.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Jaroslav&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 03 Jul 2013 19:58:16 GMT</pubDate>
    <dc:creator>JardaP</dc:creator>
    <dc:date>2013-07-03T19:58:16Z</dc:date>
    <item>
      <title>Moving a component from CW Processor Expert to Driver Suite (FreeMaster)</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Moving-a-component-from-CW-Processor-Expert-to-Driver-Suite/m-p/251015#M1422</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I wish to use the Processor Expert Driver Suite with IAR for an MQX-Lite Project on a K60F120.&amp;nbsp; I also wish to use FreeMaster in the IAR/PEx environment.&amp;nbsp; The challenge I face is that the FreeMaster Component only seems to be available in the CodeWarrior version of ProcessorExpert.&amp;nbsp; I have tried a few things to move it over, but nothing has worked.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. Is there a way to Export the component from CW and then Import it to Driver Suite so it is available in the Component Library and able to be added to any project within the Driver Suite?&lt;/P&gt;&lt;P&gt;2. Is there an .PEupd file with the FreeMaster component available?&lt;/P&gt;&lt;P&gt;3. Is there some other way to accomplish this?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind Regards,&lt;/P&gt;&lt;P&gt;Mike Maas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Jul 2013 18:02:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Moving-a-component-from-CW-Processor-Expert-to-Driver-Suite/m-p/251015#M1422</guid>
      <dc:creator>mmaas</dc:creator>
      <dc:date>2013-07-02T18:02:20Z</dc:date>
    </item>
    <item>
      <title>Re: Moving a component from CW Processor Expert to Driver Suite (FreeMaster)</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Moving-a-component-from-CW-Processor-Expert-to-Driver-Suite/m-p/251016#M1423</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Mike,&lt;/P&gt;&lt;P&gt;The update of the FreeMATSER conponent is available here:&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-95086"&gt;https://community.freescale.com/docs/DOC-95086&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regrads,&lt;/P&gt;&lt;P&gt;Jaroslav&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Jul 2013 18:28:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Moving-a-component-from-CW-Processor-Expert-to-Driver-Suite/m-p/251016#M1423</guid>
      <dc:creator>JardaP</dc:creator>
      <dc:date>2013-07-03T18:28:20Z</dc:date>
    </item>
    <item>
      <title>Re: Moving a component from CW Processor Expert to Driver Suite (FreeMaster)</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Moving-a-component-from-CW-Processor-Expert-to-Driver-Suite/m-p/251017#M1424</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jaroslav,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for posting the latest FreeMASTER component!&amp;nbsp; I have imported it into my Processor Expert Driver Suite and I do see some problems. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I look at the Components Library in a workspace without any projects I can see the FreeMASTER component in the "CPU External Devices -&amp;gt; Display" folder. &lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="FreeMASTER shown with no project.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/39767i0D89DDA184DB4F84/image-size/large?v=v2&amp;amp;px=999" role="button" title="FreeMASTER shown with no project.jpg" alt="FreeMASTER shown with no project.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;When I create a project for either a Kinetis K (MK60DN512VLQ10) or Kinetis L (MKL25Z128VLK4), the FreeMASTER component is no longer listed in the Components Library. &lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="FreeMASTER NOT shown with Kinetis project.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/39783i2EEA51573FE8A250/image-size/large?v=v2&amp;amp;px=999" role="button" title="FreeMASTER NOT shown with Kinetis project.jpg" alt="FreeMASTER NOT shown with Kinetis project.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;It seems that Processor Expert does not think that the Kinetis devices are supported by this component.&amp;nbsp; I do not see anything in the "Help on Component" that indicates what devices are supported by this component. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The end effect is that I am unable to add the FreeMASTER component to a Kinetis project within the Driver Suite.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is this a challenge for me since I am using the stand alone Driver Suite rather than the CodeWarrior tool?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind Regards,&lt;/P&gt;&lt;P&gt;Mike Maas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Jul 2013 19:08:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Moving-a-component-from-CW-Processor-Expert-to-Driver-Suite/m-p/251017#M1424</guid>
      <dc:creator>mmaas</dc:creator>
      <dc:date>2013-07-03T19:08:56Z</dc:date>
    </item>
    <item>
      <title>Re: Moving a component from CW Processor Expert to Driver Suite (FreeMaster)</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Moving-a-component-from-CW-Processor-Expert-to-Driver-Suite/m-p/251018#M1425</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Mike,&lt;/P&gt;&lt;P&gt;This was known limitation the peupd files. The update integrates the component, but does not update the list of supported devices. I expected that this was already solved. The workarround in CodeWarrior was that you could disable the component filter.&lt;/P&gt;&lt;P&gt;If stand alone suite driver does not have any option to disable component filter, I worry that you have to wait for next suite driver release.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Jaroslav&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Jul 2013 19:58:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Moving-a-component-from-CW-Processor-Expert-to-Driver-Suite/m-p/251018#M1425</guid>
      <dc:creator>JardaP</dc:creator>
      <dc:date>2013-07-03T19:58:16Z</dc:date>
    </item>
    <item>
      <title>Re: Moving a component from CW Processor Expert to Driver Suite (FreeMaster)</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Moving-a-component-from-CW-Processor-Expert-to-Driver-Suite/m-p/251019#M1426</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Greetings Jaroslav,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Finally had a moment to go back to this exercise.&amp;nbsp; Indeed, with Component Filtering disabled, the FreeMASTER component is available in the Driver Suite for the Kinetis Architectures.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="FreeMASTER available with component filter off.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/119564iF08737C93734A4E9/image-size/large?v=v2&amp;amp;px=999" role="button" title="FreeMASTER available with component filter off.jpg" alt="FreeMASTER available with component filter off.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Forward Progress!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind Regards, &lt;/P&gt;&lt;P&gt;Mike&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Jul 2013 16:37:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Moving-a-component-from-CW-Processor-Expert-to-Driver-Suite/m-p/251019#M1426</guid>
      <dc:creator>mmaas</dc:creator>
      <dc:date>2013-07-09T16:37:07Z</dc:date>
    </item>
    <item>
      <title>Re: Moving a component from CW Processor Expert to Driver Suite (FreeMaster)</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Moving-a-component-from-CW-Processor-Expert-to-Driver-Suite/m-p/251020#M1427</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Mike,&lt;/P&gt;&lt;P&gt;I uploaded an update of FreeMASTER component.&lt;/P&gt;&lt;P&gt;This fixes one internal error related to header of generated files.&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-95125"&gt;https://community.freescale.com/docs/DOC-95125&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Jaroslav&lt;/P&gt;&lt;P&gt;&lt;BR /&gt; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Jul 2013 15:25:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Moving-a-component-from-CW-Processor-Expert-to-Driver-Suite/m-p/251020#M1427</guid>
      <dc:creator>JardaP</dc:creator>
      <dc:date>2013-07-11T15:25:32Z</dc:date>
    </item>
  </channel>
</rss>