<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Processor Expert Software中的主题 FreeCntr component can't Enable/Disable Events?</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/FreeCntr-component-can-t-Enable-Disable-Events/m-p/245393#M1383</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am working with CodeWarrior 5.1 for S12(X).&amp;nbsp; My target is 9S12XA256.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am adding the FreeCntr component and setting it up to be an output compare that interrupts at a specified rate. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is no way to disable the interrupt event.&amp;nbsp; The Enable/Disable Event methods are grayed out in Processor Expert and nothing I do will enable them.&amp;nbsp; I tried connecting it to different timer sources, shared timers, individual PIT timers, etc.&amp;nbsp; Nothing works.&amp;nbsp; The Enable/Disable events are always grayed out.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How do I stop this FreeCntr componet from interrupting when I do not need it anymore?&amp;nbsp; Aside from going directly to the registers myself with my own code, I think there is something seriously wrong with this component and the way it was implemented.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 02 Feb 2013 06:37:29 GMT</pubDate>
    <dc:creator>jgirard1</dc:creator>
    <dc:date>2013-02-02T06:37:29Z</dc:date>
    <item>
      <title>FreeCntr component can't Enable/Disable Events?</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/FreeCntr-component-can-t-Enable-Disable-Events/m-p/245393#M1383</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am working with CodeWarrior 5.1 for S12(X).&amp;nbsp; My target is 9S12XA256.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am adding the FreeCntr component and setting it up to be an output compare that interrupts at a specified rate. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is no way to disable the interrupt event.&amp;nbsp; The Enable/Disable Event methods are grayed out in Processor Expert and nothing I do will enable them.&amp;nbsp; I tried connecting it to different timer sources, shared timers, individual PIT timers, etc.&amp;nbsp; Nothing works.&amp;nbsp; The Enable/Disable events are always grayed out.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How do I stop this FreeCntr componet from interrupting when I do not need it anymore?&amp;nbsp; Aside from going directly to the registers myself with my own code, I think there is something seriously wrong with this component and the way it was implemented.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 02 Feb 2013 06:37:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/FreeCntr-component-can-t-Enable-Disable-Events/m-p/245393#M1383</guid>
      <dc:creator>jgirard1</dc:creator>
      <dc:date>2013-02-02T06:37:29Z</dc:date>
    </item>
    <item>
      <title>Re: FreeCntr component can't Enable/Disable Events?</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/FreeCntr-component-can-t-Enable-Disable-Events/m-p/245394#M1384</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The events in the Events tab have to be enabled first before the Enable/Disable methods will be activated in the Methods tab.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Feb 2013 02:43:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/FreeCntr-component-can-t-Enable-Disable-Events/m-p/245394#M1384</guid>
      <dc:creator>jgirard1</dc:creator>
      <dc:date>2013-02-04T02:43:46Z</dc:date>
    </item>
  </channel>
</rss>