<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Is it possible to change target processor keeping preset parameters in PE? in Processor Expert Software</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/Is-it-possible-to-change-target-processor-keeping-preset/m-p/236476#M1258</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It seems like misunderstanding. I described transferring components with settings (not CPU) to a newly created project for another CPU. Using the menu command &lt;SPAN style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; background-color: #ffffff;"&gt;File &amp;gt; Import.. and then go to Processor Expert / Component Settings to Project.&lt;/SPAN&gt; There in the file dialog you can change extension to .pe and select another existing project and select what component you want to import. I think that this is "&lt;SPAN style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; background-color: #ffffff;"&gt;Import Settings from PE File"&lt;/SPAN&gt; that you have mentioned.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you don't want to create a new project for a new CPU, you can select and add a new CPU component using Processors tab in the Components library view. Then you can enable it and the project switches to this new CPU.&lt;/P&gt;&lt;P&gt;However, there might be issues with compiler/linker if the new CPU requires another compiler/settings, because using this you won't go through project creation wizard that does some parts of new project configuration.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;best regards&lt;/P&gt;&lt;P&gt;Petr Hradsky&lt;/P&gt;&lt;P&gt;Processor Expert Support Team&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 02 Apr 2013 12:41:18 GMT</pubDate>
    <dc:creator>Petr_H</dc:creator>
    <dc:date>2013-04-02T12:41:18Z</dc:date>
    <item>
      <title>Is it possible to change target processor keeping preset parameters in PE?</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Is-it-possible-to-change-target-processor-keeping-preset/m-p/236472#M1254</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm creating the BSP/PSP for a custom board we're developing based on MK20DN512VLK10 and using MQX (version 4.0) and Eclipse based Code Warrior 10.3 (Windows). The MK20DN512VLK10 derivative is not directly supported by current PE tools (see &lt;A href="https://community.nxp.com/message/319386"&gt;Re: Is MK20DX256VLK10 missing in Processor Expert ?&lt;/A&gt;), so using the MK20DN512VLK10 (larger flash memory) as a starting point and tweaking flash settings is the recommendation given by &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/VF"&gt;VF&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Firstly, I've created a BSP clone taking '&lt;STRONG&gt;bsp_twrk20d72m&lt;/STRONG&gt;' as source BSP for the &lt;STRONG&gt;MQX BSP cloning Wizard&lt;/STRONG&gt;. The &lt;STRONG&gt;twrk20d72m&lt;/STRONG&gt; is using even another derivative with different frequencies and pinout.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How could I do for changing the target processor in the BSP, but keeping most PE Component configuration parameters as they were set for the original BSP processor?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Mar 2013 14:32:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Is-it-possible-to-change-target-processor-keeping-preset/m-p/236472#M1254</guid>
      <dc:creator>VictorLorenzo</dc:creator>
      <dc:date>2013-03-22T14:32:46Z</dc:date>
    </item>
    <item>
      <title>Re: Is it possible to change target processor keeping preset parameters in PE?</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Is-it-possible-to-change-target-processor-keeping-preset/m-p/236473#M1255</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Correction: I typed wrongly the partnumber, it should have been MK20DX256VLK10 instead of MK20DN512VLK10 (which is indeed supported in PE). Anyway, using the 'visual_memory+mouse+keyboard+soomeee_time...' method did the job.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;At the end we finally installed one MK20DN512VLK10.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Mar 2013 11:20:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Is-it-possible-to-change-target-processor-keeping-preset/m-p/236473#M1255</guid>
      <dc:creator>VictorLorenzo</dc:creator>
      <dc:date>2013-03-26T11:20:13Z</dc:date>
    </item>
    <item>
      <title>Re: Is it possible to change target processor keeping preset parameters in PE?</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Is-it-possible-to-change-target-processor-keeping-preset/m-p/236474#M1256</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can transfer components with their settings across the projects (no matter that the CPU is different) using copy/paste pop-up menu commands or using File &amp;gt; Import.. and then go to Processor Expert / Component Settings to Project. &lt;/P&gt;&lt;P&gt;The problem can be in this case that pin names may not match, also there may be some peripherals different or missing. So after such import, you should go through all component settings and adjust the settings in the components that are not correct or report error.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;best regards&lt;/P&gt;&lt;P&gt;Petr Hradsky&lt;/P&gt;&lt;P&gt;Processor Expert Support Team&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Mar 2013 13:03:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Is-it-possible-to-change-target-processor-keeping-preset/m-p/236474#M1256</guid>
      <dc:creator>Petr_H</dc:creator>
      <dc:date>2013-03-27T13:03:21Z</dc:date>
    </item>
    <item>
      <title>Re: Is it possible to change target processor keeping preset parameters in PE?</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Is-it-possible-to-change-target-processor-keeping-preset/m-p/236475#M1257</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Petr, thanks a lot for taking a time.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried copy/paste the CPU component just as I did with some other components, but the CPU kept being the same. I also tried importing the CPU thru File/Import... with same results, not being able of changing the CPU for one not listed in PE's CPU properties view (or at least not being able to find the way to do it).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Something I found useful for saving settings for later use was the "Save Component Settings As Template" tool (mouse right-click over the CPU component in the project components view). It's a good tool.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As a complimentary PE's tool, I think it could be useful having a tool like "Apply Settings from Template" and/or "Import Settings from PE File". Freescale uses to have several CPUs from the product lines that share many characteristics (core, peripherals, memory types, clock generators, power management, etc).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards, Victor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Mar 2013 20:11:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Is-it-possible-to-change-target-processor-keeping-preset/m-p/236475#M1257</guid>
      <dc:creator>VictorLorenzo</dc:creator>
      <dc:date>2013-03-28T20:11:19Z</dc:date>
    </item>
    <item>
      <title>Re: Is it possible to change target processor keeping preset parameters in PE?</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Is-it-possible-to-change-target-processor-keeping-preset/m-p/236476#M1258</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It seems like misunderstanding. I described transferring components with settings (not CPU) to a newly created project for another CPU. Using the menu command &lt;SPAN style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; background-color: #ffffff;"&gt;File &amp;gt; Import.. and then go to Processor Expert / Component Settings to Project.&lt;/SPAN&gt; There in the file dialog you can change extension to .pe and select another existing project and select what component you want to import. I think that this is "&lt;SPAN style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; background-color: #ffffff;"&gt;Import Settings from PE File"&lt;/SPAN&gt; that you have mentioned.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you don't want to create a new project for a new CPU, you can select and add a new CPU component using Processors tab in the Components library view. Then you can enable it and the project switches to this new CPU.&lt;/P&gt;&lt;P&gt;However, there might be issues with compiler/linker if the new CPU requires another compiler/settings, because using this you won't go through project creation wizard that does some parts of new project configuration.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;best regards&lt;/P&gt;&lt;P&gt;Petr Hradsky&lt;/P&gt;&lt;P&gt;Processor Expert Support Team&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Apr 2013 12:41:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Is-it-possible-to-change-target-processor-keeping-preset/m-p/236476#M1258</guid>
      <dc:creator>Petr_H</dc:creator>
      <dc:date>2013-04-02T12:41:18Z</dc:date>
    </item>
  </channel>
</rss>