<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Processor Expert SoftwareのトピックRe: Can I do memory to memory DMA transfer in kinetis MCU using interrupt.</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/Can-I-do-memory-to-memory-DMA-transfer-in-kinetis-MCU-using/m-p/236353#M1253</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, if you mean triggering&amp;nbsp; a DMA transfer by a timer or other interrupt flag event.&lt;/P&gt;&lt;P&gt;I recommend to use DMAChanne_LDD component. There is a property Hardware request that you can enable and select the source of event that triggers the transfer. For example FTM_C0_DMA_Request comes from channel 0 of the FTM0 timer.&lt;/P&gt;&lt;P&gt;If you select it, you also need to create a timer component that initializes the timer - you can do it for example with TimerUnit_LDD where you select FTM0, period&amp;nbsp; and setup channel 0 where where you select offset and enable the DMA request in Interrupts/DMA.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Petr Hradsky&lt;/P&gt;&lt;P&gt;Processor Expert Support Team&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 26 Feb 2014 12:02:39 GMT</pubDate>
    <dc:creator>Petr_H</dc:creator>
    <dc:date>2014-02-26T12:02:39Z</dc:date>
    <item>
      <title>Can I do memory to memory DMA transfer in kinetis MCU using interrupt.</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Can-I-do-memory-to-memory-DMA-transfer-in-kinetis-MCU-using/m-p/236352#M1252</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How&amp;nbsp; can I do memory to memory DMA transfer using interrupt. May be in timer interrupt I would initiate the transfer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Prakash&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Feb 2014 16:19:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Can-I-do-memory-to-memory-DMA-transfer-in-kinetis-MCU-using/m-p/236352#M1252</guid>
      <dc:creator>prakashpatel</dc:creator>
      <dc:date>2014-02-14T16:19:53Z</dc:date>
    </item>
    <item>
      <title>Re: Can I do memory to memory DMA transfer in kinetis MCU using interrupt.</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Can-I-do-memory-to-memory-DMA-transfer-in-kinetis-MCU-using/m-p/236353#M1253</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, if you mean triggering&amp;nbsp; a DMA transfer by a timer or other interrupt flag event.&lt;/P&gt;&lt;P&gt;I recommend to use DMAChanne_LDD component. There is a property Hardware request that you can enable and select the source of event that triggers the transfer. For example FTM_C0_DMA_Request comes from channel 0 of the FTM0 timer.&lt;/P&gt;&lt;P&gt;If you select it, you also need to create a timer component that initializes the timer - you can do it for example with TimerUnit_LDD where you select FTM0, period&amp;nbsp; and setup channel 0 where where you select offset and enable the DMA request in Interrupts/DMA.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Petr Hradsky&lt;/P&gt;&lt;P&gt;Processor Expert Support Team&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Feb 2014 12:02:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Can-I-do-memory-to-memory-DMA-transfer-in-kinetis-MCU-using/m-p/236353#M1253</guid>
      <dc:creator>Petr_H</dc:creator>
      <dc:date>2014-02-26T12:02:39Z</dc:date>
    </item>
  </channel>
</rss>