<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Processor Expert Software中的主题 Re: How to run two debuggers at once</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/How-to-run-two-debuggers-at-once/m-p/236029#M1249</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for your quick reply Erich. Not using Eclipse. I'm using CodeWarrior Development Studio V5.9.0 and I my target boards both have MC9S08DZ32 micros. I do have dual monitors though (the only way to fly) :-) I did discover that I could connect to both debuggers from one session by selecting from the drop down menu you mentioned that shows which USB you are connected to and I can do it that way but man, what a process! I find myself constantly switching back and forth single stepping each. It's too tedious and time consuming. Much rather see 2 separate debug windows.&lt;/P&gt;&lt;P&gt;I appreciate your help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 24 Jan 2013 20:30:57 GMT</pubDate>
    <dc:creator>MikeM</dc:creator>
    <dc:date>2013-01-24T20:30:57Z</dc:date>
    <item>
      <title>How to run two debuggers at once</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/How-to-run-two-debuggers-at-once/m-p/236027#M1247</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a problem where it would be advantageous to run debuggers on two different devices at the same time. I have two P&amp;amp;E USB Multilink debuggers connected to two separate devices on an common CAN bus. I can run two instances of CodeWarrior but only one debugger at one time even though I can see both debuggers connected to two different USB ports and pick either one. However running one replaces the other so that they can't exist together.&lt;/P&gt;&lt;P&gt;Is it possible to run two debuggers at the same time on the same computer and if so how?&lt;/P&gt;&lt;P&gt;Thanks (I did search for this question)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Jan 2013 19:23:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/How-to-run-two-debuggers-at-once/m-p/236027#M1247</guid>
      <dc:creator>MikeM</dc:creator>
      <dc:date>2013-01-24T19:23:14Z</dc:date>
    </item>
    <item>
      <title>Re: How to run two debuggers at once</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/How-to-run-two-debuggers-at-once/m-p/236028#M1248</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;is this about Eclipse based MCU10? So yes, this is easily possible. One common way is to use the menu Window &amp;gt; New Window (see &lt;A href="http://mcuoneclipse.com/2012/02/29/go-multiply-and-detach-multiple-screens-with-eclipse/" title="http://mcuoneclipse.com/2012/02/29/go-multiply-and-detach-multiple-screens-with-eclipse/"&gt;Go, multiply and detach: Multiple Screens with Eclipse | MCU on Eclipse&lt;/A&gt;): this is especially useful if you have a dual monitor system: then you can debug one project in one window while debugging the other in the other main window.&lt;/P&gt;&lt;P&gt;That's my preferred way.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is possible as well to debug multiple boards/CPU's from one debug session. In that case you will have in the 'Debug' view/window the multiple cores, and you can switch between them.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The key point is that you need to tie the debug session/debug launch configuration to the correct USB Multilink: if you go into the debug settings, there is drop-down in the connection settings for P&amp;amp;E to select the multilink. I usually have a sticker with the USB ID on each multilink device to identify it (so I do not have to remember the number).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Jan 2013 19:49:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/How-to-run-two-debuggers-at-once/m-p/236028#M1248</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2013-01-24T19:49:28Z</dc:date>
    </item>
    <item>
      <title>Re: How to run two debuggers at once</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/How-to-run-two-debuggers-at-once/m-p/236029#M1249</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for your quick reply Erich. Not using Eclipse. I'm using CodeWarrior Development Studio V5.9.0 and I my target boards both have MC9S08DZ32 micros. I do have dual monitors though (the only way to fly) :-) I did discover that I could connect to both debuggers from one session by selecting from the drop down menu you mentioned that shows which USB you are connected to and I can do it that way but man, what a process! I find myself constantly switching back and forth single stepping each. It's too tedious and time consuming. Much rather see 2 separate debug windows.&lt;/P&gt;&lt;P&gt;I appreciate your help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Jan 2013 20:30:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/How-to-run-two-debuggers-at-once/m-p/236029#M1249</guid>
      <dc:creator>MikeM</dc:creator>
      <dc:date>2013-01-24T20:30:57Z</dc:date>
    </item>
  </channel>
</rss>