<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Processor Expert SoftwareのトピックK20FX512 LCF Alignment issue</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/K20FX512-LCF-Alignment-issue/m-p/234232#M1227</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have an application for the K20FX512 Kinetis processor that runs fine when debugging, however when I try to "Flash File To Target" via a J-Link jtag (KwikStik) I receive errors such as the following:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;CODE&gt;Downloading 0x00000049 bytes to be programmed at 0x00030034&amp;nbsp;&amp;nbsp; &lt;/CODE&gt;&lt;/P&gt;&lt;P&gt;&lt;CODE&gt;Executing program ....&amp;nbsp;&amp;nbsp; &lt;/CODE&gt;&lt;/P&gt;&lt;P&gt;&lt;CODE&gt;Error:&amp;nbsp; Program failed.&amp;nbsp;&amp;nbsp; Flash driver reports the following error(s):&amp;nbsp; Chip reported error during program. Please check that the sector you are programming is erased. &lt;/CODE&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;CODE&gt;Error: Program failed. Flash driver reports the following error(s):&amp;nbsp; Chip reported error during program. Please check that the sec tor you are programming is erased&lt;/CODE&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In looking into this I realized that it always fails on an address that is 4 byte aligned, but not 8 byte aligned. As the flash in K20FX requires 8 byte alignment I modified the PE generated lcf file to require 8 byte alignment. This resolves the issue. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My question is, is this the correct solution, or is there a setting in the hardware connection configuration I should be changing? If this is the correct solution, is there a way to prevent PE from overwriting the modified LCF?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; ~Dave&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 16 Sep 2013 16:34:02 GMT</pubDate>
    <dc:creator>davidschroeder</dc:creator>
    <dc:date>2013-09-16T16:34:02Z</dc:date>
    <item>
      <title>K20FX512 LCF Alignment issue</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/K20FX512-LCF-Alignment-issue/m-p/234232#M1227</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have an application for the K20FX512 Kinetis processor that runs fine when debugging, however when I try to "Flash File To Target" via a J-Link jtag (KwikStik) I receive errors such as the following:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;CODE&gt;Downloading 0x00000049 bytes to be programmed at 0x00030034&amp;nbsp;&amp;nbsp; &lt;/CODE&gt;&lt;/P&gt;&lt;P&gt;&lt;CODE&gt;Executing program ....&amp;nbsp;&amp;nbsp; &lt;/CODE&gt;&lt;/P&gt;&lt;P&gt;&lt;CODE&gt;Error:&amp;nbsp; Program failed.&amp;nbsp;&amp;nbsp; Flash driver reports the following error(s):&amp;nbsp; Chip reported error during program. Please check that the sector you are programming is erased. &lt;/CODE&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;CODE&gt;Error: Program failed. Flash driver reports the following error(s):&amp;nbsp; Chip reported error during program. Please check that the sec tor you are programming is erased&lt;/CODE&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In looking into this I realized that it always fails on an address that is 4 byte aligned, but not 8 byte aligned. As the flash in K20FX requires 8 byte alignment I modified the PE generated lcf file to require 8 byte alignment. This resolves the issue. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My question is, is this the correct solution, or is there a setting in the hardware connection configuration I should be changing? If this is the correct solution, is there a way to prevent PE from overwriting the modified LCF?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; ~Dave&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 Sep 2013 16:34:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/K20FX512-LCF-Alignment-issue/m-p/234232#M1227</guid>
      <dc:creator>davidschroeder</dc:creator>
      <dc:date>2013-09-16T16:34:02Z</dc:date>
    </item>
    <item>
      <title>Re: K20FX512 LCF Alignment issue</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/K20FX512-LCF-Alignment-issue/m-p/234233#M1228</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;you can disable generation of linker file on Build options tab in CPU component. Details attached. Regarding to the issue - could you please post here ProcessorExpert.pe file from your project in order to reproduce it on our side?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Vojtech Filip&lt;/P&gt;&lt;P&gt;Processor Expert Support Team&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Sep 2013 11:31:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/K20FX512-LCF-Alignment-issue/m-p/234233#M1228</guid>
      <dc:creator>vfilip</dc:creator>
      <dc:date>2013-09-17T11:31:49Z</dc:date>
    </item>
    <item>
      <title>Re: K20FX512 LCF Alignment issue</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/K20FX512-LCF-Alignment-issue/m-p/234234#M1229</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello David,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How is the project going? Any news? Please keep us posted, we'd like to know :smileywink:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best,&lt;/P&gt;&lt;P&gt;Monica.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Oct 2013 01:02:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/K20FX512-LCF-Alignment-issue/m-p/234234#M1229</guid>
      <dc:creator>Monica</dc:creator>
      <dc:date>2013-10-03T01:02:48Z</dc:date>
    </item>
    <item>
      <title>Re: Re: K20FX512 LCF Alignment issue</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/K20FX512-LCF-Alignment-issue/m-p/234235#M1230</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've been working on other projects and am just getting back to this one. Like I said in the original post, it works if I change the alignment to 8 bytes. I've attached the pe file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ~Dave&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 14 Oct 2013 15:57:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/K20FX512-LCF-Alignment-issue/m-p/234235#M1230</guid>
      <dc:creator>davidschroeder</dc:creator>
      <dc:date>2013-10-14T15:57:28Z</dc:date>
    </item>
  </channel>
</rss>