<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Processor Expert SoftwareのトピックDisable UART Rx Interrupt before Erase\Write Flash for PE App on KL15</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/Disable-UART-Rx-Interrupt-before-Erase-Write-Flash-for-PE-App-on/m-p/229460#M1182</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello:&lt;BR /&gt;The application i'm writing is built with the processor expert Serial_LDD module.&lt;BR /&gt;My problem could be solved by disabling the Serial UART interrupt service and using polling mode. However i thought it would be nice to use the rx interrupt with events.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Assuming a message could come in from the PC while erasing\writing to flash i have a couple of questions.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;1) Do i have to disable the UART Rx interrupt before Erasing\Writing to Flash to avoid rx interrupt firing during flash operation?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2) If yes to question 1. Is the best way to do this using the following macros generated by PE: UART0_PDD_EnableInterrupt\UART0_PDD_DisableInterrupt?&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; I found the UART0_PDD_EnableInterrupt macro at the bottom of the Serial_Init function that was generated by PE.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3) If yes to question 2. If a message did come in while erasing\writing flash would it be lost or is there a way to capture the complete message?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 10 Jan 2014 19:10:16 GMT</pubDate>
    <dc:creator>admin</dc:creator>
    <dc:date>2014-01-10T19:10:16Z</dc:date>
    <item>
      <title>Disable UART Rx Interrupt before Erase\Write Flash for PE App on KL15</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Disable-UART-Rx-Interrupt-before-Erase-Write-Flash-for-PE-App-on/m-p/229460#M1182</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello:&lt;BR /&gt;The application i'm writing is built with the processor expert Serial_LDD module.&lt;BR /&gt;My problem could be solved by disabling the Serial UART interrupt service and using polling mode. However i thought it would be nice to use the rx interrupt with events.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Assuming a message could come in from the PC while erasing\writing to flash i have a couple of questions.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;1) Do i have to disable the UART Rx interrupt before Erasing\Writing to Flash to avoid rx interrupt firing during flash operation?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2) If yes to question 1. Is the best way to do this using the following macros generated by PE: UART0_PDD_EnableInterrupt\UART0_PDD_DisableInterrupt?&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; I found the UART0_PDD_EnableInterrupt macro at the bottom of the Serial_Init function that was generated by PE.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3) If yes to question 2. If a message did come in while erasing\writing flash would it be lost or is there a way to capture the complete message?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Jan 2014 19:10:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Disable-UART-Rx-Interrupt-before-Erase-Write-Flash-for-PE-App-on/m-p/229460#M1182</guid>
      <dc:creator>admin</dc:creator>
      <dc:date>2014-01-10T19:10:16Z</dc:date>
    </item>
    <item>
      <title>Re: Disable UART Rx Interrupt before Erase\Write Flash for PE App on KL15</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/Disable-UART-Rx-Interrupt-before-Erase-Write-Flash-for-PE-App-on/m-p/229461#M1183</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;could you please provide more detail? Some demonstration project would be the best. Anyway you should be able to use Serial_LDD + Flash_LDD together in interrupt mode without any problem. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Vojtech Filip&lt;/P&gt;&lt;P&gt;Processor Expert Support Team&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Jan 2014 12:22:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/Disable-UART-Rx-Interrupt-before-Erase-Write-Flash-for-PE-App-on/m-p/229461#M1183</guid>
      <dc:creator>vfilip</dc:creator>
      <dc:date>2014-01-17T12:22:02Z</dc:date>
    </item>
  </channel>
</rss>