<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Processor Expert SoftwareのトピックRe: UART1 Baud setting in PE running on KL25 Freedom board problem</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/UART1-Baud-setting-in-PE-running-on-KL25-Freedom-board-problem/m-p/225543#M1136</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Erich,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am facing the same problem.&lt;/P&gt;&lt;P&gt;I am using&amp;nbsp; code warrior 10.3 for &lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=KL2x"&gt;KL25Z128&lt;/A&gt; controller.&lt;/P&gt;&lt;P&gt;I developed an application using UART1 on PTC4 And PTC3 pins.The micro controller has a crystal 8MHz and the PLL as PEE ( with Processor Expert ) at 96MHz with CoreClock at 48MHz and BusClock at 24MHz.&lt;/P&gt;&lt;P&gt;When i set baud rate 9600 for UART1 I found the output Baud Rate is half (4800) what I set in ProcessExpert Component.&lt;/P&gt;&lt;P&gt;Here my core clock to bus clock ratio is 1/2 and because of that my baud rate i (9600*(1/2))=4800.&lt;/P&gt;&lt;P&gt;If my core clock and bus clock ratio get is same it is get sets at 9600.&lt;/P&gt;&lt;P&gt;But if my core clock and bus clock ratio is changed what exact equation need to be apply?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Reg,&lt;/P&gt;&lt;P&gt;Amreen&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 04 Apr 2014 14:01:14 GMT</pubDate>
    <dc:creator>Embionics</dc:creator>
    <dc:date>2014-04-04T14:01:14Z</dc:date>
    <item>
      <title>UART1 Baud setting in PE running on KL25 Freedom board problem</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/UART1-Baud-setting-in-PE-running-on-KL25-Freedom-board-problem/m-p/225537#M1130</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have encountered a problem that when I use the UART1 on &lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=FRDM-KL25Z"&gt;KL25 Freedom Board&lt;/A&gt; on Pin18, Pin20 of connector J2 for Tx,Rx of UART1, I found the output Baud Rate is half what I set in ProcessExpert Component. For example, if I need 115200, I need to set it to 230400 in the Serial_LDD.&lt;/P&gt;&lt;P&gt;The CPU clock setting and the Serial_LDD settings are attached here.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/38296i91AB2D749A6923E6/image-size/large?v=v2&amp;amp;px=999" title="BaudProblem_ClkSetting.png" alt="BaudProblem_ClkSetting.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/38369i0413B700FB279C3D/image-size/large?v=v2&amp;amp;px=999" title="BaudProblem_UART1Setting.png" alt="BaudProblem_UART1Setting.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have checked it with oscilloscope and proved it by PC terminal. I am using CodeWarrior for MCU version 10.3&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope it's helpful to be fixed in the coming version of PE.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards'&lt;/P&gt;&lt;P&gt;Stephen Lau&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Jan 2013 02:22:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/UART1-Baud-setting-in-PE-running-on-KL25-Freedom-board-problem/m-p/225537#M1130</guid>
      <dc:creator>StephenLau</dc:creator>
      <dc:date>2013-01-16T02:22:01Z</dc:date>
    </item>
    <item>
      <title>Re: UART1 Baud setting in PE running on KL25 Freedom board problem</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/UART1-Baud-setting-in-PE-running-on-KL25-Freedom-board-problem/m-p/225538#M1131</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, I have found the same problem, and I have filed a ticket to get it fixed.&lt;/P&gt;&lt;P&gt;The issue is that Processor Expert thinks that the bus is being clocked at 48MHz. It is not taking into account that the bus clock divider on &lt;A href="http://www.freescale.com/webapp/sps/site/taxonomy.jsp?code=KINETIS_L_SERIES"&gt;L series&lt;/A&gt; is dividing down the Core clock, NOT the MCGOUTCLK that would be used on Kinetis K series.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Jan 2013 05:02:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/UART1-Baud-setting-in-PE-running-on-KL25-Freedom-board-problem/m-p/225538#M1131</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2013-01-16T05:02:24Z</dc:date>
    </item>
    <item>
      <title>Re: UART1 Baud setting in PE running on KL25 Freedom board problem</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/UART1-Baud-setting-in-PE-running-on-KL25-Freedom-board-problem/m-p/225539#M1132</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks. :smileyhappy:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Jan 2013 05:06:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/UART1-Baud-setting-in-PE-running-on-KL25-Freedom-board-problem/m-p/225539#M1132</guid>
      <dc:creator>StephenLau</dc:creator>
      <dc:date>2013-01-16T05:06:21Z</dc:date>
    </item>
    <item>
      <title>Re: UART1 Baud setting in PE running on KL25 Freedom board problem</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/UART1-Baud-setting-in-PE-running-on-KL25-Freedom-board-problem/m-p/225540#M1133</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;we are aware of this issue. It will be fixed in the upcoming update of CW V10.3. The problem is in our model, so the requested value is necessary multiply by two to get the correct output timing.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are sorry for inconvenience.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;best regards&lt;/P&gt;&lt;P&gt;Vojtech Filip&lt;/P&gt;&lt;P&gt;Processor Expert Support Team&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Jan 2013 07:27:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/UART1-Baud-setting-in-PE-running-on-KL25-Freedom-board-problem/m-p/225540#M1133</guid>
      <dc:creator>vfilip</dc:creator>
      <dc:date>2013-01-16T07:27:23Z</dc:date>
    </item>
    <item>
      <title>Re: UART1 Baud setting in PE running on KL25 Freedom board problem</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/UART1-Baud-setting-in-PE-running-on-KL25-Freedom-board-problem/m-p/225541#M1134</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am not sure if anybody has noticed. Just a tiny mistake in the documentation (&lt;EM&gt;user manual&lt;/EM&gt; and &lt;EM&gt;pin usage &amp;amp; pinout chart&lt;/EM&gt;)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The &lt;STRONG&gt;J2 20&lt;/STRONG&gt; should be &lt;STRONG&gt;PTE1&lt;/STRONG&gt; which is &lt;STRONG&gt;UART1_RX&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;and &lt;STRONG&gt;J2 18&lt;/STRONG&gt; should be &lt;STRONG&gt;PTE2&lt;/STRONG&gt; which is &lt;STRONG&gt;UART1_TX&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The quick reference card attached and the silkscreen on the bottom of the board are illustrated correctly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Feb 2013 02:04:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/UART1-Baud-setting-in-PE-running-on-KL25-Freedom-board-problem/m-p/225541#M1134</guid>
      <dc:creator>chiasyan</dc:creator>
      <dc:date>2013-02-21T02:04:30Z</dc:date>
    </item>
    <item>
      <title>Re: UART1 Baud setting in PE running on KL25 Freedom board problem</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/UART1-Baud-setting-in-PE-running-on-KL25-Freedom-board-problem/m-p/225542#M1135</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I was informed that this should be fixed in the next release of the documentation.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;best regards&lt;/P&gt;&lt;P&gt;Vojtech Filip&lt;/P&gt;&lt;P&gt;Processor Expert Support Team&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Feb 2013 07:51:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/UART1-Baud-setting-in-PE-running-on-KL25-Freedom-board-problem/m-p/225542#M1135</guid>
      <dc:creator>vfilip</dc:creator>
      <dc:date>2013-02-22T07:51:27Z</dc:date>
    </item>
    <item>
      <title>Re: UART1 Baud setting in PE running on KL25 Freedom board problem</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/UART1-Baud-setting-in-PE-running-on-KL25-Freedom-board-problem/m-p/225543#M1136</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Erich,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am facing the same problem.&lt;/P&gt;&lt;P&gt;I am using&amp;nbsp; code warrior 10.3 for &lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=KL2x"&gt;KL25Z128&lt;/A&gt; controller.&lt;/P&gt;&lt;P&gt;I developed an application using UART1 on PTC4 And PTC3 pins.The micro controller has a crystal 8MHz and the PLL as PEE ( with Processor Expert ) at 96MHz with CoreClock at 48MHz and BusClock at 24MHz.&lt;/P&gt;&lt;P&gt;When i set baud rate 9600 for UART1 I found the output Baud Rate is half (4800) what I set in ProcessExpert Component.&lt;/P&gt;&lt;P&gt;Here my core clock to bus clock ratio is 1/2 and because of that my baud rate i (9600*(1/2))=4800.&lt;/P&gt;&lt;P&gt;If my core clock and bus clock ratio get is same it is get sets at 9600.&lt;/P&gt;&lt;P&gt;But if my core clock and bus clock ratio is changed what exact equation need to be apply?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Reg,&lt;/P&gt;&lt;P&gt;Amreen&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Apr 2014 14:01:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/UART1-Baud-setting-in-PE-running-on-KL25-Freedom-board-problem/m-p/225543#M1136</guid>
      <dc:creator>Embionics</dc:creator>
      <dc:date>2014-04-04T14:01:14Z</dc:date>
    </item>
    <item>
      <title>Re: UART1 Baud setting in PE running on KL25 Freedom board problem</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/UART1-Baud-setting-in-PE-running-on-KL25-Freedom-board-problem/m-p/225544#M1137</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, this is a problem of MCU10.3 (see &lt;A href="http://mcuoneclipse.com/2013/02/17/be-aware-of-the-baud-problem/" title="http://mcuoneclipse.com/2013/02/17/be-aware-of-the-baud-problem/"&gt;Be Aware of the Baud Problem | MCU on Eclipse&lt;/A&gt;). I recommend that you verify/change the prescaler settings as outlined in above post, or switch to a later version of CodeWarrior. MCU V10.6 just came out.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Apr 2014 14:11:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/UART1-Baud-setting-in-PE-running-on-KL25-Freedom-board-problem/m-p/225544#M1137</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2014-04-04T14:11:27Z</dc:date>
    </item>
  </channel>
</rss>