<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: DMAChannel_LDD sections greyed out in Processor Expert Software</title>
    <link>https://community.nxp.com/t5/Processor-Expert-Software/DMAChannel-LDD-sections-greyed-out/m-p/225100#M1111</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Thank you for the feedback, it has been passed to the development team. I'm glad that you have been able to implement the solution that you needed.&lt;/P&gt;&lt;P&gt;The solution with Init components and direct access to the hardware will in most cases be faster and more effective than the higher level components (LDD) .&lt;/P&gt;&lt;P&gt;It's a price for having the general drivers that are not tailored for a specific task and are available on many (sometimes different) platforms (but I'm not saying that it should not be improved :-).&lt;/P&gt;&lt;P&gt;In cases like this, Init_xxx components accompanied with PDD macros are a good tool to achieve optimized code for a specific task.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Petr Hradsky&lt;/P&gt;&lt;P&gt;Processor Expert Support Team&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 26 Mar 2014 16:12:08 GMT</pubDate>
    <dc:creator>Petr_H</dc:creator>
    <dc:date>2014-03-26T16:12:08Z</dc:date>
    <item>
      <title>DMAChannel_LDD sections greyed out</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/DMAChannel-LDD-sections-greyed-out/m-p/225095#M1106</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm trying to set up SSI_LDD to use DMA, so it created DMAChannel_LDD subcomponents, but field that I need to change are greyed out, such as source start address.&amp;nbsp; Am I missing something or is there a problem with this component?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/42671iDD998B632AD23CC4/image-size/large?v=v2&amp;amp;px=999" title="DMA setting problem.png" alt="DMA setting problem.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Feb 2014 23:41:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/DMAChannel-LDD-sections-greyed-out/m-p/225095#M1106</guid>
      <dc:creator>bowerymarc</dc:creator>
      <dc:date>2014-02-11T23:41:00Z</dc:date>
    </item>
    <item>
      <title>Re: DMAChannel_LDD sections greyed out</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/DMAChannel-LDD-sections-greyed-out/m-p/225096#M1107</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;anyone home?&amp;nbsp; not sure how anyone could use this module with this bug present!?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Update: If I create a DMAChannel_LDD &lt;STRONG&gt;outside&lt;/STRONG&gt; of the SSI_LDD then those fields all work.&amp;nbsp; It's only when you enable DMA inside SSI_LDD and it creates subordinate DMAChannel_LDD's (I set one for each of the two TX pins)&amp;nbsp; Unfortunately there's no way to link that external one into the SSI_LDD.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/42806i7CFBE9B6AD0E76BE/image-size/large?v=v2&amp;amp;px=999" title="Audio0_TxDMA0 bugs.png" alt="Audio0_TxDMA0 bugs.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Feb 2014 22:02:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/DMAChannel-LDD-sections-greyed-out/m-p/225096#M1107</guid>
      <dc:creator>bowerymarc</dc:creator>
      <dc:date>2014-02-21T22:02:27Z</dc:date>
    </item>
    <item>
      <title>Re: DMAChannel_LDD sections greyed out</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/DMAChannel-LDD-sections-greyed-out/m-p/225097#M1108</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;generally SSI_LDD should behaves the same in all modes (polling, interrupts, DMA, etc...)&lt;/P&gt;&lt;P&gt;Run-time settings are pointer to user data and&amp;nbsp; number of requests count. The rest of settings is set according to configuration in SSI_LDD.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regarding Source transaction settings:&lt;/P&gt;&lt;P&gt;Start address - should be set in run-time by SendBlock method in SSI_LDD (for more details please see attached screen-shot).&lt;/P&gt;&lt;P&gt;Transaction count - is controlled by Watermark property in SSI_LDD.&lt;/P&gt;&lt;P&gt;Address adjustment - 4 is set due to SSI_LDD component correct functionality (This item is controlled by Data Type in SSI_LDD).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regarding Destination transaction settings:&lt;/P&gt;&lt;P&gt;Transaction count - is controlled by Watermark property in SSI_LDD.&lt;/P&gt;&lt;P&gt;Address adjustment - 0 is set due to SSI_LDD component correct functionality.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regarding Transfer transaction settings:&lt;/P&gt;&lt;P&gt;Transaction size - is controlled by Data Type in SSI_LDD.&lt;/P&gt;&lt;P&gt;Transaction count - is controlled by Watermark property in SSI_LDD.&lt;/P&gt;&lt;P&gt;Request count - should be set in run-time by SendBlock method in SSI_LDD (for more details please see attached screen-shot).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We will try improve hints in DMA_Channel component for next release of PEx.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Vojtech Filip&lt;/P&gt;&lt;P&gt;Processor Expert Support Team&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Feb 2014 10:40:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/DMAChannel-LDD-sections-greyed-out/m-p/225097#M1108</guid>
      <dc:creator>vfilip</dc:creator>
      <dc:date>2014-02-24T10:40:00Z</dc:date>
    </item>
    <item>
      <title>Re: DMAChannel_LDD sections greyed out</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/DMAChannel-LDD-sections-greyed-out/m-p/225098#M1109</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Vojtech,&lt;/P&gt;&lt;P&gt;You forgot the screen shot....&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Let me tell you what I'm trying to do.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have 8 channels of audio, let's say each sample is an int_32.&amp;nbsp; They are organize in memory to make signal processing easy:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P class="p1"&gt;&lt;SPAN class="s1"&gt;&lt;STRONG&gt;#define&lt;/STRONG&gt;&lt;/SPAN&gt; AUDIO_CHANPEROUT 4 &lt;SPAN class="s2"&gt;///&amp;lt; i4s format&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="p2"&gt;&lt;SPAN class="s1"&gt;&lt;STRONG&gt;#define&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;SPAN class="s3"&gt; AUDIO_NOUTS 2 &lt;/SPAN&gt;///&amp;lt; 2 TX outputs per SAI&lt;/P&gt;&lt;P class="p1"&gt;&lt;SPAN class="s4"&gt;&lt;STRONG&gt;#define&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;SPAN class="s5"&gt; AUDIO_NOUTPUTCHANNELS AUDIO_CHANPEROUT * AUDIO_NOUTS&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="p2"&gt;&lt;SPAN class="s1"&gt;&lt;STRONG&gt;#define&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;SPAN class="s3"&gt; AUDIO_OUTPUTBUFSIZE 16 &lt;/SPAN&gt;///&amp;lt; samples per channel for audio output buffer&lt;/P&gt;&lt;P class="p2"&gt;&lt;/P&gt;&lt;P class="p2"&gt;&lt;SPAN class="s3"&gt;int32_t&lt;/SPAN&gt; audioBuf[AUDIO_NOUTPUTCHANNELS][2][AUDIO_OUTPUTBUFSIZE];&lt;/P&gt;&lt;P class="p2"&gt;&lt;/P&gt;&lt;P class="p2"&gt;I'm setting each of the two TX outputs to i4s format (2 channels per stream).&amp;nbsp; Tx0 outputs channel 1-4, Tx1 outputs channel 5-8.&lt;/P&gt;&lt;P class="p2"&gt;&lt;/P&gt;&lt;P class="p2"&gt;Once the program starts, the audio *must* run continuously.&amp;nbsp; This is the usual case with audio (except the case of low power sleeping, we'll ignore that for now).&lt;/P&gt;&lt;P class="p2"&gt;&lt;/P&gt;&lt;P class="p2"&gt;So the indices for the buffer are, in order:&lt;/P&gt;&lt;P class="p2"&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;- output channel 0-7&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="p2"&gt;- pingpong = 0 or 1&lt;/P&gt;&lt;P class="p2"&gt;- sample number 0-16&lt;/P&gt;&lt;P class="p2"&gt;&lt;/P&gt;&lt;P class="p2"&gt;So when I have a DSP loop, I process 16 samples of one channel, then go to the next.&amp;nbsp; Most efficient way to do it in general.&amp;nbsp; That would happen in the "halfway there" DMA interrupt, which would also increment (mod 2) the pingpong index.&lt;/P&gt;&lt;P class="p2"&gt;&lt;/P&gt;&lt;P class="p2"&gt;I let the DMA controller do the hard work.&amp;nbsp; I set the FIFO request in the SSI to 4.&amp;nbsp; So then the DMA will get 4 words in 1 minor loop, which is the 4 channels of one sample for one output.&amp;nbsp; So the minor loop has to skip by 32 samples each time to get to the next channel.&amp;nbsp; Then, it has to skip 4 whole channels to get to the next sample, as those channels are handled by the other Tx output.&amp;nbsp; So that's the adjustment after the minor loop.&amp;nbsp; Then, after the major loop, do another adjustment to reset the address back to the beginning, and chain the DMA to itself.&amp;nbsp; Then the processor never has to get involved once it starts.&lt;/P&gt;&lt;P class="p2"&gt;&lt;/P&gt;&lt;P class="p2"&gt;So in this case, I believe the DMA settings I want are thus:&lt;/P&gt;&lt;P class="p2"&gt;&lt;/P&gt;&lt;P class="p2"&gt;DMA0:&lt;/P&gt;&lt;P class="p2"&gt;&lt;/P&gt;&lt;P class="p2"&gt;Source:&lt;/P&gt;&lt;P class="p2"&gt;start address: &amp;amp;audioBuf[0][0][0]&lt;/P&gt;&lt;P class="p2"&gt;transaction size: 32-bits&lt;/P&gt;&lt;P class="p2"&gt;address adjustment: 128&lt;/P&gt;&lt;P class="p2"&gt;&lt;/P&gt;&lt;P class="p2"&gt;Destination:&lt;/P&gt;&lt;P class="p2"&gt;start address: (LDD_DMA_TAddress)(I2S_PDD_GetTxDataChannelRegAddress(I2S0_BASE_PTR,0U))&lt;/P&gt;&lt;P class="p2"&gt;transaction size: 32-bits&lt;/P&gt;&lt;P class="p2"&gt;address adjustment: 0&lt;/P&gt;&lt;P class="p2"&gt;&lt;/P&gt;&lt;P class="p2"&gt;Transfer Settings:&lt;/P&gt;&lt;P class="p2"&gt;transactions count: 4&lt;/P&gt;&lt;P class="p2"&gt;request count: 32&lt;/P&gt;&lt;P class="p2"&gt;&lt;/P&gt;&lt;P class="p2"&gt;After request complete actions:&lt;/P&gt;&lt;P class="p2"&gt;source address adjustment: -508 (skip back to beginning but one sample ahead 512-4)&lt;/P&gt;&lt;P class="p2"&gt;&lt;/P&gt;&lt;P class="p2"&gt;After transfer complete actions:&lt;/P&gt;&lt;P class="p2"&gt;channel linking: enabled, DMA0 (same channel)&lt;/P&gt;&lt;P class="p2"&gt;source address adjustment: -636 (skip back to beginning 512+128-4)&lt;/P&gt;&lt;P class="p2"&gt;&lt;/P&gt;&lt;P class="p2"&gt;DMA1:&lt;/P&gt;&lt;P class="p2"&gt;&lt;/P&gt;&lt;P class="p2"&gt;Source:&lt;/P&gt;&lt;P class="p2"&gt;start address: &amp;amp;audioBuf[4][0][0]&lt;/P&gt;&lt;P class="p2"&gt;transaction size: 32-bits&lt;/P&gt;&lt;P class="p2"&gt;address adjustment: 128&lt;/P&gt;&lt;P class="p2"&gt;&lt;/P&gt;&lt;P class="p2"&gt;Destination:&lt;/P&gt;&lt;P class="p2"&gt;start address: (LDD_DMA_TAddress)(I2S_PDD_GetTxDataChannelRegAddress(I2S0_BASE_PTR,1U))&lt;/P&gt;&lt;P class="p2"&gt;transaction size: 32-bits&lt;/P&gt;&lt;P class="p2"&gt;address adjustment: 0&lt;/P&gt;&lt;P class="p2"&gt;&lt;/P&gt;&lt;P class="p2"&gt;Transfer Settings:&lt;/P&gt;&lt;P class="p2"&gt;transactions count: 4&lt;/P&gt;&lt;P class="p2"&gt;request count: 32&lt;/P&gt;&lt;P class="p2"&gt;&lt;/P&gt;&lt;P class="p2"&gt;After request complete actions:&lt;/P&gt;&lt;P class="p2"&gt;source address adjustment: -508&lt;/P&gt;&lt;P class="p2"&gt;&lt;/P&gt;&lt;P class="p2"&gt;After transfer complete actions:&lt;/P&gt;&lt;P class="p2"&gt;channel linking: enabled, DMA1 (same channel)&lt;/P&gt;&lt;P class="p2"&gt;source address adjustment: -636&lt;/P&gt;&lt;P class="p2"&gt;&lt;/P&gt;&lt;P class="p2"&gt;&lt;/P&gt;&lt;P class="p2"&gt;... if this makes sense, then you can see why I want to access those greyed out fields.&lt;/P&gt;&lt;P class="p2"&gt;&lt;/P&gt;&lt;P class="p2"&gt;NOTE: I edited this with updated values thanks to source code in Earl Goodrich's post here: &lt;A href="https://community.nxp.com/message/82190"&gt;Re: is there any demo code for using I2S?&lt;/A&gt; &lt;/P&gt;&lt;P class="p2"&gt;I implemented this and tested it by:&lt;/P&gt;&lt;P class="p2"&gt;1. created SSI_LDD and enabled DMA&lt;/P&gt;&lt;P class="p2"&gt;2. generated PE code&lt;/P&gt;&lt;P class="p2"&gt;3. disabled generating PE code for the audio SSI_LDD module&lt;/P&gt;&lt;P class="p2"&gt;4. once disabled, then disable DMA in the SSI_LDD interface and save (to avoid conflicts with below)&lt;/P&gt;&lt;P class="p2"&gt;5. deleted the DMA source files&lt;/P&gt;&lt;P class="p2"&gt;6. created two DMAChannel_LDD components (outside of SSI_LDD)&lt;/P&gt;&lt;P class="p2"&gt;7. renamed them the same name as the deleted DMA components&lt;/P&gt;&lt;P class="p2"&gt;8. made sure I generate the needed methods&lt;/P&gt;&lt;P class="p2"&gt;9. generate the PE code of these&lt;/P&gt;&lt;P class="p2"&gt;10. disable generating the PE code after generating once&lt;/P&gt;&lt;P class="p2"&gt;11. delete the extra events in Events.c (since the ones I want are in Audio0.c)&lt;/P&gt;&lt;P class="p2"&gt;12. added the 'halfway' interrupt flag and other bug fixes noted in other of my recent posts&lt;/P&gt;&lt;P class="p2"&gt;Its running and seems to be working fine.&amp;nbsp; Setting the bus throttle-back to 8 cycles in the two DMA engines seems to have a positive effect overall.&lt;/P&gt;&lt;P class="p2"&gt;In sum, this setup should be allowed in the component, as it's usual way to do audio.&lt;/P&gt;&lt;P class="p2"&gt;Best,&lt;BR /&gt;Marc&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Feb 2014 21:37:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/DMAChannel-LDD-sections-greyed-out/m-p/225098#M1109</guid>
      <dc:creator>bowerymarc</dc:creator>
      <dc:date>2014-02-24T21:37:13Z</dc:date>
    </item>
    <item>
      <title>Re: DMAChannel_LDD sections greyed out</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/DMAChannel-LDD-sections-greyed-out/m-p/225099#M1110</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;UPDATE:&amp;nbsp; now that I understand the DMA engine a little better, I realize I can't do what I want with the setup above.&amp;nbsp; I was getting very weird response.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It also showed another bug - you can't assign two DMA channels to the same source, or else results are unpredictable.&amp;nbsp; The PE component doesn't catch that.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Turns out I can do what I wanted (8 non-interleaved pingpong buffers to two I4S streams), using 8 DMA channels and the PIT.&amp;nbsp; So actually blowing off these PE drivers and simply using the Init_I2S, Init_DMA, and Init_PIT and literally one other line of code to enable the I2S after everything was set up, and it's working 100%, with much less code (the Init_xxx drivers are quite lean) and way less confusion.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I suggest the PE team write some actual working tests for the Audio_LDD driver - you'll find the defaults are not at all helpful.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Mar 2014 18:29:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/DMAChannel-LDD-sections-greyed-out/m-p/225099#M1110</guid>
      <dc:creator>bowerymarc</dc:creator>
      <dc:date>2014-03-04T18:29:02Z</dc:date>
    </item>
    <item>
      <title>Re: DMAChannel_LDD sections greyed out</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/DMAChannel-LDD-sections-greyed-out/m-p/225100#M1111</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Thank you for the feedback, it has been passed to the development team. I'm glad that you have been able to implement the solution that you needed.&lt;/P&gt;&lt;P&gt;The solution with Init components and direct access to the hardware will in most cases be faster and more effective than the higher level components (LDD) .&lt;/P&gt;&lt;P&gt;It's a price for having the general drivers that are not tailored for a specific task and are available on many (sometimes different) platforms (but I'm not saying that it should not be improved :-).&lt;/P&gt;&lt;P&gt;In cases like this, Init_xxx components accompanied with PDD macros are a good tool to achieve optimized code for a specific task.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Petr Hradsky&lt;/P&gt;&lt;P&gt;Processor Expert Support Team&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Mar 2014 16:12:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/DMAChannel-LDD-sections-greyed-out/m-p/225100#M1111</guid>
      <dc:creator>Petr_H</dc:creator>
      <dc:date>2014-03-26T16:12:08Z</dc:date>
    </item>
    <item>
      <title>Re: DMAChannel_LDD sections greyed out</title>
      <link>https://community.nxp.com/t5/Processor-Expert-Software/DMAChannel-LDD-sections-greyed-out/m-p/225101#M1112</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Well in this case, the design pattern for the &lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; font-size: 12px;"&gt;SSI_LDD&lt;/SPAN&gt; is not appropriate for the peripheral's intended use.&amp;nbsp;&amp;nbsp; If your team disagrees, I would like to see them produce a working example - let's say, something simple like streaming audio in, and doing some DSP for example attenuation based on the pot position on the TWR board, and then stream back out, on the TWR-K60F120M board.&amp;nbsp; I don't think it's possible using that component as it is.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Mar 2014 06:52:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Processor-Expert-Software/DMAChannel-LDD-sections-greyed-out/m-p/225101#M1112</guid>
      <dc:creator>bowerymarc</dc:creator>
      <dc:date>2014-03-27T06:52:17Z</dc:date>
    </item>
  </channel>
</rss>