<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>P-Series中的主题 Re: Linux boot hanging and kernel panic with SMP enabled</title>
    <link>https://community.nxp.com/t5/P-Series/Linux-boot-hanging-and-kernel-panic-with-SMP-enabled/m-p/276599#M826</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Thank you for your comment.&lt;/P&gt;&lt;P&gt;Yes. I&amp;nbsp; use Freescale LTIB. When I enable SMP (so the value is Y) in kernel configuration, I put&amp;nbsp; the number of CPUs equal to 2. When I disable it, the line to select the number of CPUs will not be there. In the latter case, the built uImage works fine.&amp;nbsp; As I explained, I can also build the Linux with SMP (2 CPUs) but pass "-nosmp" in U-boot boot args. It works fine. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Arash&lt;/P&gt;&lt;P&gt;&lt;BR /&gt; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 19 Jul 2013 12:37:50 GMT</pubDate>
    <dc:creator>arashaz_</dc:creator>
    <dc:date>2013-07-19T12:37:50Z</dc:date>
    <item>
      <title>Linux boot hanging and kernel panic with SMP enabled</title>
      <link>https://community.nxp.com/t5/P-Series/Linux-boot-hanging-and-kernel-panic-with-SMP-enabled/m-p/276597#M824</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear All,&lt;BR /&gt;I have a strange problem regarding synchronous multiprocessing (SMP) with a&lt;BR /&gt;P1020 compatible board and I appreciate if could advise me.&amp;nbsp; While booting&lt;BR /&gt;Linux, if I pass "-nosmp" as a boot argument, it works fine.&amp;nbsp; Enabling the SMP&lt;BR /&gt;(removing the -nosmp"), Linux crashes and does not boot. Note that when it&lt;BR /&gt;crashes, the kernel log appears somehow randomly (find some of them below). Most of the time,&amp;nbsp; it reports a "Data Cache Parity Error" or "Data Cache Push Parity Error" and sometimes "Unable to handle kernel paging request for instruction fetch" and “Unable to handle kernel paging request for data at address...”. In some cases, it even halts with no error message (just hangs up in the middle of the boot). So, I guess that the error can not be related&lt;BR /&gt;to one of the kernel drivers which are being loaded one by one.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Since the problem has a random nature, I even tried putting a big fan on the board, using a more strong power supply, using different Linux images with&lt;BR /&gt;different boot arguments such as &lt;EM&gt;-noapic&lt;/EM&gt; , &lt;EM&gt;-nomce&lt;/EM&gt;, ... None of them solved the problem.&lt;/P&gt;&lt;P&gt;Any comment is appreciated. &lt;/P&gt;&lt;P&gt;&lt;BR /&gt; &lt;SPAN style="font-size: 8pt;"&gt;Unable to handle kernel paging request for instruction fetch&amp;nbsp; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 8pt;"&gt;Faulting instruction address: 0x00000000&amp;nbsp; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 8pt;"&gt;Oops: Kernel access of bad area, sig: 11 [#1]&amp;nbsp; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 8pt;"&gt;SMP NR_CPUS=2 P1020 RDB &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 8pt;"&gt;Modules linked in: &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 8pt;"&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 8pt;"&gt; Machine check in kernel mode.&amp;nbsp; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 8pt;"&gt;Caused by (from MCSR=20000000): Data Cache Push Parity Error&amp;nbsp; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 8pt;"&gt;Oops: Machine check, sig: 7 [#2]&amp;nbsp; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 8pt;"&gt;SMP NR_CPUS=2 P1020 RDB&amp;nbsp; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 8pt;"&gt;Modules linked in: &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 8pt;"&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 8pt;"&gt; &lt;/SPAN&gt;&lt;SPAN style="font-size: 8pt;"&gt;Oops: Exception in kernel mode, sig: 4 [#1]&amp;nbsp; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 8pt;"&gt;SMP NR_CPUS=2 P1020 RDB&amp;nbsp; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 8pt;"&gt;Modules linked in: &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 8pt;"&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 8pt;"&gt; &lt;/SPAN&gt;&lt;SPAN style="font-size: 8pt;"&gt;Machine check in kernel mode.&amp;nbsp; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 8pt;"&gt;Caused by (from MCSR=20000000): Data Cache Push Parity Error&amp;nbsp; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 8pt;"&gt;Oops: Machine check, sig: 7 [#2]&amp;nbsp; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 8pt;"&gt;SMP NR_CPUS=2 P1020 RDB&amp;nbsp; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 8pt;"&gt;Modules linked in: &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 8pt;"&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 8pt;"&gt;Fixing recursive fault but reboot is needed! &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 8pt;"&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 8pt;"&gt; Unable to handle kernel paging request for instruction fetch&amp;nbsp; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 8pt;"&gt;Faulting instruction address: 0x00000000&amp;nbsp; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 8pt;"&gt;Oops: Kernel access of bad area, sig: 11 [#1]&amp;nbsp; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 8pt;"&gt;SMP NR_CPUS=2 P1020 RDB&amp;nbsp; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 8pt;"&gt;Modules linked in: &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 8pt;"&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 8pt;"&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 8pt;"&gt;Unable to handle kernel paging request for data at address 0x81a403b0&amp;nbsp; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 8pt;"&gt;Faulting instruction address: 0xc01d7d88&amp;nbsp; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 8pt;"&gt;Oops: Kernel access of bad area, sig: 11 [#1]&amp;nbsp; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 8pt;"&gt;SMP NR_CPUS=2 P1020 RDB &lt;/SPAN&gt; &lt;/P&gt;&lt;P&gt;&lt;BR /&gt; &lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Jul 2013 22:36:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Linux-boot-hanging-and-kernel-panic-with-SMP-enabled/m-p/276597#M824</guid>
      <dc:creator>arashaz_</dc:creator>
      <dc:date>2013-07-16T22:36:43Z</dc:date>
    </item>
    <item>
      <title>Re: Linux boot hanging and kernel panic with SMP enabled</title>
      <link>https://community.nxp.com/t5/P-Series/Linux-boot-hanging-and-kernel-panic-with-SMP-enabled/m-p/276598#M825</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;See below technical support comment:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you use Freescale SDK on the P1020 board?&lt;/P&gt;&lt;P&gt;What is value of the CONFIG_SMP variable in Linux kernel?&lt;/P&gt;&lt;P&gt;There is the following information about this parameter in the Linux kernel:&lt;/P&gt;&lt;P&gt;CONFIG_SMP: &lt;/P&gt;&lt;P&gt;This enables support for systems with more than one CPU. If you have a system with only one CPU, say N. If you have a system with more than one CPU, say Y. Note that the kernel does not currently support SMP machines with 603/603e/603ev or PPC750 ("G3") processors since they have inadequate hardware support for multiprocessor operation. &lt;/P&gt;&lt;P&gt;If you say N here, the kernel will run on single and multiprocessor machines, but will use only one CPU of a multiprocessor machine. If you say Y here, the kernel will run on single-processor machines. On a single-processor machine, the kernel will run faster if you say N here. &lt;/P&gt;&lt;P&gt;If you don't know what to do here, say N.&lt;/P&gt;&lt;P&gt;Symbol: SMP [=y]&lt;/P&gt;&lt;P&gt;Type : boolean&lt;/P&gt;&lt;P&gt;Prompt: Symmetric multi-processing support Defined at arch/powerpc/platforms/Kconfig.cputype:427&lt;/P&gt;&lt;P&gt;Depends on: PPC_BOOK3S [=n] || PPC_BOOK3E [=n] || FSL_BOOKE [=y] || PPC_47x [=n]&lt;/P&gt;&lt;P&gt;Location: &lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;SPAN lang="EN-US" style="font-size: 10.5pt; font-family: 'Calibri','sans-serif';"&gt; -&amp;gt; Processor support&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Jul 2013 09:30:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Linux-boot-hanging-and-kernel-panic-with-SMP-enabled/m-p/276598#M825</guid>
      <dc:creator>lunminliang</dc:creator>
      <dc:date>2013-07-18T09:30:51Z</dc:date>
    </item>
    <item>
      <title>Re: Linux boot hanging and kernel panic with SMP enabled</title>
      <link>https://community.nxp.com/t5/P-Series/Linux-boot-hanging-and-kernel-panic-with-SMP-enabled/m-p/276599#M826</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Thank you for your comment.&lt;/P&gt;&lt;P&gt;Yes. I&amp;nbsp; use Freescale LTIB. When I enable SMP (so the value is Y) in kernel configuration, I put&amp;nbsp; the number of CPUs equal to 2. When I disable it, the line to select the number of CPUs will not be there. In the latter case, the built uImage works fine.&amp;nbsp; As I explained, I can also build the Linux with SMP (2 CPUs) but pass "-nosmp" in U-boot boot args. It works fine. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Arash&lt;/P&gt;&lt;P&gt;&lt;BR /&gt; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Jul 2013 12:37:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Linux-boot-hanging-and-kernel-panic-with-SMP-enabled/m-p/276599#M826</guid>
      <dc:creator>arashaz_</dc:creator>
      <dc:date>2013-07-19T12:37:50Z</dc:date>
    </item>
    <item>
      <title>Re: Linux boot hanging and kernel panic with SMP enabled</title>
      <link>https://community.nxp.com/t5/P-Series/Linux-boot-hanging-and-kernel-panic-with-SMP-enabled/m-p/276600#M827</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Arash, what is the kernel version you are running there ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Jul 2013 15:06:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Linux-boot-hanging-and-kernel-panic-with-SMP-enabled/m-p/276600#M827</guid>
      <dc:creator>sinanakman</dc:creator>
      <dc:date>2013-07-19T15:06:27Z</dc:date>
    </item>
    <item>
      <title>Re: Linux boot hanging and kernel panic with SMP enabled</title>
      <link>https://community.nxp.com/t5/P-Series/Linux-boot-hanging-and-kernel-panic-with-SMP-enabled/m-p/276601#M828</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;The default version used by P1020WLAN Rev. D. LTIB, which is 2.6.32 (or 34). Sorry if I could not check 32 or 34 because I am out of office now. I will let you know.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Cheers,&lt;/P&gt;&lt;P&gt;Arash&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Jul 2013 19:17:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Linux-boot-hanging-and-kernel-panic-with-SMP-enabled/m-p/276601#M828</guid>
      <dc:creator>arashaz_</dc:creator>
      <dc:date>2013-07-19T19:17:10Z</dc:date>
    </item>
    <item>
      <title>Re: Linux boot hanging and kernel panic with SMP enabled</title>
      <link>https://community.nxp.com/t5/P-Series/Linux-boot-hanging-and-kernel-panic-with-SMP-enabled/m-p/276602#M829</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;The version is 2.6.32.&lt;/P&gt;&lt;P&gt;Arash&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Jul 2013 18:16:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Linux-boot-hanging-and-kernel-panic-with-SMP-enabled/m-p/276602#M829</guid>
      <dc:creator>arashaz_</dc:creator>
      <dc:date>2013-07-23T18:16:05Z</dc:date>
    </item>
  </channel>
</rss>