<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>P-SeriesのトピックRe: P2020RDB reference board booting</title>
    <link>https://community.nxp.com/t5/P-Series/P2020RDB-reference-board-booting/m-p/275643#M805</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It is not clear how exactly (U-Boot log) the Flash was programmed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt; After writing the image, and flipping SW3[7], we only get a steady &lt;/P&gt;&lt;P&gt;&amp;gt; power LED, and the two eTSEC2 LED rapidly blinking.&lt;/P&gt;&lt;P&gt;Why SW3[7]?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt; The switch information references the upper 4 sectors or middle 4 sectors. &lt;/P&gt;&lt;P&gt;&amp;gt; Can someone clarify these addresses?&lt;/P&gt;&lt;P&gt;"middle" is a typo - should be "low".&lt;/P&gt;&lt;P&gt;Please refer to the P2020RDB-PCA Specification, 5.1 NOR Flash Memory.&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 27 Apr 2013 08:41:51 GMT</pubDate>
    <dc:creator>lunminliang</dc:creator>
    <dc:date>2013-04-27T08:41:51Z</dc:date>
    <item>
      <title>P2020RDB reference board booting</title>
      <link>https://community.nxp.com/t5/P-Series/P2020RDB-reference-board-booting/m-p/275642#M804</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We bought a P2020RDB, which boots successfully to the Linux distro installed on the SD card.&amp;nbsp; However, we are now trying to install a VxWorks boot loader to the other part of the NOR flash.&amp;nbsp; After writing the image, and flipping SW3[7], we only get a steady power LED, and the two eTSEC2 LED rapidly blinking.&amp;nbsp; I would assume that this indicates a specific error, but can't find it anywhere in the documentation.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A few other potential issues with this:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The board docs indicate that the upper bank of the NOR flash starts at 0xEFF80000 and the lower bank at 0xEF780000.&amp;nbsp; The switch information references the upper 4 sectors or middle 4 sectors.&amp;nbsp; Can someone clarify these addresses?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;VxWorks says to copy the boot loader starting at address 0xEF700000, which wouldn't seem to be correct?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Apr 2013 21:00:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P2020RDB-reference-board-booting/m-p/275642#M804</guid>
      <dc:creator>cwrstl</dc:creator>
      <dc:date>2013-04-18T21:00:59Z</dc:date>
    </item>
    <item>
      <title>Re: P2020RDB reference board booting</title>
      <link>https://community.nxp.com/t5/P-Series/P2020RDB-reference-board-booting/m-p/275643#M805</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It is not clear how exactly (U-Boot log) the Flash was programmed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt; After writing the image, and flipping SW3[7], we only get a steady &lt;/P&gt;&lt;P&gt;&amp;gt; power LED, and the two eTSEC2 LED rapidly blinking.&lt;/P&gt;&lt;P&gt;Why SW3[7]?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt; The switch information references the upper 4 sectors or middle 4 sectors. &lt;/P&gt;&lt;P&gt;&amp;gt; Can someone clarify these addresses?&lt;/P&gt;&lt;P&gt;"middle" is a typo - should be "low".&lt;/P&gt;&lt;P&gt;Please refer to the P2020RDB-PCA Specification, 5.1 NOR Flash Memory.&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 27 Apr 2013 08:41:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P2020RDB-reference-board-booting/m-p/275643#M805</guid>
      <dc:creator>lunminliang</dc:creator>
      <dc:date>2013-04-27T08:41:51Z</dc:date>
    </item>
    <item>
      <title>Re: P2020RDB reference board booting</title>
      <link>https://community.nxp.com/t5/P-Series/P2020RDB-reference-board-booting/m-p/275644#M806</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;SW3[7] means POR cfg_boot_seq[1], it should be ON (Disables boot sequencer). If you switch to OFF and board will always reboot.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Jun 2013 06:55:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P2020RDB-reference-board-booting/m-p/275644#M806</guid>
      <dc:creator>paulgan</dc:creator>
      <dc:date>2013-06-21T06:55:19Z</dc:date>
    </item>
    <item>
      <title>Re: P2020RDB reference board booting</title>
      <link>https://community.nxp.com/t5/P-Series/P2020RDB-reference-board-booting/m-p/275645#M807</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I suspect those addresses given are meant to be the place to write U-Boot for booting from a particular bank -- not the actual start of the bank.&amp;nbsp; Boot images go at the end of flash (as seen after the address is transformed based on the selected bank).&amp;nbsp; If VxWorks is larger than U-Boot, then it will go at a lower address.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Jun 2013 17:03:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P2020RDB-reference-board-booting/m-p/275645#M807</guid>
      <dc:creator>scottwood</dc:creator>
      <dc:date>2013-06-26T17:03:39Z</dc:date>
    </item>
  </channel>
</rss>