<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>P-SeriesのトピックP1022DS DIU interrupt</title>
    <link>https://community.nxp.com/t5/P-Series/P1022DS-DIU-interrupt/m-p/273382#M795</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear sir,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I want to use DIU interrupt,but I do not know the meaning of the Vsync interrupt,the underrun interrupt,and the lines before Vsync interrupt.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 20 Dec 2013 07:20:44 GMT</pubDate>
    <dc:creator>hudi</dc:creator>
    <dc:date>2013-12-20T07:20:44Z</dc:date>
    <item>
      <title>P1022DS DIU interrupt</title>
      <link>https://community.nxp.com/t5/P-Series/P1022DS-DIU-interrupt/m-p/273382#M795</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear sir,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I want to use DIU interrupt,but I do not know the meaning of the Vsync interrupt,the underrun interrupt,and the lines before Vsync interrupt.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Dec 2013 07:20:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P1022DS-DIU-interrupt/m-p/273382#M795</guid>
      <dc:creator>hudi</dc:creator>
      <dc:date>2013-12-20T07:20:44Z</dc:date>
    </item>
    <item>
      <title>Re: P1022DS DIU interrupt</title>
      <link>https://community.nxp.com/t5/P-Series/P1022DS-DIU-interrupt/m-p/273383#M796</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; font-family: 'Courier New';"&gt;For VSYNC and LS_BF_VS interrupts, please refer to the Section 9.5.3 of the P1022 Reference Manual:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; font-family: 'Courier New';"&gt;If enabled, the VSYNC status bit will always be asserted with the first vsync pulse cycle. With this interrupt, the host can always observe the beginning of a new frame. Beside this, another interrupt, the LS_BF_VS (lines before vsync) can be used to set a deadline for the host to program the pointers for the current next frame. This interrupt is asserted at user-specified lines (set by the LS_BF_VS threshold, Section 9.3.17, “THRESHOLDS Register”) before the vertical front porch (FP_V). The host can program the pointer registers after it detects the LS_BF_VS interrupt. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; font-family: 'Courier New';"&gt;Figure Figure 9-36 shows a diagram on how these two interrupts can be used to synchronize the host and the DIU.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; font-family: 'Courier New';"&gt;UNDRUN interrupt.Under run exception interrupt is asserted when display needs data and output buffer filling is lower than or equal to the OUT_BUF_LOW threshold. See please the Section 9.5.5&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Dec 2013 09:45:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P1022DS-DIU-interrupt/m-p/273383#M796</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2013-12-20T09:45:28Z</dc:date>
    </item>
  </channel>
</rss>