<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>P-SeriesのトピックRe: P1022 Incorrect i2c clock frequency</title>
    <link>https://community.nxp.com/t5/P-Series/P1022-Incorrect-i2c-clock-frequency/m-p/1697468#M5167</link>
    <description>&lt;P&gt;hi,&lt;/P&gt;&lt;P&gt;Yes I have consulted that section and confirmed that everything is being computed correctly, at least according to what the kernel messages say.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;But as I mentioned, the reported set frequency does not match the measured frequency with the oscilloscope&lt;/P&gt;</description>
    <pubDate>Wed, 02 Aug 2023 09:39:40 GMT</pubDate>
    <dc:creator>rro</dc:creator>
    <dc:date>2023-08-02T09:39:40Z</dc:date>
    <item>
      <title>P1022 Incorrect i2c clock frequency</title>
      <link>https://community.nxp.com/t5/P-Series/P1022-Incorrect-i2c-clock-frequency/m-p/1692978#M5159</link>
      <description>&lt;P&gt;We are configuring our i2c clock-frequency to be 100,000 kHz, but are measuring just about 2x that with the oscilloscope (199 in attached picture, also measuring ~189 on occasion).&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;i2c@3100 {
			clock-frequency = &amp;lt;100000&amp;gt;;
};&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;kernel logs indicated a correct clock-frequency being set&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;[ 3.458027] mpc-i2c ffe03100.i2c: clock 94696 Hz (dfsrr=43 fdr=13)
[ 3.464217] mpc-i2c ffe03100.i2c: timeout 1000000 us&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;CCB is 533MHz&lt;/P&gt;&lt;P&gt;Kernel is&amp;nbsp;4.19.87&lt;/P&gt;</description>
      <pubDate>Wed, 26 Jul 2023 10:08:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P1022-Incorrect-i2c-clock-frequency/m-p/1692978#M5159</guid>
      <dc:creator>rro</dc:creator>
      <dc:date>2023-07-26T10:08:34Z</dc:date>
    </item>
    <item>
      <title>Re: P1022 Incorrect i2c clock frequency</title>
      <link>https://community.nxp.com/t5/P-Series/P1022-Incorrect-i2c-clock-frequency/m-p/1695621#M5160</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/155851"&gt;@rro&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Which sdk version you are using for your setup?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks&lt;/P&gt;
&lt;P&gt;Khushbu&lt;/P&gt;</description>
      <pubDate>Mon, 31 Jul 2023 07:45:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P1022-Incorrect-i2c-clock-frequency/m-p/1695621#M5160</guid>
      <dc:creator>khushbur</dc:creator>
      <dc:date>2023-07-31T07:45:35Z</dc:date>
    </item>
    <item>
      <title>Re: P1022 Incorrect i2c clock frequency</title>
      <link>https://community.nxp.com/t5/P-Series/P1022-Incorrect-i2c-clock-frequency/m-p/1695642#M5162</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;None. Everything is built using a custom toolchain built using crosstool-ng for the&amp;nbsp;powerpc-e500v2 architecture&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 31 Jul 2023 07:55:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P1022-Incorrect-i2c-clock-frequency/m-p/1695642#M5162</guid>
      <dc:creator>rro</dc:creator>
      <dc:date>2023-07-31T07:55:04Z</dc:date>
    </item>
    <item>
      <title>Re: P1022 Incorrect i2c clock frequency</title>
      <link>https://community.nxp.com/t5/P-Series/P1022-Incorrect-i2c-clock-frequency/m-p/1695646#M5163</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/155851"&gt;@rro&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Can you please share kernel version and boot logs?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks&lt;/P&gt;
&lt;P&gt;Khushbu&lt;/P&gt;</description>
      <pubDate>Mon, 31 Jul 2023 07:57:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P1022-Incorrect-i2c-clock-frequency/m-p/1695646#M5163</guid>
      <dc:creator>khushbur</dc:creator>
      <dc:date>2023-07-31T07:57:02Z</dc:date>
    </item>
    <item>
      <title>Re: P1022 Incorrect i2c clock frequency</title>
      <link>https://community.nxp.com/t5/P-Series/P1022-Incorrect-i2c-clock-frequency/m-p/1695657#M5164</link>
      <description>&lt;P&gt;Kernel version is&amp;nbsp;4.19.87&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;relevant logs&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;U-Boot 2019.07-rel_6_1_0 (Aug 01 2022 - 13:53:06 +0200)

CPU0:  P1022, Version: 1.1, (0x80e60011)
Core:  e500, Version: 5.1, (0x80211151)
Clock Configuration:
       CPU0:1066.667 MHz, CPU1:533.333 MHz,
       CCB:533.333 MHz,
       DDR:400  MHz (800 MT/s data rate) (Asynchronous), LBC:533.333 MHz
L1:    D-cache 32 KiB enabled
       I-cache 32 KiB enabled
I2C:   ready
DRAM:  Detected UDIMM M3ST-2GSVFLPC-E
2 GiB (DDR3, 64-bit, CL=6, ECC off)
Flash: 256 MiB
L2:    256 KiB enabled
MMC:   FSL_SDHC: 0
Delay startup for 1000 ms to wait for FPGA configuration!
PCIe1: Root Complex, x1 gen1, regs @ 0xffe0a000
PCIe1: Bus 00 - 02
In:    serial
Out:   serial
Err:   serial
MA0:   00:01:bb:01:e5:29
MA1:   00:01:bb:21:e5:29
RTC:   Valid
Net:   eTSEC0, eTSEC1 [PRIME]

....

[    0.000000] Linux version 4.19.87 (gcc version 9.2.0 (crosstool-NG - rel_1_24_4)) #1 SMP PREEMPT Fri Jul 22 13:58:29 CEST 2022

....
[    3.442921] i2c /dev entries driver
[    3.446552] mpc-i2c ffe03000.i2c: clock 396825 Hz (dfsrr=32 fdr=3)
[    3.452739] mpc-i2c ffe03000.i2c: timeout 1000000 us
[    3.458027] mpc-i2c ffe03100.i2c: clock 94696 Hz (dfsrr=43 fdr=13)
[    3.464217] mpc-i2c ffe03100.i2c: timeout 1000000 us&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 31 Jul 2023 08:05:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P1022-Incorrect-i2c-clock-frequency/m-p/1695657#M5164</guid>
      <dc:creator>rro</dc:creator>
      <dc:date>2023-07-31T08:05:25Z</dc:date>
    </item>
    <item>
      <title>Re: P1022 Incorrect i2c clock frequency</title>
      <link>https://community.nxp.com/t5/P-Series/P1022-Incorrect-i2c-clock-frequency/m-p/1697461#M5166</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/155851"&gt;@rro&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please refer p1022 reference manual section&amp;nbsp;11.4.3 I2C frequency divider register and&amp;nbsp;11.4.7 I2C digital filter sampling rate register. I2c frequency can be affected by FDR. Please refer&amp;nbsp;application note AN2919 for FDR calculation.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks&lt;/P&gt;
&lt;P&gt;Khushbu&amp;nbsp;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 02 Aug 2023 09:35:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P1022-Incorrect-i2c-clock-frequency/m-p/1697461#M5166</guid>
      <dc:creator>khushbur</dc:creator>
      <dc:date>2023-08-02T09:35:53Z</dc:date>
    </item>
    <item>
      <title>Re: P1022 Incorrect i2c clock frequency</title>
      <link>https://community.nxp.com/t5/P-Series/P1022-Incorrect-i2c-clock-frequency/m-p/1697468#M5167</link>
      <description>&lt;P&gt;hi,&lt;/P&gt;&lt;P&gt;Yes I have consulted that section and confirmed that everything is being computed correctly, at least according to what the kernel messages say.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;But as I mentioned, the reported set frequency does not match the measured frequency with the oscilloscope&lt;/P&gt;</description>
      <pubDate>Wed, 02 Aug 2023 09:39:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P1022-Incorrect-i2c-clock-frequency/m-p/1697468#M5167</guid>
      <dc:creator>rro</dc:creator>
      <dc:date>2023-08-02T09:39:40Z</dc:date>
    </item>
    <item>
      <title>Re: P1022 Incorrect i2c clock frequency</title>
      <link>https://community.nxp.com/t5/P-Series/P1022-Incorrect-i2c-clock-frequency/m-p/1701941#M5168</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/155851"&gt;@rro&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Can you please set clock-frequency = &amp;lt;400000&amp;gt; and measure clock. Please also share your dts file.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks&lt;/P&gt;
&lt;P&gt;Khushbu&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 09 Aug 2023 12:41:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P1022-Incorrect-i2c-clock-frequency/m-p/1701941#M5168</guid>
      <dc:creator>khushbur</dc:creator>
      <dc:date>2023-08-09T12:41:16Z</dc:date>
    </item>
    <item>
      <title>Re: P1022 Incorrect i2c clock frequency</title>
      <link>https://community.nxp.com/t5/P-Series/P1022-Incorrect-i2c-clock-frequency/m-p/1708288#M5169</link>
      <description>&lt;P&gt;I need to clarify internally how I should proceed on this issue. I will follow up with more information / the results of the 400000 test.&lt;/P&gt;&lt;P&gt;The relevant section of the DTS has already been provided in the original post&lt;/P&gt;</description>
      <pubDate>Mon, 21 Aug 2023 10:20:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P1022-Incorrect-i2c-clock-frequency/m-p/1708288#M5169</guid>
      <dc:creator>rro</dc:creator>
      <dc:date>2023-08-21T10:20:12Z</dc:date>
    </item>
  </channel>
</rss>