<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>P-SeriesのトピックRe: Performance evaluation</title>
    <link>https://community.nxp.com/t5/P-Series/Performance-evaluation/m-p/1417256#M5066</link>
    <description>&lt;P&gt;Online Power Monitoring&lt;BR /&gt;The Lm-sensors tool ( download from &lt;A href="http://dl.lm-sensors.org/lm-sensors/releases" target="_blank"&gt;http://dl.lm-sensors.org/lm-sensors/releases&lt;/A&gt;) will be used to read the power/temperature from on-boards sensors.&lt;/P&gt;
&lt;P&gt;Memory and CPU usage, you could use "top" command provided in Linux.&lt;/P&gt;</description>
    <pubDate>Tue, 22 Feb 2022 06:59:43 GMT</pubDate>
    <dc:creator>yipingwang</dc:creator>
    <dc:date>2022-02-22T06:59:43Z</dc:date>
    <item>
      <title>Performance evaluation</title>
      <link>https://community.nxp.com/t5/P-Series/Performance-evaluation/m-p/1416945#M5063</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am developing security solutions for embedded applications on the P2020-RDB design board. I would like to know if there is a way for me to evaluate the overhead of my solution (power, processing, memory) as the target solutions are constrained.&lt;/P&gt;&lt;P&gt;I am using SDK 1.9 Linux image, so any solution being either Linux-based or from a NXP tool/plugin would do. I am using TAP over ethernet for probing, so anything on that direction would do for me too.&lt;/P&gt;&lt;P&gt;Thanks,&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 21 Feb 2022 17:59:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Performance-evaluation/m-p/1416945#M5063</guid>
      <dc:creator>felipe-gm</dc:creator>
      <dc:date>2022-02-21T17:59:20Z</dc:date>
    </item>
    <item>
      <title>Re: Performance evaluation</title>
      <link>https://community.nxp.com/t5/P-Series/Performance-evaluation/m-p/1417256#M5066</link>
      <description>&lt;P&gt;Online Power Monitoring&lt;BR /&gt;The Lm-sensors tool ( download from &lt;A href="http://dl.lm-sensors.org/lm-sensors/releases" target="_blank"&gt;http://dl.lm-sensors.org/lm-sensors/releases&lt;/A&gt;) will be used to read the power/temperature from on-boards sensors.&lt;/P&gt;
&lt;P&gt;Memory and CPU usage, you could use "top" command provided in Linux.&lt;/P&gt;</description>
      <pubDate>Tue, 22 Feb 2022 06:59:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Performance-evaluation/m-p/1417256#M5066</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2022-02-22T06:59:43Z</dc:date>
    </item>
    <item>
      <title>Re: Performance evaluation</title>
      <link>https://community.nxp.com/t5/P-Series/Performance-evaluation/m-p/1417614#M5069</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/52411"&gt;@yipingwang&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;thank you very much for your response. The link seems to be broken.&lt;BR /&gt;One question though, aren't these methods intrusive, in the sense that they can interfere with the metrics?&lt;/P&gt;&lt;P&gt;Thanks once again&lt;/P&gt;</description>
      <pubDate>Tue, 22 Feb 2022 16:25:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Performance-evaluation/m-p/1417614#M5069</guid>
      <dc:creator>felipe-gm</dc:creator>
      <dc:date>2022-02-22T16:25:37Z</dc:date>
    </item>
    <item>
      <title>Re: Performance evaluation</title>
      <link>https://community.nxp.com/t5/P-Series/Performance-evaluation/m-p/1418146#M5070</link>
      <description>&lt;P&gt;Please download QorIQ SDK 1.9 user manual from the following link.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://drive.google.com/file/d/1GdxWp1zd8HyBCGka2T5j1euphEfLf9iU/view?usp=sharing" target="_blank"&gt;https://drive.google.com/file/d/1GdxWp1zd8HyBCGka2T5j1euphEfLf9iU/view?usp=sharing&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Please refer to section "Offline Power Monitoring" section in this user manual.&lt;/P&gt;</description>
      <pubDate>Wed, 23 Feb 2022 10:00:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Performance-evaluation/m-p/1418146#M5070</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2022-02-23T10:00:44Z</dc:date>
    </item>
    <item>
      <title>Re: Performance evaluation</title>
      <link>https://community.nxp.com/t5/P-Series/Performance-evaluation/m-p/1429407#M5071</link>
      <description>&lt;P&gt;For the offiline solution, that is great thanks! As for the memory and CPU, top gives me the metrics while they are executing, but I was looking for something that could capture these for programs that execute and end. It is tricky to capture the metrics with top like that.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any suggestions?&lt;/P&gt;</description>
      <pubDate>Wed, 16 Mar 2022 15:20:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Performance-evaluation/m-p/1429407#M5071</guid>
      <dc:creator>felipe-gm</dc:creator>
      <dc:date>2022-03-16T15:20:03Z</dc:date>
    </item>
  </channel>
</rss>