<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>P-Series中的主题 P2041 USB High Speed EHCI Controller Disable / Forcing only Full-Speed Connect</title>
    <link>https://community.nxp.com/t5/P-Series/P2041-USB-High-Speed-EHCI-Controller-Disable-Forcing-only-Full/m-p/1244118#M4987</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We are wondering that whether we can disable the USB High-Speed Control interface in P2041 in order to force the USB controller work in only Full-Speed or Low-Speed Mode.&amp;nbsp;&lt;/P&gt;&lt;P&gt;24th bit (PFSC) of USBx_PORTSC register is usefull for this purpose but, in this register, there is a note that " this bit is only for debugging purposes".&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 11 Mar 2021 10:48:32 GMT</pubDate>
    <dc:creator>fsever</dc:creator>
    <dc:date>2021-03-11T10:48:32Z</dc:date>
    <item>
      <title>P2041 USB High Speed EHCI Controller Disable / Forcing only Full-Speed Connect</title>
      <link>https://community.nxp.com/t5/P-Series/P2041-USB-High-Speed-EHCI-Controller-Disable-Forcing-only-Full/m-p/1244118#M4987</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We are wondering that whether we can disable the USB High-Speed Control interface in P2041 in order to force the USB controller work in only Full-Speed or Low-Speed Mode.&amp;nbsp;&lt;/P&gt;&lt;P&gt;24th bit (PFSC) of USBx_PORTSC register is usefull for this purpose but, in this register, there is a note that " this bit is only for debugging purposes".&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 11 Mar 2021 10:48:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P2041-USB-High-Speed-EHCI-Controller-Disable-Forcing-only-Full/m-p/1244118#M4987</guid>
      <dc:creator>fsever</dc:creator>
      <dc:date>2021-03-11T10:48:32Z</dc:date>
    </item>
    <item>
      <title>Re: P2041 USB High Speed EHCI Controller Disable / Forcing only Full-Speed Connect</title>
      <link>https://community.nxp.com/t5/P-Series/P2041-USB-High-Speed-EHCI-Controller-Disable-Forcing-only-Full/m-p/1244139#M4988</link>
      <description>&lt;P&gt;The &lt;FONT class="&amp;amp;quothighlight&amp;quot;"&gt;PFSC&lt;/FONT&gt; bit prevents the USB controller from declaring itself as a High-Speed and the Full-Speed link is established at a USB bus reset. So, the &lt;FONT class="&amp;amp;quothighlight&amp;quot;"&gt;PFSC&lt;/FONT&gt; bit can be used for both testing and functional modes; there is no limitation to use it in debug mode only.&lt;/P&gt;</description>
      <pubDate>Thu, 11 Mar 2021 11:42:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P2041-USB-High-Speed-EHCI-Controller-Disable-Forcing-only-Full/m-p/1244139#M4988</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2021-03-11T11:42:49Z</dc:date>
    </item>
    <item>
      <title>Re: P2041 USB High Speed EHCI Controller Disable / Forcing only Full-Speed Connect</title>
      <link>https://community.nxp.com/t5/P-Series/P2041-USB-High-Speed-EHCI-Controller-Disable-Forcing-only-Full/m-p/1268280#M4992</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I need to force full speed for EHCI host in u-boot. Do you know where in the driver I need to set the PFSC bit?&lt;/P&gt;&lt;P&gt;Thanks,&amp;nbsp;-Vitaly&lt;/P&gt;</description>
      <pubDate>Mon, 26 Apr 2021 17:13:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P2041-USB-High-Speed-EHCI-Controller-Disable-Forcing-only-Full/m-p/1268280#M4992</guid>
      <dc:creator>vitaly_a</dc:creator>
      <dc:date>2021-04-26T17:13:55Z</dc:date>
    </item>
  </channel>
</rss>