<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>P-SeriesのトピックRe: PCie in P2020</title>
    <link>https://community.nxp.com/t5/P-Series/PCie-in-P2020/m-p/1193143#M4972</link>
    <description>&lt;P&gt;&amp;gt; Does the commands give registers inside the ICs connected to miniPCIe&lt;BR clear="none" /&gt;No.&lt;/P&gt;
&lt;P&gt;To determine how PCIe EP memory is mapped into the P2020 local address space you have to read the P2020 PCIe Outbound ATMU registers values.&lt;/P&gt;</description>
    <pubDate>Thu, 03 Dec 2020 10:18:18 GMT</pubDate>
    <dc:creator>ufedor</dc:creator>
    <dc:date>2020-12-03T10:18:18Z</dc:date>
    <item>
      <title>PCie in P2020</title>
      <link>https://community.nxp.com/t5/P-Series/PCie-in-P2020/m-p/1193060#M4971</link>
      <description>&lt;P&gt;I have P2020 RDB to which i have connected a miniPCIe board on which 2 ICs are there.&lt;/P&gt;&lt;P&gt;I am able to access the mini pCie device in uboot log as shown-&lt;/P&gt;&lt;P&gt;PCIe1: Root Complex of mini PCIe SLOT, x1, regs @ 0xffe0a000&lt;BR /&gt;01:00.0 - 104c:8240 - Bridge device&lt;BR /&gt;02:00.0 - 4ddc:1a00 - Simple comm. controller&lt;BR /&gt;02:01.0 - 4ddc:1a00 - Simple comm. controller&lt;/P&gt;&lt;P&gt;And further command show in the log as follows-&lt;/P&gt;&lt;P&gt;pci header 02.00.0&lt;BR /&gt;vendor ID = 0x4ddc&lt;BR /&gt;device ID = 0x1a00&lt;BR /&gt;command register = 0x0006&lt;BR /&gt;status register = 0x02a0&lt;BR /&gt;revision ID = 0x10&lt;BR /&gt;class code = 0x07 (Simple comm. controller)&lt;BR /&gt;sub class code = 0x80&lt;BR /&gt;programming interface = 0x00&lt;BR /&gt;cache line = 0x08&lt;BR /&gt;latency time = 0x80&lt;BR /&gt;header type = 0x00&lt;BR /&gt;BIST = 0x00&lt;BR /&gt;base address 0 = 0x80000000&lt;BR /&gt;base address 1 = 0x80040000&lt;BR /&gt;base address 2 = 0x00000000&lt;BR /&gt;base address 3 = 0x00000000&lt;BR /&gt;base address 4 = 0x00000000&lt;BR /&gt;base address 5 = 0x00000000&lt;BR /&gt;cardBus CIS pointer = 0x00000000&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I want to access the registers inside the device at "2.00.0". Seeing the BAR0, I gave the following command-&lt;/P&gt;&lt;P&gt;md 0x80000000 10.&amp;nbsp;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Capture2.JPG" style="width: 855px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/131659iFFA928E2FA311034/image-size/large?v=v2&amp;amp;px=999" role="button" title="Capture2.JPG" alt="Capture2.JPG" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Capture3.JPG" style="width: 825px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/131660iCA881CE323E28B05/image-size/large?v=v2&amp;amp;px=999" role="button" title="Capture3.JPG" alt="Capture3.JPG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is it correct way to access the registers inside the pCIe device? How do i know whether i am accessing correct memory address.&amp;nbsp; Can anyone tell.&lt;/P&gt;</description>
      <pubDate>Thu, 03 Dec 2020 09:21:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/PCie-in-P2020/m-p/1193060#M4971</guid>
      <dc:creator>monalihaware</dc:creator>
      <dc:date>2020-12-03T09:21:32Z</dc:date>
    </item>
    <item>
      <title>Re: PCie in P2020</title>
      <link>https://community.nxp.com/t5/P-Series/PCie-in-P2020/m-p/1193143#M4972</link>
      <description>&lt;P&gt;&amp;gt; Does the commands give registers inside the ICs connected to miniPCIe&lt;BR clear="none" /&gt;No.&lt;/P&gt;
&lt;P&gt;To determine how PCIe EP memory is mapped into the P2020 local address space you have to read the P2020 PCIe Outbound ATMU registers values.&lt;/P&gt;</description>
      <pubDate>Thu, 03 Dec 2020 10:18:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/PCie-in-P2020/m-p/1193143#M4972</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2020-12-03T10:18:18Z</dc:date>
    </item>
  </channel>
</rss>