<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>P-SeriesのトピックRe: Quick Start Guidance</title>
    <link>https://community.nxp.com/t5/P-Series/Quick-Start-Guidance/m-p/1151705#M4953</link>
    <description>&lt;P&gt;How do you plug and play without a monitor?&amp;nbsp; Do you have guidance on how to use a laptop as a host and get in that way?&amp;nbsp; Putty? Port id's, IP addresses, Username, Password?&lt;/P&gt;&lt;P&gt;Does it not have Linux already installed?&amp;nbsp;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 10 Sep 2020 17:12:57 GMT</pubDate>
    <dc:creator>WmBAnderson</dc:creator>
    <dc:date>2020-09-10T17:12:57Z</dc:date>
    <item>
      <title>Quick Start Guidance</title>
      <link>https://community.nxp.com/t5/P-Series/Quick-Start-Guidance/m-p/1151120#M4951</link>
      <description>&lt;P&gt;Just recieved the P4080DS-PC kit and can find no initial startup instructions.&amp;nbsp; There is a spec sheet with default settings and a set of Linux CD's.&amp;nbsp; The support chat line offers no assistance.&amp;nbsp; Do I just plug and play?&amp;nbsp; Any concerns about static discharge damage to inspect the internals?&amp;nbsp; Shipping retainer bolts or hold downs that should be removed?&amp;nbsp; Other cautions?&lt;/P&gt;&lt;P&gt;Thanks for any suggestions.&lt;/P&gt;&lt;P&gt;Bill&lt;/P&gt;</description>
      <pubDate>Wed, 09 Sep 2020 21:04:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Quick-Start-Guidance/m-p/1151120#M4951</guid>
      <dc:creator>WmBAnderson</dc:creator>
      <dc:date>2020-09-09T21:04:14Z</dc:date>
    </item>
    <item>
      <title>Re: Quick Start Guidance</title>
      <link>https://community.nxp.com/t5/P-Series/Quick-Start-Guidance/m-p/1151254#M4952</link>
      <description>&lt;P&gt;&amp;gt; Do I just plug and play?&lt;/P&gt;
&lt;P&gt;Yes.&lt;/P&gt;
&lt;P&gt;&amp;gt; Any concerns about static discharge damage to inspect the internals?&lt;/P&gt;
&lt;P&gt;General principles of electronic equipment handling have to be considered.&lt;/P&gt;
&lt;P&gt;&amp;gt; Shipping retainer bolts or hold downs that should be removed?&lt;/P&gt;
&lt;P&gt;No.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;P4080DS User's Guide:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/user-guide/P4080DSUG.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/user-guide/P4080DSUG.pdf&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 10 Sep 2020 03:29:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Quick-Start-Guidance/m-p/1151254#M4952</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2020-09-10T03:29:36Z</dc:date>
    </item>
    <item>
      <title>Re: Quick Start Guidance</title>
      <link>https://community.nxp.com/t5/P-Series/Quick-Start-Guidance/m-p/1151705#M4953</link>
      <description>&lt;P&gt;How do you plug and play without a monitor?&amp;nbsp; Do you have guidance on how to use a laptop as a host and get in that way?&amp;nbsp; Putty? Port id's, IP addresses, Username, Password?&lt;/P&gt;&lt;P&gt;Does it not have Linux already installed?&amp;nbsp;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 10 Sep 2020 17:12:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Quick-Start-Guidance/m-p/1151705#M4953</guid>
      <dc:creator>WmBAnderson</dc:creator>
      <dc:date>2020-09-10T17:12:57Z</dc:date>
    </item>
    <item>
      <title>Re: Quick Start Guidance</title>
      <link>https://community.nxp.com/t5/P-Series/Quick-Start-Guidance/m-p/1151711#M4954</link>
      <description>&lt;P&gt;Default UART port is the bottom one (close to the PCB). To view the output, connect a null-modem serial cable from the serial port to your computer. Open a terminal program and set it up to match these settings:&lt;BR /&gt;Baud Rate: 115200 Data Bits: 8&lt;BR /&gt;Parity: None&lt;BR /&gt;Stop Bits: 1&lt;BR /&gt;Flow Control: None&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;gt; Does it not have Linux already installed?&amp;nbsp;&lt;/P&gt;&lt;P&gt;U-Boot and Linux should be installed.&lt;/P&gt;</description>
      <pubDate>Thu, 10 Sep 2020 17:38:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Quick-Start-Guidance/m-p/1151711#M4954</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2020-09-10T17:38:41Z</dc:date>
    </item>
    <item>
      <title>Re: Quick Start Guidance</title>
      <link>https://community.nxp.com/t5/P-Series/Quick-Start-Guidance/m-p/1151725#M4955</link>
      <description>&lt;P&gt;Can I use a USB port to connect as a terminal?&lt;/P&gt;&lt;P&gt;BTW - What is the function of the&amp;nbsp; "Hydrid" switch next to the power on/off switch and how should it be set?&amp;nbsp; (i can't find the word "Hybrid" in the user manual).&lt;/P&gt;</description>
      <pubDate>Thu, 10 Sep 2020 18:15:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Quick-Start-Guidance/m-p/1151725#M4955</guid>
      <dc:creator>WmBAnderson</dc:creator>
      <dc:date>2020-09-10T18:15:49Z</dc:date>
    </item>
    <item>
      <title>Re: Quick Start Guidance</title>
      <link>https://community.nxp.com/t5/P-Series/Quick-Start-Guidance/m-p/1151731#M4956</link>
      <description>&lt;P&gt;&amp;gt; Can I use a USB port to connect as a terminal?&lt;/P&gt;
&lt;P&gt;It is possible using COM-to-USB converter.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;There is no mentioned button in the P4080DS schematics.&lt;/P&gt;</description>
      <pubDate>Thu, 10 Sep 2020 18:28:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Quick-Start-Guidance/m-p/1151731#M4956</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2020-09-10T18:28:35Z</dc:date>
    </item>
    <item>
      <title>Re: Quick Start Guidance</title>
      <link>https://community.nxp.com/t5/P-Series/Quick-Start-Guidance/m-p/1158723#M4957</link>
      <description>&lt;P&gt;OK I have my P4080 and T1040 up and running with a terminal interface.&lt;/P&gt;&lt;P&gt;How do I enable ethernet ?&lt;/P&gt;&lt;P&gt;I can the /etc/network/interfaces file, at least on the P4080 looks like this;&lt;/P&gt;&lt;P&gt;The loopback interface&lt;BR /&gt;auto lo&lt;BR /&gt;iface lo inet loopback&lt;/P&gt;&lt;P&gt;# Wireless interfaces&lt;BR /&gt;iface wlan0 inet dhcp&lt;BR /&gt;wireless_mode managed&lt;BR /&gt;wireless_essid any&lt;BR /&gt;wpa-driver wext&lt;BR /&gt;wpa-conf /etc/wpa_supplicant.conf&lt;/P&gt;&lt;P&gt;iface atml0 inet dhcp&lt;/P&gt;&lt;P&gt;# Wired or wireless interfaces&lt;BR /&gt;#auto eth0&lt;BR /&gt;iface eth0 inet dhcp&lt;BR /&gt;iface eth1 inet dhcp&lt;/P&gt;&lt;P&gt;# Ethernet/RNDIS gadget (g_ether)&lt;BR /&gt;# ... or on host side, usbnet and random hwaddr&lt;BR /&gt;iface usb0 inet static&lt;BR /&gt;address 192.168.7.2&lt;BR /&gt;netmask 255.255.255.0&lt;BR /&gt;network 192.168.7.0&lt;BR /&gt;gateway 192.168.7.1&lt;/P&gt;&lt;P&gt;# Bluetooth networking&lt;BR /&gt;iface bnep0 inet dhcp&lt;/P&gt;&lt;P&gt;But how do I id my wireless lan SID &amp;amp; password or provide login info for a wired ethernet?&lt;/P&gt;&lt;P&gt;Any help is much appreciated,&lt;/P&gt;&lt;P&gt;R/&lt;/P&gt;&lt;P&gt;Bill&lt;/P&gt;</description>
      <pubDate>Thu, 24 Sep 2020 13:46:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Quick-Start-Guidance/m-p/1158723#M4957</guid>
      <dc:creator>WmBAnderson</dc:creator>
      <dc:date>2020-09-24T13:46:32Z</dc:date>
    </item>
  </channel>
</rss>